CreateNewComponentBuilderComponentReferenceSetType Enumeration¶
NXOpen.Assemblies.CreateNewComponentBuilder.ComponentReferenceSetType is an alias for NXOpen.Assemblies.CreateNewComponentBuilderComponentReferenceSetType
-
class
NXOpen.Assemblies.
CreateNewComponentBuilderComponentReferenceSetType
¶ Bases:
object
Set the reference set
Enum Members
Enum Member Enum Member Description Model Set the reference set to modelEntirePartOnly Set the reference set to entire part onlyOther Set the reference to other-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-