AssembliesGeneralPropertiesBuilderReferenceComponentOptions Enumeration¶
NXOpen.Assemblies.AssembliesGeneralPropertiesBuilder.ReferenceComponentOptions is an alias for NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderReferenceComponentOptions
-
class
NXOpen.Assemblies.
AssembliesGeneralPropertiesBuilderReferenceComponentOptions
¶ Bases:
object
Options for setting the reference-only property on the components
Enum Members
Enum Member Enum Member Description No Objects will be non reference-only componentsYes Objects will be reference-only componentsMixed Objects are a mixture of reference-only and non reference-only components, and will not be changed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-