AttributeSearchTermBuilder Class¶
-
class
NXOpen.Assemblies.
AttributeSearchTermBuilder
¶ Bases:
NXOpen.Assemblies.SearchTermBuilder
An AttributeSearchTermBuilder is used to create or edit an
NXOpen.Assemblies.AttributeSearchTerm
.To create a new instance of this class, use
NXOpen.Assemblies.SubsetCollection.CreateAttributeSearchTermBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
QueryName | Returns or sets the name of the saved query upon which this search term is based. |
SearchTermLogic | Returns or sets the search term logic. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCriteria | Get the entry titles and values that are used to populate the saved query. |
GetObject | Returns the object currently being edited by this builder. |
SetCriteria | Set the entry titles and values that are used to populate the saved query. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
QueryName¶
-
AttributeSearchTermBuilder.
QueryName
¶ Returns or sets the name of the saved query upon which this search term is based.
-------------------------------------
Getter Method
Signature
QueryName()
Returns: Return type: str New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
QueryName(queryName)
Parameters: queryName (str) – New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SearchTermLogic¶
-
AttributeSearchTermBuilder.
SearchTermLogic
¶ Returns or sets the search term logic.
-------------------------------------
Getter Method
Signature
SearchTermLogic()
Returns: Return type: NXOpen.Assemblies.SearchTermSearchTermLogicType
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
SearchTermLogic(searchTermLogic)
Parameters: searchTermLogic ( NXOpen.Assemblies.SearchTermSearchTermLogicType
) –New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Method Detail¶
GetCriteria¶
-
AttributeSearchTermBuilder.
GetCriteria
¶ Get the entry titles and values that are used to populate the saved query.
Signature
GetCriteria()
Returns: a tuple Return type: A tuple consisting of (titles, values). titles is a list of str. search criteria titles values is a list of str. search criteria values New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SetCriteria¶
-
AttributeSearchTermBuilder.
SetCriteria
¶ Set the entry titles and values that are used to populate the saved query.
Signature
SetCriteria(titles, values)
Parameters: - titles (list of str) – search criteria titles
- values (list of str) – search criteria values
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Validate¶
-
AttributeSearchTermBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.