ComponentPatternBuilder Class¶
-
class
NXOpen.Assemblies.
ComponentPatternBuilder
¶ Bases:
NXOpen.Builder
Represents a builder class that performs various
NXOpen.Assemblies.ComponentPattern
operations.Input to this class can be PSM facet objects.
To create a new instance of this class, use
NXOpen.Assemblies.ComponentAssembly.CreateComponentPatternBuilder()
Default values.
Property Value PatternService.AlongPathDefinition.XOnPathSpacing.NCopies.Value 2 PatternService.AlongPathDefinition.XOnPathSpacing.SpaceType Offset PatternService.AlongPathDefinition.XPathOption Offset PatternService.AlongPathDefinition.YDirectionOption Section PatternService.AlongPathDefinition.YOnPathSpacing.NCopies.Value 1 PatternService.AlongPathDefinition.YPathOption Offset PatternService.AlongPathDefinition.YSpacing.NCopies.Value 1 PatternService.AlongPathDefinition.YSpacing.PitchDistance.Value 10 (millimeters part), 1 (inches part) PatternService.AlongPathDefinition.YSpacing.SpaceType Offset PatternService.AlongPathDefinition.YSpacing.SpanDistance.Value 100 (millimeters part), 10 (inches part) PatternService.CircularDefinition.AngularSpacing.NCopies.Value 12 PatternService.CircularDefinition.AngularSpacing.PitchAngle.Value 30 PatternService.CircularDefinition.AngularSpacing.PitchDistance.Value 10 (millimeters part), 1 (inches part) PatternService.CircularDefinition.AngularSpacing.SpaceType Offset PatternService.CircularDefinition.AngularSpacing.SpanAngle.Value 360 (millimeters part), 360 (inches part) PatternService.CircularDefinition.AngularSpacing.UsePitchOption Angle PatternService.CircularDefinition.CreateLastStaggered true PatternService.CircularDefinition.HorizontalRef.RotationAngle.Value 0 (millimeters part), 0 (inches part) PatternService.CircularDefinition.IncludeSeedToggle true PatternService.CircularDefinition.RadialSpacing.NCopies.Value 1 PatternService.CircularDefinition.StaggerType None PatternService.HelixDefinition.AnglePitch.Value 30 PatternService.HelixDefinition.CountOfInstances.Value 6 PatternService.HelixDefinition.DirectionType Righthand PatternService.HelixDefinition.DistancePitch.Value 10 (millimeters part), 0.4 (inches part) PatternService.HelixDefinition.HelixPitch.Value 50 (millimeters part), 2 (inches part) PatternService.HelixDefinition.HelixSpan.Value 100 (millimeters part), 4 (inches part) PatternService.HelixDefinition.NumberOfTurns.Value 2 PatternService.HelixDefinition.SizeOption CountAngleDistance PatternService.PatternFill.FillMargin.Value 0 (millimeters part), 0 (inches part) PatternService.PatternFill.FillOptions None PatternService.PatternFill.SimplifiedBoundaryToggle False PatternService.PatternOrientation.AlongOrientationOption NormalToPath PatternService.PatternOrientation.CircularOrientationOption FollowPattern PatternService.PatternOrientation.FollowFaceProjDirOption PatternPlaneNormal PatternService.PatternOrientation.GeneralOrientationOption Fixed PatternService.PatternOrientation.HelixOrientationOption FollowPattern PatternService.PatternOrientation.LinearOrientationOption Fixed PatternService.PatternOrientation.MirrorOrientationOption FollowPattern PatternService.PatternOrientation.OrientationOption Fixed PatternService.PatternOrientation.PolygonOrientationOption FollowPattern PatternService.PatternOrientation.SpiralOrientationOption FollowPattern PatternService.PatternType Linear PatternService.PolygonDefinition.NumberOfSides.Value 6 PatternService.PolygonDefinition.PolygonSizeOption Inscribed PatternService.PolygonDefinition.PolygonSpacing.NCopies.Value 4 PatternService.PolygonDefinition.PolygonSpacing.PitchDistance.Value 25 (millimeters part), 1 (inches part) PatternService.PolygonDefinition.PolygonSpacing.SpaceType Offset PatternService.PolygonDefinition.PolygonSpacing.SpanAngle.Value 360 PatternService.PolygonDefinition.RadialSpacing.NCopies.Value 1 PatternService.PolygonDefinition.RadialSpacing.PitchDistance.Value 25 (millimeters part), 1 (inches part) PatternService.PolygonDefinition.RadialSpacing.SpanDistance.Value 100 (millimeters part), 4 (inches part) PatternService.RectangularDefinition.CreateLastStaggered true PatternService.RectangularDefinition.SimplifiedLayoutType Square PatternService.RectangularDefinition.StaggerType None PatternService.RectangularDefinition.XSpacing.NCopies.Value 2 PatternService.RectangularDefinition.YSpacing.NCopies.Value 1 PatternService.SpiralDefinition.DirectionType Lefthand PatternService.SpiralDefinition.NumberOfTurns.Value 1 (millimeters part), 1 (inches part) PatternService.SpiralDefinition.RadialPitch.Value 50 (millimeters part), 2 (inches part) PatternService.SpiralDefinition.SizeSpiralType NumberOfTurns PatternService.SpiralDefinition.TotalAngle.Value 360 (millimeters part), 360 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the option to specify whether the NXOpen.Assemblies.ComponentPattern is associative or not. |
ComponentPatternSet | Returns the NXOpen.Assemblies.Component for pattern. |
CopyConstraintPattern | Returns or sets the copy constraint option. |
PatternService | Returns the NXOpen.GeometricUtilities.PatternDefinition . |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDynamicPositioning | Returns the dynamic positioning flag. |
GetObject | Returns the object currently being edited by this builder. |
SetDynamicPositioning | Sets the dynamic positioning flag. |
SetObject | Sets the object selected for pattern definition |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Associative¶
-
ComponentPatternBuilder.
Associative
¶ Returns or sets the option to specify whether the
NXOpen.Assemblies.ComponentPattern
is associative or not.-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(isAssociative)
Parameters: isAssociative (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ComponentPatternSet¶
-
ComponentPatternBuilder.
ComponentPatternSet
¶ Returns the
NXOpen.Assemblies.Component
for pattern.-------------------------------------
Getter Method
Signature
ComponentPatternSet()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX9.0.0.
License requirements: None.
CopyConstraintPattern¶
-
ComponentPatternBuilder.
CopyConstraintPattern
¶ Returns or sets the copy constraint option.
The copy constraint type of pattern is created when this option is enabled otherwise Pure Reference pattern is created.
-------------------------------------
Getter Method
Signature
CopyConstraintPattern()
Returns: Return type: bool New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyConstraintPattern(isCopyConstraintReferencePattern)
Parameters: isCopyConstraintReferencePattern (bool) – New in version NX9.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
PatternService¶
-
ComponentPatternBuilder.
PatternService
¶ Returns the
NXOpen.GeometricUtilities.PatternDefinition
.-------------------------------------
Getter Method
Signature
PatternService()
Returns: Return type: NXOpen.GeometricUtilities.PatternDefinition
New in version NX9.0.0.
License requirements: None.
Method Detail¶
GetDynamicPositioning¶
-
ComponentPatternBuilder.
GetDynamicPositioning
¶ Returns the dynamic positioning flag.
Signature
GetDynamicPositioning()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
SetDynamicPositioning¶
-
ComponentPatternBuilder.
SetDynamicPositioning
¶ Sets the dynamic positioning flag.
It will enable or disable the dynamic preview of the components.
Signature
SetDynamicPositioning(isDynamicPositioning)
Parameters: isDynamicPositioning (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SetObject¶
-
ComponentPatternBuilder.
SetObject
¶ Sets the object selected for pattern definition
Signature
SetObject(compPattern)
Parameters: compPattern ( NXOpen.Assemblies.ComponentPattern
) – The pattern definition objectNew in version NX11.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Validate¶
-
ComponentPatternBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.