ComponentAssemblyCheckinCheckoutOption Enumeration¶
NXOpen.Assemblies.ComponentAssembly.CheckinCheckoutOption is an alias for NXOpen.Assemblies.ComponentAssemblyCheckinCheckoutOption
-
class
NXOpen.Assemblies.
ComponentAssemblyCheckinCheckoutOption
¶ Bases:
object
Check in and Check out options for components
Enum Members
Enum Member Enum Member Description DesignElement Checks in or Checks out the design elementSourceItem Checks in or Checks out the source item that is referenced by a reuse design element or subordinate design elementBoth Checks in or Checks out the design element and its referenced source itemDefault Check In or Check Out option is determined by the system using whatever option is appropriate for the selected object type. For Reuse design element, the system defaults to checking out both the design element and the underlying item.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-