PlaneSearchTermPlaneOverlapLogicType Enumeration¶
NXOpen.Assemblies.PlaneSearchTerm.PlaneOverlapLogicType is an alias for NXOpen.Assemblies.PlaneSearchTermPlaneOverlapLogicType
-
class
NXOpen.Assemblies.
PlaneSearchTermPlaneOverlapLogicType
¶ Bases:
object
Logic used to determine the type of inclusion used in a plane search term within a recipe.
Enum Members
Enum Member Enum Member Description Above Include objects residing above the plane defined by this search termBelow Include objects residing below the plane defined by this search termIntersects Include objects intersecting the plane defined by this search termAboveOrIntersects Include objects residing above or intersecting the plane defined by this search termBelowOrIntersects Include objects residing below or intersecting the plane defined by this search term-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-