ClearanceAnalysisBuilder Class¶
-
class
NXOpen.Assemblies.
ClearanceAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents
NXOpen.Assemblies.ClearanceAnalysisBuilder
.The builder builds the clearance set which contains properties for the analysis. The properties are:
Clearance Set Name: the name of the clearance set.
Clearance Type: either components or bodies or PSM facet objects.
Number of collections: either one or two. Where one collection is chosen, the analysis is performed between all objects in the collection. Where two collections are chosen, the analysis compares objects from one collection with objects from the other.
Exceptions: Select Subassemblies: Specific subassemblies selected within the displayed part can be treated as a single entity.
Explicitly Ignore: A number of options to reduce the amount of results reported.
Additional exceptions: Addtional pairs of objects to be excluded or included regardless of exception rules previously defined.
To create a new instance of this class, use
NXOpen.Assemblies.AssemblyManager.CreateClearanceAnalysisBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CalculationMethod | Returns or sets the setting for the clearance calculation method. |
ClearanceBetween | Returns or sets the setting to determine whether components or bodies should be used. |
ClearanceSetName | Returns or sets the clearance set name. |
CollectionOneObjects | Returns the selected objects for collection one. |
CollectionOneRange | Returns or sets the range setting for collection one. |
CollectionTwoObjects | Returns the selected objects for collection two. |
CollectionTwoRange | Returns or sets the range setting for collection two. |
InterferenceColor | Returns or sets the color of the interference geometry. |
IsCalculatePenetrationDepth | Returns or sets the setting to determine whether penetration depth should be calculated. |
IsIgnorePairsWithinSameGroup | Returns or sets the setting to determine whether to ignore pairs within same group. |
IsIgnorePairsWithinSamePart | Returns or sets the setting to determine whether to ignore pairs within same part. |
IsIgnorePairsWithinSameSubassembly | Returns or sets the setting to determine whether to ignore pairs within same subassembly. |
IsIgnorePairsWithinSelectedSubassemblies | Returns or sets the setting to determine whether to ignore pairs within the selected subassemblies. |
Layer | Returns or sets the layer for interference geometry. |
SaveInterferenceGeometry | Returns or sets the setting to determine if interference geometry should be saved. |
Tag | Returns the Tag for this object. |
TotalCollectionCount | Returns or sets the setting to determine whether one collection or two collections should be used. |
UnitSubassemblies | Returns the selected unit subassemblies. |
Methods¶
Method | Description |
---|---|
AddException | Add an exception. |
AddObjectClearanceZone | Add a Clearance Zone around an object. |
AddPairClearanceZone | Add a Clearance Zone between a pair of objects. |
Commit | Commits any edits that have been applied to the builder. |
CreateClearanceZoneExpression | Create an expression using the Clearance Zone naming convention. |
DeleteException | Delete an exception. |
DeleteObjectClearanceZone | Delete an existing Clearance Zone from around an object. |
DeletePairClearanceZone | Delete an existing Clearance Zone between the given pair of objects. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDefaultClearanceZone | Get the default Clearance Zone expression. |
GetIsPairIncluded | Inquires if an object pair is to be included in the analysis. |
GetObject | Returns the object currently being edited by this builder. |
GetObjectClearanceZone | Inquire the Clearance Zone assigned to a given object. |
GetPairClearanceZone | Inquire the Clearance Zone for a specific pair of objects. |
SetDefaultClearanceZone | Set the expression as the default Clearance Zone. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ClearanceAnalysisBuilderCalculationMethodType Enumeration | Specify the analysis method. |
ClearanceAnalysisBuilderClearanceBetweenEntity Enumeration | Specify the type of clearance analysis. |
ClearanceAnalysisBuilderClearanceZoneSource Enumeration | Specify the source of the clearance zone |
ClearanceAnalysisBuilderCollectionRange Enumeration | Specify how to compare objects inside a collection. |
ClearanceAnalysisBuilderNumberOfCollections Enumeration | Specify the number of collections used for clearance analysis. |
ClearanceAnalysisBuilderPairExcludedReason Enumeration | Specify the reason for excluding the pair |
ClearanceAnalysisBuilderZoneType Enumeration | Specify the clearance zone type. |
Property Detail¶
CalculationMethod¶
-
ClearanceAnalysisBuilder.
CalculationMethod
¶ Returns or sets the setting for the clearance calculation method.
-------------------------------------
Getter Method
Signature
CalculationMethod()
Returns: Return type: NXOpen.Assemblies.ClearanceAnalysisBuilderCalculationMethodType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CalculationMethod(calculateMethod)
Parameters: calculateMethod ( NXOpen.Assemblies.ClearanceAnalysisBuilderCalculationMethodType
) –New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ClearanceBetween¶
-
ClearanceAnalysisBuilder.
ClearanceBetween
¶ Returns or sets the setting to determine whether components or bodies should be used.
Please note that changing the collection type will clear the collections, exceptions and clearance zones from the clearance set
-------------------------------------
Getter Method
Signature
ClearanceBetween()
Returns: Return type: NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceBetweenEntity
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearanceBetween(clearanceBetweenEntity)
Parameters: clearanceBetweenEntity ( NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceBetweenEntity
) –New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ClearanceSetName¶
-
ClearanceAnalysisBuilder.
ClearanceSetName
¶ Returns or sets the clearance set name.
-------------------------------------
Getter Method
Signature
ClearanceSetName()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearanceSetName(clearanceSetName)
Parameters: clearanceSetName (str) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
CollectionOneObjects¶
-
ClearanceAnalysisBuilder.
CollectionOneObjects
¶ Returns the selected objects for collection one.
-------------------------------------
Getter Method
Signature
CollectionOneObjects()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
CollectionOneRange¶
-
ClearanceAnalysisBuilder.
CollectionOneRange
¶ Returns or sets the range setting for collection one.
-------------------------------------
Getter Method
Signature
CollectionOneRange()
Returns: Return type: NXOpen.Assemblies.ClearanceAnalysisBuilderCollectionRange
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollectionOneRange(collectionRange)
Parameters: collectionRange ( NXOpen.Assemblies.ClearanceAnalysisBuilderCollectionRange
) –New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
CollectionTwoObjects¶
-
ClearanceAnalysisBuilder.
CollectionTwoObjects
¶ Returns the selected objects for collection two.
-------------------------------------
Getter Method
Signature
CollectionTwoObjects()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX9.0.0.
License requirements: None.
CollectionTwoRange¶
-
ClearanceAnalysisBuilder.
CollectionTwoRange
¶ Returns or sets the range setting for collection two.
-------------------------------------
Getter Method
Signature
CollectionTwoRange()
Returns: Return type: NXOpen.Assemblies.ClearanceAnalysisBuilderCollectionRange
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollectionTwoRange(collectionRange)
Parameters: collectionRange ( NXOpen.Assemblies.ClearanceAnalysisBuilderCollectionRange
) –New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
InterferenceColor¶
-
ClearanceAnalysisBuilder.
InterferenceColor
¶ Returns or sets the color of the interference geometry.
-------------------------------------
Getter Method
Signature
InterferenceColor()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterferenceColor(color)
Parameters: color (Id) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
IsCalculatePenetrationDepth¶
-
ClearanceAnalysisBuilder.
IsCalculatePenetrationDepth
¶ Returns or sets the setting to determine whether penetration depth should be calculated.
-------------------------------------
Getter Method
Signature
IsCalculatePenetrationDepth()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCalculatePenetrationDepth(isCalculatePenetrationDepth)
Parameters: isCalculatePenetrationDepth (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
IsIgnorePairsWithinSameGroup¶
-
ClearanceAnalysisBuilder.
IsIgnorePairsWithinSameGroup
¶ Returns or sets the setting to determine whether to ignore pairs within same group.
-------------------------------------
Getter Method
Signature
IsIgnorePairsWithinSameGroup()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsIgnorePairsWithinSameGroup(isIgnorePairsWithinSameGroup)
Parameters: isIgnorePairsWithinSameGroup (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
IsIgnorePairsWithinSamePart¶
-
ClearanceAnalysisBuilder.
IsIgnorePairsWithinSamePart
¶ Returns or sets the setting to determine whether to ignore pairs within same part.
-------------------------------------
Getter Method
Signature
IsIgnorePairsWithinSamePart()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsIgnorePairsWithinSamePart(isIgnorePairsWithinSamePart)
Parameters: isIgnorePairsWithinSamePart (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
IsIgnorePairsWithinSameSubassembly¶
-
ClearanceAnalysisBuilder.
IsIgnorePairsWithinSameSubassembly
¶ Returns or sets the setting to determine whether to ignore pairs within same subassembly.
-------------------------------------
Getter Method
Signature
IsIgnorePairsWithinSameSubassembly()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsIgnorePairsWithinSameSubassembly(isIgnorePairsWithinSameSubassembly)
Parameters: isIgnorePairsWithinSameSubassembly (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
IsIgnorePairsWithinSelectedSubassemblies¶
-
ClearanceAnalysisBuilder.
IsIgnorePairsWithinSelectedSubassemblies
¶ Returns or sets the setting to determine whether to ignore pairs within the selected subassemblies.
-------------------------------------
Getter Method
Signature
IsIgnorePairsWithinSelectedSubassemblies()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsIgnorePairsWithinSelectedSubassemblies(isIgnorePairsWithinSelectedSubassemblies)
Parameters: isIgnorePairsWithinSelectedSubassemblies (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Layer¶
-
ClearanceAnalysisBuilder.
Layer
¶ Returns or sets the layer for interference geometry.
-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SaveInterferenceGeometry¶
-
ClearanceAnalysisBuilder.
SaveInterferenceGeometry
¶ Returns or sets the setting to determine if interference geometry should be saved.
-------------------------------------
Getter Method
Signature
SaveInterferenceGeometry()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveInterferenceGeometry(saveInterferenceGeometry)
Parameters: saveInterferenceGeometry (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
TotalCollectionCount¶
-
ClearanceAnalysisBuilder.
TotalCollectionCount
¶ Returns or sets the setting to determine whether one collection or two collections should be used.
-------------------------------------
Getter Method
Signature
TotalCollectionCount()
Returns: Return type: NXOpen.Assemblies.ClearanceAnalysisBuilderNumberOfCollections
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TotalCollectionCount(totalCollectionCount)
Parameters: totalCollectionCount ( NXOpen.Assemblies.ClearanceAnalysisBuilderNumberOfCollections
) –New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
UnitSubassemblies¶
-
ClearanceAnalysisBuilder.
UnitSubassemblies
¶ Returns the selected unit subassemblies.
-------------------------------------
Getter Method
Signature
UnitSubassemblies()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX9.0.0.
License requirements: None.
Method Detail¶
AddException¶
-
ClearanceAnalysisBuilder.
AddException
¶ Add an exception.
Signature
AddException(isExclude, comp1, comp2, text)
Parameters: - isExclude (bool) – exclude or include type of the exception
- comp1 (
NXOpen.DisplayableObject
) – the first object of the pair - comp2 (
NXOpen.DisplayableObject
) – the second object of the pair - text (str) – note for the exception
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
AddObjectClearanceZone¶
-
ClearanceAnalysisBuilder.
AddObjectClearanceZone
¶ Add a Clearance Zone around an object.
Create the expression using
CreateClearanceZoneExpression()
if the Clearance Zone expression naming convention is desired.Signature
AddObjectClearanceZone(object, expression)
Parameters: - object (
NXOpen.DisplayableObject
) – the object - expression (
NXOpen.Expression
) – the expression
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object (
AddPairClearanceZone¶
-
ClearanceAnalysisBuilder.
AddPairClearanceZone
¶ Add a Clearance Zone between a pair of objects.
Create the expression using
CreateClearanceZoneExpression()
if the Clearance Zone expression naming convention is desired.Signature
AddPairClearanceZone(object1, object2, expression)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object - object2 (
NXOpen.DisplayableObject
) – the second object - expression (
NXOpen.Expression
) – the expression
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
CreateClearanceZoneExpression¶
-
ClearanceAnalysisBuilder.
CreateClearanceZoneExpression
¶ Create an expression using the Clearance Zone naming convention.
The expression is intended for use in the following methods:
NXOpen.Assemblies.ClearanceAnalysisBuilder.SetDefaultClearanceZone()
NXOpen.Assemblies.ClearanceAnalysisBuilder.AddPairClearanceZone()
NXOpen.Assemblies.ClearanceAnalysisBuilder.AddObjectClearanceZone()
Signature
CreateClearanceZoneExpression(rhsExpression)
Parameters: rhsExpression (str) – the text for the expression Returns: the new expression Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DeleteException¶
-
ClearanceAnalysisBuilder.
DeleteException
¶ Delete an exception.
Signature
DeleteException(comp1, comp2)
Parameters: - comp1 (
NXOpen.DisplayableObject
) – the first object of the pair - comp2 (
NXOpen.DisplayableObject
) – the second object of the pair
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- comp1 (
DeleteObjectClearanceZone¶
-
ClearanceAnalysisBuilder.
DeleteObjectClearanceZone
¶ Delete an existing Clearance Zone from around an object.
Signature
DeleteObjectClearanceZone(object)
Parameters: object ( NXOpen.DisplayableObject
) – the objectNew in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DeletePairClearanceZone¶
-
ClearanceAnalysisBuilder.
DeletePairClearanceZone
¶ Delete an existing Clearance Zone between the given pair of objects.
Signature
DeletePairClearanceZone(object1, object2)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object - object2 (
NXOpen.DisplayableObject
) – the second object
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
GetDefaultClearanceZone¶
-
ClearanceAnalysisBuilder.
GetDefaultClearanceZone
¶ Get the default Clearance Zone expression.
If there is no expression set previously, a None will be returned.
Signature
GetDefaultClearanceZone()
Returns: the expression Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetIsPairIncluded¶
-
ClearanceAnalysisBuilder.
GetIsPairIncluded
¶ Inquires if an object pair is to be included in the analysis.
Both objects must be solid bodies or facet models that are members of the clearance analysis data set. If the pair is to be analyzed, the includeIt is returned as TRUE. The reason parameter signifies why the pair is included or excluded. The text parameter is only returned for the
NXOpen.Assemblies.ClearanceAnalysisBuilderPairExcludedReason.UserDefined
reason.Signature
GetIsPairIncluded(object1, object2)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object - object2 (
NXOpen.DisplayableObject
) – the second object
Returns: a tuple
Return type: A tuple consisting of (includeIt, reason, text). includeIt is a bool. the flag reason is a
NXOpen.Assemblies.ClearanceAnalysisBuilderPairExcludedReason
. the reason text is a str. the textNew in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
GetObjectClearanceZone¶
-
ClearanceAnalysisBuilder.
GetObjectClearanceZone
¶ Inquire the Clearance Zone assigned to a given object.
The object must be a member of the dataset. The expression, the distance, and the source are the outputs. If no expression has ever been set, the part of the given object is checked for a Clearance Zone expression, if none is found, None will be returned for the expression. Interpret its value as 0.0 (this is the default value). The source parameter tells where the clearance zone comes from.
NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource.Defined
specifies that the object has its own Clearance Zone.NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource.Default
means the default clearance zone is used.Signature
GetObjectClearanceZone(object)
Parameters: object ( NXOpen.DisplayableObject
) – the objectReturns: a tuple Return type: A tuple consisting of (source, expression). source is a NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource
. the source of the clearance zone expression is aNXOpen.Expression
. the expressionNew in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetPairClearanceZone¶
-
ClearanceAnalysisBuilder.
GetPairClearanceZone
¶ Inquire the Clearance Zone for a specific pair of objects.
Both objects must be members of the Clearance Set. The source parameter tells where the clearance zone comes from. The clearance zone could be the greater of the zones from object 1 or 2 (
NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource.Object1
orNXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource.Object2
.NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource.Pair
means this pair has its own explicit clearance zone.NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource.Default
means the default clearance zone is used..Signature
GetPairClearanceZone(object1, object2)
Parameters: - object1 (
NXOpen.DisplayableObject
) – the first object - object2 (
NXOpen.DisplayableObject
) – the second object
Returns: a tuple
Return type: A tuple consisting of (source, expression). source is a
NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource
. the source of the clearance zone expression is aNXOpen.Expression
. the corresponding expressionNew in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- object1 (
SetDefaultClearanceZone¶
-
ClearanceAnalysisBuilder.
SetDefaultClearanceZone
¶ Set the expression as the default Clearance Zone.
Create the expression using
CreateClearanceZoneExpression()
if the Clearance Zone expression naming convention is desired.Signature
SetDefaultClearanceZone(expression)
Parameters: expression ( NXOpen.Expression
) – the expressionNew in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Validate¶
-
ClearanceAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.