WaveQuery Class¶
-
class
NXOpen.Assemblies.
WaveQuery
¶ Bases:
NXOpen.TransientObject
Provides information about the inter-part relations (e.g. WAVE, inter-part expressions) in a NX model.
The returned XML string contains information from parts loaded in the NX session and from published TeamCenter data. The XML must be unmarshaled using the Browser_model_schema.xsd.The XML identifiers are valid for the life of the session and are used in sequent queries.
For the selected parts, the queries return the first level parent (source) and child (target) parts. The object-object relations that comprise a part-part relation are included if the information is available. Each query provides a context for the meaning of a selected part. For example, the work part is the only selected part for GetWorkPartWithPartRelationsXml. However, the method GetPartsInContextAssemblyXml considers all the unique parts in the context assembly to be selected.
Since the queries also return the first level parent and child parents, these non-selected parts could exist only in TeamCenter.
This is an abstract class, and cannot be created.
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
AreAssemblyConstraintsDelayed | Returns true if update of assembly constraints is delayed @return whether constraints are delayed |
Dispose | Free resources associated with the instance. |
GetAllSelectedPartsXml | Gets all the parts in the current selection list in the NX session. |
GetChildPartRelationsXml | Gets the child parts for a given part. |
GetChildRevisionOption | Returns the child revision option @return the child revision option that is currently set |
GetInSessionPartsXml | Gets the parts that are in-session. |
GetInterPartLinksXml | Gets the inter-part links and their sources for a given part. |
GetParentPartRelationsXml | Gets the parent parts for a given part. |
GetPartFeatureDependenciesXml | Gets the feature dependency lists for a fully loaded part. |
GetPartPreview | Gets the part’s preview image. |
GetPartsInContextAssemblyXml | Gets the parts that are in the context assembly. |
GetProductInterfacesXml | Gets the product interfaces and their references for a given part. |
GetReferencesToProductInterfaceXml | Gets a product interface’s referencing objects. |
GetSpecifiedPartRelationsXml | Gets information about the specified parts. |
GetWorkPartWithPartRelationsXml | Gets the current work part. |
HandleApplicationEvents | Provides application (e. |
SetChildRevisionOption | Specifies what child revisions to fetch from Teamcenter |
Method Detail¶
AreAssemblyConstraintsDelayed¶
-
WaveQuery.
AreAssemblyConstraintsDelayed
¶ Returns true if update of assembly constraints is delayed
Signature
AreAssemblyConstraintsDelayed()
Returns: whether constraints are delayed Return type: bool New in version NX7.5.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
Dispose¶
-
WaveQuery.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetAllSelectedPartsXml¶
-
WaveQuery.
GetAllSelectedPartsXml
¶ Gets all the parts in the current selection list in the NX session.
Signature
GetAllSelectedPartsXml(includeOnlyWithLinks)
Parameters: includeOnlyWithLinks (bool) – true if only parts that own inter-part links are returned Returns: the XML Return type: str New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetChildPartRelationsXml¶
-
WaveQuery.
GetChildPartRelationsXml
¶ Gets the child parts for a given part.
The parts are not necessarily fully loaded. The specified part and its children are considered to be “selected” parts.
Signature
GetChildPartRelationsXml(parentPartSpec, parentPartIdentifier, walkAll)
Parameters: - parentPartSpec (str) – the part’s specification
- parentPartIdentifier (int) – part’s in-session identifier
- walkAll (bool) – true if children of all descendants are obtained
Returns: the XML
Return type: str
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetChildRevisionOption¶
-
WaveQuery.
GetChildRevisionOption
¶ Returns the child revision option
Signature
GetChildRevisionOption()
Returns: the child revision option that is currently set Return type: NXOpen.Assemblies.AssembliesChildRevisionOptions
New in version NX8.5.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetInSessionPartsXml¶
-
WaveQuery.
GetInSessionPartsXml
¶ Gets the parts that are in-session.
The parts are not necessarily fully loaded.
Signature
GetInSessionPartsXml(includeOnlyWithLinks)
Parameters: includeOnlyWithLinks (bool) – true if only parts that own inter-part links are returned Returns: the XML Return type: str New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetInterPartLinksXml¶
-
WaveQuery.
GetInterPartLinksXml
¶ Gets the inter-part links and their sources for a given part.
The owning part is the “selected” part.
Signature
GetInterPartLinksXml(partSpec, partIdentifier)
Parameters: - partSpec (str) – the part’s specification
- partIdentifier (int) – part’s in-session identifier
Returns: the XML
Return type: str
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetParentPartRelationsXml¶
-
WaveQuery.
GetParentPartRelationsXml
¶ Gets the parent parts for a given part.
The parts are not necessarily fully loaded. The specified part and its parents are considered to be “selected” parts.
Signature
GetParentPartRelationsXml(childPartSpec, childPartIdentifier, walkAll)
Parameters: - childPartSpec (str) – the part’s specification
- childPartIdentifier (int) – part’s in-session identifier
- walkAll (bool) – true if parents of all ancestors are obtained
Returns: the XML
Return type: str
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetPartFeatureDependenciesXml¶
-
WaveQuery.
GetPartFeatureDependenciesXml
¶ Gets the feature dependency lists for a fully loaded part.
Signature
GetPartFeatureDependenciesXml(partSpec, partIdentifier)
Parameters: - partSpec (str) – the part’s specification
- partIdentifier (int) – part’s in-session identifier
Returns: the XML
Return type: str
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetPartPreview¶
-
WaveQuery.
GetPartPreview
¶ Gets the part’s preview image.
Signature
GetPartPreview(partSpec, partIdentifier)
Parameters: - partSpec (str) – the part’s specification
- partIdentifier (int) – part’s in-session identifier
Returns: a tuple
Return type: A tuple consisting of (height, width, pixels). height is a int. height of preview image width is a int. width of preview image pixels is a list of int. the pixels
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetPartsInContextAssemblyXml¶
-
WaveQuery.
GetPartsInContextAssemblyXml
¶ Gets the parts that are in the context assembly.
The parts are not necessarily fully loaded.
Signature
GetPartsInContextAssemblyXml(includeOnlyWithLinks)
Parameters: includeOnlyWithLinks (bool) – true if only parts that own inter-part links are returned Returns: the XML Return type: str New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetProductInterfacesXml¶
-
WaveQuery.
GetProductInterfacesXml
¶ Gets the product interfaces and their references for a given part.
The owning part is the “selected” part.
Signature
GetProductInterfacesXml(partSpec, partIdentifier)
Parameters: - partSpec (str) – the part’s specification
- partIdentifier (int) – part’s in-session identifier
Returns: the XML
Return type: str
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetReferencesToProductInterfaceXml¶
-
WaveQuery.
GetReferencesToProductInterfaceXml
¶ Gets a product interface’s referencing objects.
The owning part is the “selected” part.
Signature
GetReferencesToProductInterfaceXml(owningPartSpec, owningPartIdentifier, prodintHandle, prodintIdentifier)
Parameters: - owningPartSpec (str) – the owning part’s specification
- owningPartIdentifier (int) – owning part’s in-session identifier
- prodintHandle (str) – the product interface’s handle
- prodintIdentifier (int) – product interface’s in-session identifier
Returns: the XML
Return type: str
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetSpecifiedPartRelationsXml¶
-
WaveQuery.
GetSpecifiedPartRelationsXml
¶ Gets information about the specified parts.
The parts are not necessarily fully loaded.
Signature
GetSpecifiedPartRelationsXml(partSpecs, partIdentifiers, includeOnlyWithLinks)
Parameters: - partSpecs (list of str) – the NX part specifications
- partIdentifiers (list of int) – the NX part identifiers
- includeOnlyWithLinks (bool) – true if only parts that own inter-part links are returned
Returns: the XML
Return type: str
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
GetWorkPartWithPartRelationsXml¶
-
WaveQuery.
GetWorkPartWithPartRelationsXml
¶ Gets the current work part.
Signature
GetWorkPartWithPartRelationsXml()
Returns: the XML Return type: str New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
HandleApplicationEvents¶
-
WaveQuery.
HandleApplicationEvents
¶ Provides application (e.
g. the graphical browser) event processing by NX. Some events refer to part level actions while others refer to part object level actions.
Signature
HandleApplicationEvents(eventType, eventDescription, entitySpecs, entityIdentifiers)
Parameters: - eventType (
NXOpen.Assemblies.AssembliesEventTypes
) – type of event for processing - eventDescription (str) – textual description of the event for reporting
- entitySpecs (list of str) – the NX part specifications or the handles of the objects
- entityIdentifiers (list of int) – the NX part or object identifiers
Returns: the return status of this method
Return type: int
New in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
- eventType (
SetChildRevisionOption¶
-
WaveQuery.
SetChildRevisionOption
¶ Specifies what child revisions to fetch from Teamcenter
Signature
SetChildRevisionOption(optionType)
Parameters: optionType ( NXOpen.Assemblies.AssembliesChildRevisionOptions
) – what child revisions to fetch from TeamcenterNew in version NX8.5.0.
License requirements: wave (“WAVE FUNCTIONALITY”)