Order Class¶
-
class
NXOpen.Assemblies.
Order
¶ Bases:
NXOpen.NXObject
Represents base class for all Order classes.
It is an abstract class and cannot be instantiated on its own. All Order classes should inherit from this class. This is an abstract class, and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OrderState | Returns the state of NXOpen.Assemblies.Order . |
OrderType | Returns the type of NXOpen.Assemblies.Order . |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Activate | Applies this order |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
Delete | Deletes an order |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetChildrenOrder | Returns immediate children of input NXOpen.Assemblies.Component as they are ordered in this NXOpen.Assemblies.ComponentOrder |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetReversed | Gets the reverse state of the NXOpen.Assemblies.Order @return True if order is reversed else False |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
IsActive | Returns true if this order is the active order in owning NXOpen.Assemblies.ComponentAssembly > @return True if the current order is active |
Prints a representation of this object to the system log file. | |
Save | Saves an order |
SaveAs | Creates a copy of the order, and gives the copy a new name. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetReversed | Sets the reverse state of the NXOpen.Assemblies.Order |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
OrderState Enumeration | Represents whether an order is saved or not |
OrderType Enumeration | Represents the type of an order |
Property Detail¶
IsOccurrence¶
-
Order.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Order.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Order.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OrderState¶
-
Order.
OrderState
¶ Returns the state of
NXOpen.Assemblies.Order
.An order can be in one of the
NXOpen.Assemblies.OrderState
.-------------------------------------
Getter Method
Signature
OrderState()
Returns: Return type: NXOpen.Assemblies.OrderState
New in version NX9.0.0.
License requirements: None.
OrderType¶
-
Order.
OrderType
¶ Returns the type of
NXOpen.Assemblies.Order
.An order can be of
NXOpen.Assemblies.OrderType
-------------------------------------
Getter Method
Signature
OrderType()
Returns: Return type: NXOpen.Assemblies.OrderType
New in version NX9.0.0.
License requirements: None.
OwningComponent¶
-
Order.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Order.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Order.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
Activate¶
-
Order.
Activate
¶ Applies this order
Signature
Activate()
New in version NX9.0.0.
License requirements: None.
Delete¶
-
Order.
Delete
¶ Deletes an order
Signature
Delete()
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
FindObject¶
-
Order.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetChildrenOrder¶
-
Order.
GetChildrenOrder
¶ Returns immediate children of input
NXOpen.Assemblies.Component
as they are ordered in thisNXOpen.Assemblies.ComponentOrder
Signature
GetChildrenOrder(parent)
Parameters: parent ( NXOpen.Assemblies.Component
) –Returns: Returns children in order Return type: list of NXOpen.Assemblies.Component
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Assemblies.ComponentOrder.AskChildrenOrder()
instead to get children order in thisNXOpen.Assemblies.ComponentOrder
.License requirements: None.
GetReversed¶
-
Order.
GetReversed
¶ Gets the reverse state of the
NXOpen.Assemblies.Order
Signature
GetReversed()
Returns: True if order is reversed else False Return type: bool New in version NX9.0.0.
License requirements: None.
IsActive¶
-
Order.
IsActive
¶ Returns true if this order is the active order in owning
NXOpen.Assemblies.ComponentAssembly
>Signature
IsActive()
Returns: True if the current order is active Return type: bool New in version NX10.0.3.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Print¶
-
Order.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
Save¶
-
Order.
Save
¶ Saves an order
Signature
Save()
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SaveAs¶
-
Order.
SaveAs
¶ Creates a copy of the order, and gives the copy a new name.
Each
NXOpen.Assemblies.ComponentAssembly
contains a set of system defined orders, which could be queried usingNXOpen.Assemblies.ComponentAssembly.GetComponentOrders()
method. A newNXOpen.Assemblies.OrderType.UserDefinedComponent
order can only be created using this method.Signature
SaveAs(newName)
Parameters: newName (str) – Returns: The new Order Return type: NXOpen.Assemblies.Order
New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SetName¶
-
Order.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetReversed¶
-
Order.
SetReversed
¶ Sets the reverse state of the
NXOpen.Assemblies.Order
Signature
SetReversed(isReversed)
Parameters: isReversed (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)