AssembliesGeneralPropertiesBuilderQuantityOptions Enumeration¶
NXOpen.Assemblies.AssembliesGeneralPropertiesBuilder.QuantityOptions is an alias for NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderQuantityOptions
-
class
NXOpen.Assemblies.
AssembliesGeneralPropertiesBuilderQuantityOptions
¶ Bases:
object
Options for assigning the quantity on the components
Enum Members
Enum Member Enum Member Description Number Use either the integer or real value to set the quantityAsRequired Sets the as-required quantity on this component.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-