DesignElementBuilderPositioningOption Enumeration¶
NXOpen.Assemblies.DesignElementBuilder.PositioningOption is an alias for NXOpen.Assemblies.DesignElementBuilderPositioningOption
-
class
NXOpen.Assemblies.
DesignElementBuilderPositioningOption
¶ Bases:
object
Represents the positioning option of a design element.
Enum Members
Applicable only if the edit action type is set to
DesignElementBuilderEditActionType.Category
““AsSpecified”, ” Applies the specified position on the design elements”-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-