DesignElementBuilderReferenceSetType Enumeration¶
NXOpen.Assemblies.DesignElementBuilder.ReferenceSetType is an alias for NXOpen.Assemblies.DesignElementBuilderReferenceSetType
-
class
NXOpen.Assemblies.
DesignElementBuilderReferenceSetType
¶ Bases:
object
Represents the reference set of a design element
Enum Members
Enum Member Enum Member Description Model ModelEntirePart Entire partAsSpecified As specified reference set-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-