AssembliesGeneralPropertiesBuilderLayerOptions Enumeration¶
NXOpen.Assemblies.AssembliesGeneralPropertiesBuilder.LayerOptions is an alias for NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderLayerOptions
-
class
NXOpen.Assemblies.
AssembliesGeneralPropertiesBuilderLayerOptions
¶ Bases:
object
Layer options for the components
Enum Members
Enum Member Enum Member Description OriginalLayer Objects will be placed on original layerSpecifiedLayer Objects will be placed on a user specified layerMixed Objects are on different layers and will not be changed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-