NXOpen.Features.ShipDesign.AlongGuideCut |
Represents a corner cut feature |
NXOpen.Features.ShipDesign.AlongGuideCutBuilder |
Represents a NXOpen.Features.ShipDesign.AlongGuideCut builder |
NXOpen.Features.ShipDesign.AnchorPoint |
Represents a NXOpen.Features.ShipDesign.AnchorPoint builder. |
NXOpen.Features.ShipDesign.AnchorPointList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.BuiltUpBlockBuilder |
Represents a NXOpen.Features.ShipDesign.BuiltUpBlockBuilder |
NXOpen.Features.ShipDesign.BuiltUpManModeBuilder |
This class allows you to set the NX Ship BuiltUp Profile Manufacturing Mode for one or more components. |
NXOpen.Features.ShipDesign.BuiltUpOffsetBuilder |
Represents a NXOpen.Features.ShipDesign.BuiltUpOffsetBuilder . |
NXOpen.Features.ShipDesign.BulkHeadListItemBuilder |
Represents a NXOpen.Features.ShipDesign.BulkHeadListItemBuilder |
NXOpen.Features.ShipDesign.BulkHeadListItemBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.BulkHeads |
Represents a bulk head feature |
NXOpen.Features.ShipDesign.BulkHeadsBuilder |
Represents a NXOpen.Features.ShipDesign.BulkHeads builder |
NXOpen.Features.ShipDesign.CompareModeBuilder |
This class is used to compare between the two Shipbuilding modes of Design and Manufacturing. |
NXOpen.Features.ShipDesign.ConceptFromSpreadsheet |
Represents a concept from spreadsheet feature |
NXOpen.Features.ShipDesign.ConceptFromSpreadsheetBuilder |
Represents a NXOpen.Features.ShipDesign.ConceptFromSpreadsheet builder |
NXOpen.Features.ShipDesign.CopyObjectsBuilder |
Represents a NXOpen.Features.ShipDesign.CopyObjectsBuilder It is used in Ship Building Application. |
NXOpen.Features.ShipDesign.CopyPasteNewBuilder |
Represents a NXOpen.Features.ShipDesign.CopyPasteNewBuilder It is used in Ship Building Application. |
NXOpen.Features.ShipDesign.CornerCut |
Represents a corner cut feature |
NXOpen.Features.ShipDesign.CornerCutBuilder |
Builder used to create or edit a NXOpen.Features.ShipDesign.CornerCut feature. |
NXOpen.Features.ShipDesign.CornerCutListItemBuilder |
Used to supply the list of corner cut locations and seam curves to the NXOpen.Features.ShipDesign.CornerCutBuilder |
NXOpen.Features.ShipDesign.CornerCutListItemBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.CustomBracket |
Represents a custom bracket feature |
NXOpen.Features.ShipDesign.CustomBracketBuilder |
Represents a NXOpen.Features.ShipDesign.CustomBracket builder |
NXOpen.Features.ShipDesign.Cutout2 |
Represents a cutout2 feature |
NXOpen.Features.ShipDesign.Cutout2Builder |
Represents a NXOpen.Features.ShipDesign.Cutout2 builder |
NXOpen.Features.ShipDesign.CuttingSideFacesBuilder |
Used to create a NXOpen.Features.ShipDesign.CuttingSideFacesBuilder which is used to attribute the cutting side, and opposing cutting side, faces on the plate bodies. |
NXOpen.Features.ShipDesign.Deck |
Represents a Deck feature in Basic Design. |
NXOpen.Features.ShipDesign.DeckBuilder |
This class is used to create or edit a NXOpen.Features.ShipDesign.Deck feature. |
NXOpen.Features.ShipDesign.DeckListItemBuilder |
Represents a DeckListItemBuilder. |
NXOpen.Features.ShipDesign.DeckListItemBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.Decks |
Represents a decks feature |
NXOpen.Features.ShipDesign.DecksBuilder |
Represents a NXOpen.Features.ShipDesign.Decks builder. |
NXOpen.Features.ShipDesign.DeleteSeamBuilder |
Used to create a NXOpen.Features.ShipDesign.DeleteSeamBuilder which is used to delete the seams from the ship structural components. |
NXOpen.Features.ShipDesign.DisplaySolidBuilder |
This class is used to identify ship structure that is to have a temporary solid display built for it. |
NXOpen.Features.ShipDesign.DrawingAnnotationBuilder |
This builder allows you to define the drawing annotation information. |
NXOpen.Features.ShipDesign.DrawingTemplateBuilder |
Represents a drawing template selection block |
NXOpen.Features.ShipDesign.DvToMvMapping |
Represents a plate feature |
NXOpen.Features.ShipDesign.DvToMvMappingBuilder |
Represents a NXOpen.Features.ShipDesign.DvToMvMapping builder. |
NXOpen.Features.ShipDesign.EdgeCut |
Represents a edge cut feature |
NXOpen.Features.ShipDesign.EdgeCutBuilder |
Represents a NXOpen.Features.ShipDesign.EdgeCut builder. |
NXOpen.Features.ShipDesign.EdgeReinforcement |
Represents a edge reinforcement feature. |
NXOpen.Features.ShipDesign.EdgeReinforcementBuilder |
Represents a NXOpen.Features.ShipDesign.EdgeReinforcement builder which is used to create or edit a edge reinforcement system feature. |
NXOpen.Features.ShipDesign.EditContextAttributesBuilder |
Represents the class Features. |
NXOpen.Features.ShipDesign.EditStockBuilder |
Used to create a NXOpen.Features.ShipDesign.EditStockBuilder which is used to change the stock information on the basic design features. |
NXOpen.Features.ShipDesign.EditWeldingBuilder |
Used to create a NXOpen.Features.ShipDesign.EditWeldingBuilder which is used to change the welding characteristics on the seams in the plate systems. |
NXOpen.Features.ShipDesign.EndCut |
Represents an end cut feature |
NXOpen.Features.ShipDesign.EndCutBuilder |
Represents a NXOpen.Features.ShipDesign.EndCut builder. |
NXOpen.Features.ShipDesign.ExamineSteelFeatureBuilder |
Represents the examine steel feature builder to examine steel feature. |
NXOpen.Features.ShipDesign.ExcessMaterial |
Represents a excess material feature |
NXOpen.Features.ShipDesign.ExcessMaterialBuilder |
Represents a NXOpen.Features.ShipDesign.ExcessMaterial builder. |
NXOpen.Features.ShipDesign.ExpansionDrawing |
Represents a expansion drawing feature. |
NXOpen.Features.ShipDesign.ExpansionDrawingBuilder |
Represents a NXOpen.Features.ShipDesign.ExpansionDrawingBuilder . |
NXOpen.Features.ShipDesign.FeatureParmsBuilder |
This class is used to create or edit the information shared among all Ship Design features. |
NXOpen.Features.ShipDesign.FeaturesBatchOperationBuilder |
Use this to cycle through the assembly components and perform the operation globally on the specified feature type. |
NXOpen.Features.ShipDesign.FeaturesToTagBuilder |
This class is used to add an attribute to profile features that have been modified by the user to display a ‘Metal to Metal’ design ‘feature’. |
NXOpen.Features.ShipDesign.FilterBuilder |
A builder that allows the user to define common properties of ship objects and then add objects of similar properties to the select object list. |
NXOpen.Features.ShipDesign.FrameBarOut |
Represents a FrameBarOut |
NXOpen.Features.ShipDesign.FrameBarOutBuilder |
Represents a NXOpen.Features.ShipDesign.FrameBarOut builder. |
NXOpen.Features.ShipDesign.GenericPlateSystem |
Represents a Generic Plate System feature. |
NXOpen.Features.ShipDesign.GenericPlateSystemBuilder |
This class is used to create or edit a NXOpen.Features.ShipDesign.GenericPlateSystem feature. |
NXOpen.Features.ShipDesign.Hull |
Represents a Hull feature. |
NXOpen.Features.ShipDesign.HullBuilder |
This class is used to create or edit a NXOpen.Features.ShipDesign.Hull feature. |
NXOpen.Features.ShipDesign.InsertFramesBuilder |
Represents a NXOpen.Features.ShipDesign.InsertFramesBuilder builder |
NXOpen.Features.ShipDesign.InsertSheetBody |
Represents a insert sheet body feature |
NXOpen.Features.ShipDesign.InsertSheetBodyBuilder |
Represents a NXOpen.Features.ShipDesign.InsertSheetBody builder |
NXOpen.Features.ShipDesign.InverseBendingLines |
Represents a inverse bending lines feature |
NXOpen.Features.ShipDesign.InverseBendingLinesBuilder |
Used to create or edit a NXOpen.Features.ShipDesign.InverseBendingLines feature. |
NXOpen.Features.ShipDesign.ItFrameListItemBuilder |
Represents a NXOpen.Features.ShipDesign.ItFrameListItemBuilder |
NXOpen.Features.ShipDesign.ItFrameListItemBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.ItFrames |
Represents a Inter Transverse Frame feature |
NXOpen.Features.ShipDesign.ItFramesBuilder |
Represents a NXOpen.Features.ShipDesign.ItFrames builder |
NXOpen.Features.ShipDesign.KnuckledProfiles |
Represents a knuckled profiles manufacturing preparation feature |
NXOpen.Features.ShipDesign.KnuckledProfilesBuilder |
Represents a NXOpen.Features.ShipDesign.KnuckledProfiles builder |
NXOpen.Features.ShipDesign.LongitudinalBulkhead |
Represents a Longitudinal Bulkhead feature. |
NXOpen.Features.ShipDesign.LongitudinalBulkheadBuilder |
This class is used to create or edit a NXOpen.Features.ShipDesign.LongitudinalBulkhead feature. |
NXOpen.Features.ShipDesign.MainDimensions |
Represents a main dimensions feature |
NXOpen.Features.ShipDesign.MainDimensionsBuilder |
Represents a NXOpen.Features.ShipDesign.MainDimensions builder. |
NXOpen.Features.ShipDesign.ManufacturingDataBuilder |
This class is used to generate Manufacturing data. |
NXOpen.Features.ShipDesign.ManufacturingOut |
Represents a ManufacturingOut |
NXOpen.Features.ShipDesign.ManufacturingOutBuilder |
Represents a NXOpen.Features.ShipDesign.ManufacturingOut builder |
NXOpen.Features.ShipDesign.ManufacturingPreparation |
Represents a manufacturing preparation feature |
NXOpen.Features.ShipDesign.ManufacturingPreparationBuilder |
This builder is used to adds attributes to the part and body identifying manufacturing related data. |
NXOpen.Features.ShipDesign.ManufacturingStockBuilder |
Represents a NXOpen.Features.ShipDesign.ManufacturingStockBuilder builder. |
NXOpen.Features.ShipDesign.MarkingLine |
Represents a marking line feature. |
NXOpen.Features.ShipDesign.MarkingLineBuilder |
Represents a MarkingLine Feature builder |
NXOpen.Features.ShipDesign.MarkingLineDesign |
Represents a marking line feature. |
NXOpen.Features.ShipDesign.MarkingLineDesignBuilder |
Represents a new MarkingLine Feature builder. |
NXOpen.Features.ShipDesign.MaterialAllowanceBuilder |
Represents the material allowance feature builder to examine steel feature. |
NXOpen.Features.ShipDesign.MaterialEstimationBuilder |
Represents the class Features. |
NXOpen.Features.ShipDesign.MirrorShipStructureBuilder |
Copy the selected parts (components) about the Mirror Plane with full model history and feature data. |
NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilder |
This class defines the method of angle definition used in the definition of the region’s orientation. |
NXOpen.Features.ShipDesign.OrientationDefinition |
Represents a Orientation SubObject. |
NXOpen.Features.ShipDesign.OrientationDefinitionBuilder |
This class defines the top level object for use in definining the orientation of stiffeners and edge reinforcements. |
NXOpen.Features.ShipDesign.OrientationPointMethodsBuilder |
This class is used to define the boundary of the regions when definining the orientation of a profile. |
NXOpen.Features.ShipDesign.OrientationRegionItemBuilder |
This class defines each region of the orientation. |
NXOpen.Features.ShipDesign.OrientationRegionItemBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.PenetrationAssociationBuilder |
Represents a NXOpen.Features.ShipDesign.PenetrationAssociationBuilder builder |
NXOpen.Features.ShipDesign.PenetrationAttachment |
Represents the Penetration Attachment object. |
NXOpen.Features.ShipDesign.PenetrationCutoutBuilder |
Represents a NXOpen.Features.ShipDesign.PenetrationRequest builder |
NXOpen.Features.ShipDesign.PenetrationFolder |
Represents the Penetration Folder object. |
NXOpen.Features.ShipDesign.PenetrationList |
Represents the Penetration List object. |
NXOpen.Features.ShipDesign.PenetrationManager |
Contains the collection objects for creating and iterating over Penetration Request Properties objects. |
NXOpen.Features.ShipDesign.PenetrationRequest |
Represents the Penetration Request object. |
NXOpen.Features.ShipDesign.PenetrationRequestBuilder |
Represents a NXOpen.Features.ShipDesign.PenetrationRequest builder |
NXOpen.Features.ShipDesign.PenetrationRequestCollection |
Represents a NXOpen.Mechatronics.FunctionObjectCollection |
NXOpen.Features.ShipDesign.PenetrationRequestForCutoutBuilder |
Represents a Features.ShipDesign.PenetrationRequest builder |
NXOpen.Features.ShipDesign.PenetrationReviewRequestBuilder |
Represents a Features.ShipDesign.PenetrationRequest builder |
NXOpen.Features.ShipDesign.PenetrationSite |
Represents the Penetration Site object. |
NXOpen.Features.ShipDesign.PenetrationUtils |
Contains various penetration utility methods |
NXOpen.Features.ShipDesign.Pillar |
Represents a Pillar feature |
NXOpen.Features.ShipDesign.PillarBuilder |
Represents a NXOpen.Features.ShipDesign.Pillar builder |
NXOpen.Features.ShipDesign.PillarSystem |
Represents a pillar system feature. |
NXOpen.Features.ShipDesign.PillarSystemBuilder |
Represents a NXOpen.Features.ShipDesign.PillarSystem builder which is used to create or edit a pillar system feature. |
NXOpen.Features.ShipDesign.PinJig |
Represents a Pinjig feature |
NXOpen.Features.ShipDesign.PinJigBuilder |
Represents a NXOpen.Features.ShipDesign.PinJig builder |
NXOpen.Features.ShipDesign.PlaneListBuilder |
This class is used to place a plane into a list. |
NXOpen.Features.ShipDesign.PlaneListBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.PlanePairBuilder |
This class is used to define a pair of planes in a list. |
NXOpen.Features.ShipDesign.Plate |
Represents a plate feature |
NXOpen.Features.ShipDesign.PlateBuilder |
Represents a NXOpen.Features.ShipDesign.Plate builder. |
NXOpen.Features.ShipDesign.PlateChamfer |
Represents a plate chamfer feature |
NXOpen.Features.ShipDesign.PlateChamferBuilder |
Represents a NXOpen.Features.ShipDesign.PlateChamfer builder. |
NXOpen.Features.ShipDesign.PlatePreparation |
Represents a ship plate preparation feature |
NXOpen.Features.ShipDesign.PlatePreparationBuilder |
Used to create or edit a NXOpen.Features.ShipDesign.PlatePreparation feature. |
NXOpen.Features.ShipDesign.PlateStockBuilder |
This builder allows you to define the stock information for plate system features in ship design. |
NXOpen.Features.ShipDesign.PlateSystem |
Represents a Plate System feature. |
NXOpen.Features.ShipDesign.PlateSystemBuilder |
This class is used to create or edit the information shared between all the Basic Design plate system features in the Ship Design application. |
NXOpen.Features.ShipDesign.PointPairBuilder |
This class is used to define a pair of points in a list. |
NXOpen.Features.ShipDesign.Profile |
Represents a profile feature |
NXOpen.Features.ShipDesign.ProfileBuilder |
Represents a NXOpen.Features.ShipDesign.Profile builder |
NXOpen.Features.ShipDesign.ProfileCutout |
Represents a profile cutout feature for NX8. |
NXOpen.Features.ShipDesign.ProfileCutoutBuilder |
Represents a NXOpen.Features.ShipDesign.ProfileCutout builder |
NXOpen.Features.ShipDesign.ProfileList |
Represents a profile list feature |
NXOpen.Features.ShipDesign.ProfileListBuilder |
Represents a NXOpen.Features.ShipDesign.ProfileList builder |
NXOpen.Features.ShipDesign.ProfileSystem |
Represents a profile system feature. |
NXOpen.Features.ShipDesign.ProfileSystemBuilder |
This class is used to create or edit the information shared between all the Basic Design profile system features in the Ship Design application. |
NXOpen.Features.ShipDesign.ProfileTransition |
Represents a profile transition feature |
NXOpen.Features.ShipDesign.ProfileTransitionBuilder |
Builder used to create or edit a NXOpen.Features.ShipDesign.ProfileTransition feature. |
NXOpen.Features.ShipDesign.QualifySketchBuilder |
Represents a NXOpen.Features.ShipDesign.QualifySketchBuilder builder. |
NXOpen.Features.ShipDesign.ReadDataSetBuilder |
This class will read a data set file from Team Center |
NXOpen.Features.ShipDesign.RebaseBuilder |
This class is used to synchronize the end cuts from the ones in mfg group to design group. |
NXOpen.Features.ShipDesign.ReferenceLine |
Represents a reference line feature. |
NXOpen.Features.ShipDesign.ReferenceLineBuilder |
Represents a NXOpen.Features.ShipDesign.ReferenceLine builder. |
NXOpen.Features.ShipDesign.RemoveSplitBuilder |
Represents a NXOpen.Features.ShipDesign.RemoveSplitBuilder . |
NXOpen.Features.ShipDesign.ReverseSplitBuilder |
This class is used to provide the capability to reverse the split interaction between ship structures. |
NXOpen.Features.ShipDesign.RollingLine |
Represents a rolling line feature. |
NXOpen.Features.ShipDesign.RollingLineBuilder |
Represents a NXOpen.Features.ShipDesign.RollingLine builder. |
NXOpen.Features.ShipDesign.Seam |
Represents a ship design seam feature. |
NXOpen.Features.ShipDesign.SeamBlockBuilder |
Represents a NXOpen.Features.ShipDesign.SeamBlockBuilder |
NXOpen.Features.ShipDesign.SeamBlockBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.SeamBuilder |
A NXOpen.Features.ShipDesign.SeamBuilder used to create or edit a ship design NXOpen.Features.ShipDesign.Seam feature. |
NXOpen.Features.ShipDesign.SectionDrawingBuilder |
This builder allows you to define the section drawing information. |
NXOpen.Features.ShipDesign.SectionViewBuilder |
This builder allows you to define the section view information for ship drawing. |
NXOpen.Features.ShipDesign.SectionViewBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.SetModeBuilder |
This class is used to set the mode to design or manufacturing. |
NXOpen.Features.ShipDesign.ShellExpansion |
Represents a shell expansion feature |
NXOpen.Features.ShipDesign.ShellExpansionBuilder |
Represents a NXOpen.Features.ShipDesign.ShellExpansion builder |
NXOpen.Features.ShipDesign.ShellTemplate |
Represents a shell template feature. |
NXOpen.Features.ShipDesign.ShellTemplateBuilder |
Used to edit or create a NXOpen.Features.ShipDesign.ShellTemplate feature. |
NXOpen.Features.ShipDesign.ShipAttributeHolder |
Represents a NXOpen.Features.ShipDesign.ShipAttributeHolder builder |
NXOpen.Features.ShipDesign.ShipContainerBuilder |
This class is used to specify the “container” part for the Ship Structures application, i. |
NXOpen.Features.ShipDesign.ShipCoordinates |
Represents a ship coordinates feature |
NXOpen.Features.ShipDesign.ShipCoordinatesBuilder |
Represents a NXOpen.Features.ShipDesign.ShipCoordinates builder |
NXOpen.Features.ShipDesign.ShipCutout |
Represents a ship cutout feature |
NXOpen.Features.ShipDesign.ShipCutoutBuilder |
Represents a NXOpen.Features.ShipDesign.ShipCutout builder |
NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilder |
Represents a NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilder which is used to change default object display settings for ship structures. |
NXOpen.Features.ShipDesign.ShipDesignVersionUpBuilder |
Represents a NXOpen.Features.ShipDesign.ShipDesignVersionUpBuilder builder. |
NXOpen.Features.ShipDesign.ShipEndCut |
Represents a ship end cut feature |
NXOpen.Features.ShipDesign.ShipEndCutBuilder |
Represents a NXOpen.Features.ShipDesign.ShipEndCut builder |
NXOpen.Features.ShipDesign.ShipFeatureConverter |
This class is used to convert/upgrade legacy Ship Design features. |
NXOpen.Features.ShipDesign.ShipFlatPattern |
Represents a ship flat pattern feature |
NXOpen.Features.ShipDesign.ShipFlatPatternBuilder |
Represents a NXOpen.Features.ShipDesign.ShipFlatPattern builder |
NXOpen.Features.ShipDesign.ShipIntersections |
Represents a ship intersection feature |
NXOpen.Features.ShipDesign.ShipIntersectionsBuilder |
Represents a NXOpen.Features.ShipDesign.ShipIntersections builder |
NXOpen.Features.ShipDesign.ShipNameFieldBuilder |
A field, combined with other fields, to generate a name for a Ship Basic Design Object such as a Deck. |
NXOpen.Features.ShipDesign.ShipNamesBuilder |
This class provides the mechanism for defining the names of Basic Design objects such as Decks, Bulkheads, Stiffener Systems, etc. |
NXOpen.Features.ShipDesign.ShipNamesBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.ShipNamesListBuilder |
This class provides a list of :py:class:`NXOpen.Features.ShipDesign.ShipNamesBuilder`objects. |
NXOpen.Features.ShipDesign.ShipPreparationBuilder |
Creates a builder used to prepare basic design data for meshing. |
NXOpen.Features.ShipDesign.ShipProfileCutout |
Represents a profile cutout feature for NX75 using sketch expression modifier block. |
NXOpen.Features.ShipDesign.ShipProfileCutoutBuilder |
Represents a NXOpen.Features.ShipDesign.ProfileCutout builder for editing legacy(NX75) profile cutout feature. |
NXOpen.Features.ShipDesign.ShipSection |
Represents a ship section feature |
NXOpen.Features.ShipDesign.ShipSectionBuilder |
Represents a NXOpen.Features.ShipDesign.ShipSection builder |
NXOpen.Features.ShipDesign.ShipTrimBody |
Represents a ship trim body feature |
NXOpen.Features.ShipDesign.ShipTrimBodyBuilder |
Represents a NXOpen.Features.ShipDesign.ShipTrimBodyBuilder . |
NXOpen.Features.ShipDesign.SmartRule |
Represents a smart rule feature. |
NXOpen.Features.ShipDesign.SmartRuleBuilder |
Represents a NXOpen.Features.ShipDesign.SmartRule builder |
NXOpen.Features.ShipDesign.SplitProfilePlateBuilder |
Represents a NXOpen.Features.ShipDesign.SplitProfilePlateBuilder . |
NXOpen.Features.ShipDesign.SplitStandardPart |
Represents a split standard part feature. |
NXOpen.Features.ShipDesign.SplitStandardPartBuilder |
Represents a NXOpen.Features.ShipDesign.SplitStandardPartBuilder . |
NXOpen.Features.ShipDesign.StandardPart |
Represents a standard part feature. |
NXOpen.Features.ShipDesign.StandardPartFrameworkBuilder |
Represents the standard part framework builder to add or edit ship standard part. |
NXOpen.Features.ShipDesign.StandardPartItemBuilder |
Represents the ship standard part item builder. |
NXOpen.Features.ShipDesign.StandardPartItemBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.StandardPartSCAssist |
Represents |
NXOpen.Features.ShipDesign.SteelCollarPlate |
Represents a collar plate steel feature |
NXOpen.Features.ShipDesign.SteelCollarPlateBuilder |
Represents a NXOpen.Features.ShipDesign.SteelCollarPlate builder |
NXOpen.Features.ShipDesign.SteelDistribution |
Represents a steel distribution feature |
NXOpen.Features.ShipDesign.SteelDistributionBuilder |
Represents a NXOpen.Features.ShipDesign.SteelDistribution builder |
NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder |
Represents a NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder builder. |
NXOpen.Features.ShipDesign.SteelInsulation |
Represents a steel insulation feature. |
NXOpen.Features.ShipDesign.SteelInsulationBoundaryBuilder |
Represents a Steel Insulation Boundary builder. |
NXOpen.Features.ShipDesign.SteelInsulationBoundaryBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.SteelInsulationBuilder |
Represents a builder that is used to create or edit a NXOpen.Features.ShipDesign.SteelInsulation feature. |
NXOpen.Features.ShipDesign.SteelSupport |
Represents a steel support feature |
NXOpen.Features.ShipDesign.SteelSupportBuilder |
Represents a NXOpen.Features.ShipDesign.SteelSupport builder |
NXOpen.Features.ShipDesign.SteelVentHoles |
Represents a ship vent holes feature |
NXOpen.Features.ShipDesign.SteelVentHolesBuilder |
Represents a NXOpen.Features.ShipDesign.SteelVentHoles builder |
NXOpen.Features.ShipDesign.Stiffener |
Represents a stiffener feature |
NXOpen.Features.ShipDesign.StiffenerBuilder |
Represents a NXOpen.Features.ShipDesign.Stiffener builder |
NXOpen.Features.ShipDesign.StiffenerBySupportPathBuilder |
This class defines the builder to collect stiffener by support path data for Stiffener feature. |
NXOpen.Features.ShipDesign.StiffenerLimitBuilder |
This class defines the path limit method used by a Stiffener or Edge Reinforcement feature. |
NXOpen.Features.ShipDesign.StiffenerStockBuilder |
This class defines the Profile or Plate stock for a Stiffener or Edge Reinforcement feature. |
NXOpen.Features.ShipDesign.StiffenerSystem |
Represents a stiffener system feature. |
NXOpen.Features.ShipDesign.StiffenerSystemBuilder |
This class is used to create or edit a NXOpen.Features.ShipDesign.StiffenerSystem feature. |
NXOpen.Features.ShipDesign.SubSystemBuilder |
This class is used to edit the Sub System Definition of a NXOpen.Features.ShipDesign.SubSystems feature. |
NXOpen.Features.ShipDesign.SubSystemBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.SubSystems |
Represents a sub systems feature. |
NXOpen.Features.ShipDesign.SubSystemsBuilder |
This class is used to edit a NXOpen.Features.ShipDesign.SubSystems feature. |
NXOpen.Features.ShipDesign.SynchronizeDesignViewBuilder |
This class is used to synchronize body features from design view to manufacturing view. |
NXOpen.Features.ShipDesign.ThicknessDirectionBuilder |
This class allows you to define the thickness direction for plate system features in Ship Basic Design and and for grid planes in Ship Concept Design. |
NXOpen.Features.ShipDesign.TraceLines |
Represents a trace lines feature |
NXOpen.Features.ShipDesign.TraceLinesBuilder |
Represents a NXOpen.Features.ShipDesign.TraceLines builder |
NXOpen.Features.ShipDesign.TransFrame |
Represents a TransVerse Frame feature |
NXOpen.Features.ShipDesign.TransFrameBuilder |
Represents a NXOpen.Features.ShipDesign.TransFrame builder |
NXOpen.Features.ShipDesign.TransFrameListItemBuilder |
Represents a NXOpen.Features.ShipDesign.TransFrameListItemBuilder |
NXOpen.Features.ShipDesign.TransFrameListItemBuilderList |
Represents a list of objects. |
NXOpen.Features.ShipDesign.TransitionBuilder |
This is to create a NXOpen.Features.ShipDesign.TransitionBuilder which is used to create Detail Design elements from Basic Design elements. |
NXOpen.Features.ShipDesign.TransverseBulkhead |
Represents a Transverse Bulkhead feature. |
NXOpen.Features.ShipDesign.TransverseBulkheadBuilder |
This class is used to create or edit a NXOpen.Features.ShipDesign.TransverseBulkhead feature. |
NXOpen.Features.ShipDesign.UnfoldedMinRecBuilder |
Represents the class Features. |
NXOpen.Features.ShipDesign.UpdateShipLibrary |
Represents a update ship library feature |
NXOpen.Features.ShipDesign.UpdateShipLibraryBuilder |
Represents a NXOpen.Features.ShipDesign.UpdateShipLibrary builder |
NXOpen.Features.ShipDesign.VentHolesMarking |
Represents a vent holes marking feature |
NXOpen.Features.ShipDesign.VentHolesMarkingBuilder |
Represents a NXOpen.Features.ShipDesign.VentHolesMarking builder |
NXOpen.Features.ShipDesign.VentilationHoles2 |
Represents a ventilation holes2 feature |
NXOpen.Features.ShipDesign.VentilationHoles2Builder |
Represents a NXOpen.Features.ShipDesign.VentilationHoles2 builder |
NXOpen.Features.ShipDesign.VerifyPenetrationBuilder |
Represents a NXOpen.Features.ShipDesign.VerifyPenetrationBuilder builder |
NXOpen.Features.ShipDesign.WeightAndCGBuilder |
Represents the class Features. |
NXOpen.Features.ShipDesign.WeldCut |
Represents a weld cut feature |
NXOpen.Features.ShipDesign.WeldCut2 |
Represents a weld cut2 feature |
NXOpen.Features.ShipDesign.WeldCut2Builder |
Represents a NXOpen.Features.ShipDesign.WeldCut2 builder |
NXOpen.Features.ShipDesign.WeldCutBuilder |
Represents a NXOpen.Features.ShipDesign.WeldCut builder |
NXOpen.Features.ShipDesign.YFrameBuilder |
Represents a NXOpen.Features.ShipDesign.YFrameBuilder |
NXOpen.Features.ShipDesign.ZFrameBuilder |
Represents a NXOpen.Features.ShipDesign.ZFrameBuilder |