ProfileTransitionBuilderFeatureModeType Enumeration¶
NXOpen.Features.ShipDesign.ProfileTransitionBuilder.FeatureModeType is an alias for NXOpen.Features.ShipDesign.ProfileTransitionBuilderFeatureModeType
-
class
NXOpen.Features.ShipDesign.
ProfileTransitionBuilderFeatureModeType
¶ Bases:
object
Represents the feature mode option.
Enum Members
Enum Member Enum Member Description Target Create transition on the target body.SeparateWebAndFace Create in seperate parts for web and face plate.SeparateFace Create web trim on target body and face plate in a seperate part.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-