SubSystemsBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
SubSystemsBuilder
¶ Bases:
NXOpen.Features.ShipDesign.FeatureParmsBuilder
This class is used to edit a
NXOpen.Features.ShipDesign.SubSystems
feature.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateSubSystemsBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the tolerance, in degrees, used to determine when angles are zero. |
DistanceTolerance | Returns or sets the tolerance used to determine when distances are considered zero. |
OrientationAngleRule | Returns or sets the angle rule to use when measuring angles. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Seams | Returns the seams that you want to actually split the plate system or profile system. |
SubPillarDefinitionList | Returns the list of Sub Pillar System Definitions. |
SubPlateDefinitionList | Returns the list of Sub Plate System Definitions. |
SubProfileDefinitionList | Returns the list of Sub Profile System Definitions. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreatePlaneForList | Create a NXOpen.Features.ShipDesign.PlaneListBuilder to add a defined plane to a list. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubSystemsBuilderTypes Enumeration | Used to indicate the type of sub system definition that is being edited. |
Property Detail¶
Seams¶
-
SubSystemsBuilder.
Seams
¶ Returns the seams that you want to actually split the plate system or profile system.
Straking seams will be ignored if added to this selection.
-------------------------------------
Getter Method
Signature
Seams()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
SubPillarDefinitionList¶
-
SubSystemsBuilder.
SubPillarDefinitionList
¶ Returns the list of Sub Pillar System Definitions.
-------------------------------------
Getter Method
Signature
SubPillarDefinitionList()
Returns: Return type: NXOpen.Features.ShipDesign.SubSystemBuilderList
New in version NX8.0.0.
License requirements: None.
SubPlateDefinitionList¶
-
SubSystemsBuilder.
SubPlateDefinitionList
¶ Returns the list of Sub Plate System Definitions.
-------------------------------------
Getter Method
Signature
SubPlateDefinitionList()
Returns: Return type: NXOpen.Features.ShipDesign.SubSystemBuilderList
New in version NX8.0.0.
License requirements: None.
SubProfileDefinitionList¶
-
SubSystemsBuilder.
SubProfileDefinitionList
¶ Returns the list of Sub Profile System Definitions.
-------------------------------------
Getter Method
Signature
SubProfileDefinitionList()
Returns: Return type: NXOpen.Features.ShipDesign.SubSystemBuilderList
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SubSystemsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.