StandardPartFrameworkBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
StandardPartFrameworkBuilder
¶ Bases:
NXOpen.Builder
Represents the standard part framework builder to add or edit ship standard part.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateStandardPartFrameworkBuilder
Default values.
Property Value Thickness.Value (deprecated) 5 (millimeters part), 0.02 (inches part) New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ConfigAttribute | Returns or sets the configure attribute, which is read from the design environment by the settings in the configuration XML file. |
FirstCompartment | Returns or sets the first compartment option. |
ManufacturingStock | Returns the manufacturing stock builder that holds the manufacturing data. |
PartCategory | Returns or sets the part category, which is defined in registration file. |
PartCreationType | Returns or sets the creation type. |
PartSubType | Returns or sets the part sub type, which is the sub category of sub type. |
PartType | Returns or sets the part type, which is the sub category of part type. |
ReverseDirection | Returns or sets the option whether to reverse direction. |
SecondCompartment | Returns or sets the second compartment option. |
ShipNames | Returns the Ship Names builder, used to assign names to the Standard Parts created. |
StandardPartGroupOption | Returns or sets the option whether to group multiple standard parts together to share the same parameters during the update when editing. |
StandardPartItem | Returns the standard part item, which is the builder of the selection item. |
StandardPartList | Returns the standard part list, which supports to add more than one standard part at one time. |
Tag | Returns the Tag for this object. |
Thickness | Returns the standard part thickness. |
ThicknessDirection | Returns or sets the option whether to change thickness direction. |
WeldCharacteristics | Returns the weld characteristics. |
Methods¶
Method | Description |
---|---|
AddStandardPart | Adds a standard part into the assembly context, restores the broken wave links and renames the standard part when all external references are defined. |
ApplySmartRuleResult | Applies the smart rule results to the spreadsheet data block. |
CheckInterference | Checks the clearance between the standard parts and the other components in current assembly. |
CheckSpreadsheetInput | Looks for the parameter values that are owned by reference geometeries(Attributes) and/or template parts(attributes or expressions) and used as inputs to look for the parameter values in spreadsheet. |
Commit | Commits any edits that have been applied to the builder. |
CopyFromWeldCharacteristics | Copies the weld characteristics from the specific standard part item builder. |
CopyToWeldCharacteristics | Copies the weld characteristics to the specific standard part item builder. |
CreateStandardPartItem | Creates a new StandardPartItemBuilder and intialize the builder with data from the reference builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EndRunSmartRule | End run the smart rules. |
FlipThicknessDirection | Flips the standard part thickness direction. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDataFile | Retrieves the data file name from the registration spread sheet. |
GetModelFile | Retrieves the model file name from the registration spread sheet. |
GetObject | Returns the object currently being edited by this builder. |
GetStandardPartName | Returns the default name of the added standard part name @return |
ModifySpreadsheetData | Modifies specific parameter values without change parameter statuses. |
PostUpdate | Does the final check to finish the process of updating standar parts. |
RemoveInstance | Removes the standard part instance. |
ResetPartIndex | Resets the standard part index so that the next standard part would be added with the index in its name starting from 1. |
ResetRuleInputCache | Resets rule trigger source cache so the rule trigger evaluation can start from original point. |
RunSmartRule | Runs the smart rule engine to get the inference result. |
SetCurrentStandardPartItem | Sets the current standard part item that is edited. |
SetStandardPartVersion | Set the standard part version. |
SetView | Sets the current view normal to the main plane, which is the base plane to construct the primary sketch in the template part. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateModel | Updates all standard parts |
UpdateSpreadsheetData | Updates the parameter values which are defined in the parameter spreadsheet. |
UpdateSpreadsheetDataNoUpdate | Updates the parameter values which are defined in the parameter spreadsheet but not update the standard parts. |
UpdateThickness | Updates the user input thickness to the standard parts. |
UpdateThicknessDirection | Updates the standard part thickness direction. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StandardPartFrameworkBuilderCreationType Enumeration | Indicates the creation type |
StandardPartFrameworkBuilderSmartRuleStage Enumeration | Indicates the stage of the smart rule. |
Property Detail¶
ConfigAttribute¶
-
StandardPartFrameworkBuilder.
ConfigAttribute
¶ Returns or sets the configure attribute, which is read from the design environment by the settings in the configuration XML file.
-------------------------------------
Getter Method
Signature
ConfigAttribute()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfigAttribute(strConfigAttr)
Parameters: strConfigAttr (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
FirstCompartment¶
-
StandardPartFrameworkBuilder.
FirstCompartment
¶ Returns or sets the first compartment option.
-------------------------------------
Getter Method
Signature
FirstCompartment()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstCompartment(firstOption)
Parameters: firstOption (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ManufacturingStock¶
-
StandardPartFrameworkBuilder.
ManufacturingStock
¶ Returns the manufacturing stock builder that holds the manufacturing data.
-------------------------------------
Getter Method
Signature
ManufacturingStock()
Returns: Return type: NXOpen.Features.ShipDesign.ManufacturingStockBuilder
New in version NX8.5.0.
License requirements: None.
PartCategory¶
-
StandardPartFrameworkBuilder.
PartCategory
¶ Returns or sets the part category, which is defined in registration file.
The typical standard part types include stiffener end bracket, collar plate, tripping bracket, flat bar etc.
-------------------------------------
Getter Method
Signature
PartCategory()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartCategory(partType)
Parameters: partType (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
PartCreationType¶
-
StandardPartFrameworkBuilder.
PartCreationType
¶ Returns or sets the creation type.
-------------------------------------
Getter Method
Signature
PartCreationType()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartFrameworkBuilderCreationType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartCreationType(creationType)
Parameters: creationType ( NXOpen.Features.ShipDesign.StandardPartFrameworkBuilderCreationType
) –New in version NX9.0.2.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
PartSubType¶
-
StandardPartFrameworkBuilder.
PartSubType
¶ Returns or sets the part sub type, which is the sub category of sub type.
-------------------------------------
Getter Method
Signature
PartSubType()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartSubType(partLeafType)
Parameters: partLeafType (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
PartType¶
-
StandardPartFrameworkBuilder.
PartType
¶ Returns or sets the part type, which is the sub category of part type.
-------------------------------------
Getter Method
Signature
PartType()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartType(partSubType)
Parameters: partSubType (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ReverseDirection¶
-
StandardPartFrameworkBuilder.
ReverseDirection
¶ Returns or sets the option whether to reverse direction.
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX8.0.3: Removed with no replacement
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirectionOption)
Parameters: reverseDirectionOption (bool) – New in version NX8.0.0.
Deprecated since version NX8.0.3: Use
NXOpen.Features.ShipDesign.StandardPartFrameworkBuilder
.ModifySpreadSheetData() instead.License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SecondCompartment¶
-
StandardPartFrameworkBuilder.
SecondCompartment
¶ Returns or sets the second compartment option.
-------------------------------------
Getter Method
Signature
SecondCompartment()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondCompartment(secondOption)
Parameters: secondOption (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ShipNames¶
-
StandardPartFrameworkBuilder.
ShipNames
¶ Returns the Ship Names builder, used to assign names to the Standard Parts created.
-------------------------------------
Getter Method
Signature
ShipNames()
Returns: Ship Names Builder Return type: NXOpen.Features.ShipDesign.ShipNamesBuilder
New in version NX9.0.2.
License requirements: None.
StandardPartGroupOption¶
-
StandardPartFrameworkBuilder.
StandardPartGroupOption
¶ Returns or sets the option whether to group multiple standard parts together to share the same parameters during the update when editing.
-------------------------------------
Getter Method
Signature
StandardPartGroupOption()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardPartGroupOption(stdPartGroupOption)
Parameters: stdPartGroupOption (bool) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
StandardPartItem¶
-
StandardPartFrameworkBuilder.
StandardPartItem
¶ Returns the standard part item, which is the builder of the selection item.
-------------------------------------
Getter Method
Signature
StandardPartItem()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilder
New in version NX8.0.0.
License requirements: None.
StandardPartList¶
-
StandardPartFrameworkBuilder.
StandardPartList
¶ Returns the standard part list, which supports to add more than one standard part at one time.
-------------------------------------
Getter Method
Signature
StandardPartList()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderList
New in version NX8.0.0.
License requirements: None.
Thickness¶
-
StandardPartFrameworkBuilder.
Thickness
¶ Returns the standard part thickness.
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
Deprecated since version NX8.0.3: Removed with no replacement
License requirements: None.
ThicknessDirection¶
-
StandardPartFrameworkBuilder.
ThicknessDirection
¶ Returns or sets the option whether to change thickness direction.
-------------------------------------
Getter Method
Signature
ThicknessDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessDirection(thicknessDirectionOption)
Parameters: thicknessDirectionOption ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
WeldCharacteristics¶
-
StandardPartFrameworkBuilder.
WeldCharacteristics
¶ Returns the weld characteristics.
-------------------------------------
Getter Method
Signature
WeldCharacteristics()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
AddStandardPart¶
-
StandardPartFrameworkBuilder.
AddStandardPart
¶ Adds a standard part into the assembly context, restores the broken wave links and renames the standard part when all external references are defined.
Signature
AddStandardPart()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ApplySmartRuleResult¶
-
StandardPartFrameworkBuilder.
ApplySmartRuleResult
¶ Applies the smart rule results to the spreadsheet data block.
Signature
ApplySmartRuleResult(pStrParamName, pStrParamValue)
Parameters: - pStrParamName (list of str) –
- pStrParamValue (list of str) –
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
CheckInterference¶
-
StandardPartFrameworkBuilder.
CheckInterference
¶ Checks the clearance between the standard parts and the other components in current assembly.
There are two types of interference to be checked. 1) Interference between standard part and other componenets, and 2) interference between standard part and cutouts.
Signature
CheckInterference()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
CheckSpreadsheetInput¶
-
StandardPartFrameworkBuilder.
CheckSpreadsheetInput
¶ Looks for the parameter values that are owned by reference geometeries(Attributes) and/or template parts(attributes or expressions) and used as inputs to look for the parameter values in spreadsheet.
Signature
CheckSpreadsheetInput(pItemBuilder)
Parameters: pItemBuilder ( NXOpen.Features.ShipDesign.StandardPartItemBuilder
) –Returns: a tuple Return type: A tuple consisting of (ppStrParamName, ppStrParamValue). ppStrParamName is a list of str. ppStrParamValue is a list of str. New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
CopyFromWeldCharacteristics¶
-
StandardPartFrameworkBuilder.
CopyFromWeldCharacteristics
¶ Copies the weld characteristics from the specific standard part item builder.
Signature
CopyFromWeldCharacteristics(stdPartItemBuilder)
Parameters: stdPartItemBuilder ( NXOpen.Features.ShipDesign.StandardPartItemBuilder
) –New in version NX9.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
CopyToWeldCharacteristics¶
-
StandardPartFrameworkBuilder.
CopyToWeldCharacteristics
¶ Copies the weld characteristics to the specific standard part item builder.
Signature
CopyToWeldCharacteristics(stdPartItemBuilder)
Parameters: stdPartItemBuilder ( NXOpen.Features.ShipDesign.StandardPartItemBuilder
) –New in version NX9.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
CreateStandardPartItem¶
-
StandardPartFrameworkBuilder.
CreateStandardPartItem
¶ Creates a new StandardPartItemBuilder and intialize the builder with data from the reference builder.
Signature
CreateStandardPartItem(refBuilder)
Parameters: refBuilder ( NXOpen.Features.ShipDesign.StandardPartItemBuilder
) –Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilder
New in version NX8.0.0.
License requirements: None.
EndRunSmartRule¶
-
StandardPartFrameworkBuilder.
EndRunSmartRule
¶ End run the smart rules.
Signature
EndRunSmartRule(pItemBuilder)
Parameters: pItemBuilder ( NXOpen.Features.ShipDesign.StandardPartItemBuilder
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
FlipThicknessDirection¶
-
StandardPartFrameworkBuilder.
FlipThicknessDirection
¶ Flips the standard part thickness direction.
If bUpdateModel is true, the model will be updated. If it is false, the thickness direction will be flipped but the model will not be updated.
Signature
FlipThicknessDirection(bUpdateModel)
Parameters: bUpdateModel (bool) – New in version NX8.0.0.
Deprecated since version NX8.0.3: Use
NXOpen.Features.ShipDesign.StandardPartFrameworkBuilder
.ModifySpreadSheetData() instead.License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
GetDataFile¶
-
StandardPartFrameworkBuilder.
GetDataFile
¶ Retrieves the data file name from the registration spread sheet.
Signature
GetDataFile(updateConfiguration)
Parameters: updateConfiguration (bool) – Whether to update the selection configuration New in version NX8.0.0.
License requirements: None.
GetModelFile¶
-
StandardPartFrameworkBuilder.
GetModelFile
¶ Retrieves the model file name from the registration spread sheet.
Signature
GetModelFile()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
GetStandardPartName¶
-
StandardPartFrameworkBuilder.
GetStandardPartName
¶ Returns the default name of the added standard part name
Signature
GetStandardPartName(bFullName)
Parameters: bFullName (bool) – Returns: Return type: str New in version NX8.0.0.
License requirements: None.
ModifySpreadsheetData¶
-
StandardPartFrameworkBuilder.
ModifySpreadsheetData
¶ Modifies specific parameter values without change parameter statuses.
This could be used to apply smart rule result.
Signature
ModifySpreadsheetData(strParamName, strParamValue)
Parameters: - strParamName (list of str) –
- strParamValue (list of str) –
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
PostUpdate¶
-
StandardPartFrameworkBuilder.
PostUpdate
¶ Does the final check to finish the process of updating standar parts.
Signature
PostUpdate()
New in version NX8.0.0.
License requirements: None.
RemoveInstance¶
-
StandardPartFrameworkBuilder.
RemoveInstance
¶ Removes the standard part instance.
Signature
RemoveInstance(itemBuilder)
Parameters: itemBuilder ( NXOpen.Features.ShipDesign.StandardPartItemBuilder
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ResetPartIndex¶
-
StandardPartFrameworkBuilder.
ResetPartIndex
¶ Resets the standard part index so that the next standard part would be added with the index in its name starting from 1.
Signature
ResetPartIndex()
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ResetRuleInputCache¶
-
StandardPartFrameworkBuilder.
ResetRuleInputCache
¶ Resets rule trigger source cache so the rule trigger evaluation can start from original point.
Signature
ResetRuleInputCache()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
RunSmartRule¶
-
StandardPartFrameworkBuilder.
RunSmartRule
¶ Runs the smart rule engine to get the inference result.
Signature
RunSmartRule(pItemBuilder, stage)
Parameters: Returns: a tuple
Return type: A tuple consisting of (ppStrParamName, ppStrParamValue, ppStrParamDescription). ppStrParamName is a list of str. ppStrParamValue is a list of str. ppStrParamDescription is a list of str.
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SetCurrentStandardPartItem¶
-
StandardPartFrameworkBuilder.
SetCurrentStandardPartItem
¶ Sets the current standard part item that is edited.
This is useful if standard part framework works in non-group mode.
Signature
SetCurrentStandardPartItem(pCurItemBuilder)
Parameters: pCurItemBuilder ( NXOpen.Features.ShipDesign.StandardPartItemBuilder
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SetStandardPartVersion¶
-
StandardPartFrameworkBuilder.
SetStandardPartVersion
¶ Set the standard part version.
Signature
SetStandardPartVersion(standardPartVersion)
Parameters: standardPartVersion (float) – New in version NX9.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SetView¶
-
StandardPartFrameworkBuilder.
SetView
¶ Sets the current view normal to the main plane, which is the base plane to construct the primary sketch in the template part.
If there is no sketch found, nothing will be done.
Signature
SetView()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
UpdateModel¶
-
StandardPartFrameworkBuilder.
UpdateModel
¶ Updates all standard parts
Signature
UpdateModel()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
UpdateSpreadsheetData¶
-
StandardPartFrameworkBuilder.
UpdateSpreadsheetData
¶ Updates the parameter values which are defined in the parameter spreadsheet.
It also updates the standard parts.
Signature
UpdateSpreadsheetData(strParamName, strParamValue, pnParamStatus)
Parameters: - strParamName (list of str) –
- strParamValue (list of str) –
- pnParamStatus (list of int) –
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
UpdateSpreadsheetDataNoUpdate¶
-
StandardPartFrameworkBuilder.
UpdateSpreadsheetDataNoUpdate
¶ Updates the parameter values which are defined in the parameter spreadsheet but not update the standard parts.
Signature
UpdateSpreadsheetDataNoUpdate(strParamName, strParamValue, pnParamStatus)
Parameters: - strParamName (list of str) –
- strParamValue (list of str) –
- pnParamStatus (list of int) –
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
UpdateThickness¶
-
StandardPartFrameworkBuilder.
UpdateThickness
¶ Updates the user input thickness to the standard parts.
If bUpdateModel is true, the model will be updated. If it is false, the thickness value will be changed but the model will not be updated.
Signature
UpdateThickness(bUpdateModel)
Parameters: bUpdateModel (bool) – New in version NX8.0.0.
Deprecated since version NX8.0.3: Use
NXOpen.Features.ShipDesign.StandardPartFrameworkBuilder
.ModifySpreadSheetData() instead.License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
UpdateThicknessDirection¶
-
StandardPartFrameworkBuilder.
UpdateThicknessDirection
¶ Updates the standard part thickness direction.
If bUpdateModel is true, the model will be updated. If it is false, the thickness direction will be flipped but the model will not be updated.
Signature
UpdateThicknessDirection(bUpdateModel)
Parameters: bUpdateModel (bool) – New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
Validate¶
-
StandardPartFrameworkBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.