ExpansionDrawingBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ExpansionDrawingBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ShipDesign.ExpansionDrawingBuilder
.This class is for expansion drawing
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateExpansionDrawingBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AftPlane | Returns or sets the aft plane |
BasePlane | Returns or sets the base plane |
DrawingTemplate | Returns the drawing template |
ForePlane | Returns or sets the fore plane |
PlatesToExpand | Returns the plates to be expanded |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
UpperPlane | Returns or sets the upper plane |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AftPlane¶
-
ExpansionDrawingBuilder.
AftPlane
¶ Returns or sets the aft plane
-------------------------------------
Getter Method
Signature
AftPlane()
Returns: Return type: NXOpen.Plane
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AftPlane(aftPlane)
Parameters: aftPlane ( NXOpen.Plane
) –New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
BasePlane¶
-
ExpansionDrawingBuilder.
BasePlane
¶ Returns or sets the base plane
-------------------------------------
Getter Method
Signature
BasePlane()
Returns: Return type: NXOpen.Plane
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePlane(basePlane)
Parameters: basePlane ( NXOpen.Plane
) –New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
DrawingTemplate¶
-
ExpansionDrawingBuilder.
DrawingTemplate
¶ Returns the drawing template
-------------------------------------
Getter Method
Signature
DrawingTemplate()
Returns: Return type: NXOpen.Features.ShipDesign.DrawingTemplateBuilder
New in version NX10.0.0.
License requirements: None.
ForePlane¶
-
ExpansionDrawingBuilder.
ForePlane
¶ Returns or sets the fore plane
-------------------------------------
Getter Method
Signature
ForePlane()
Returns: Return type: NXOpen.Plane
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForePlane(forePlane)
Parameters: forePlane ( NXOpen.Plane
) –New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
PlatesToExpand¶
-
ExpansionDrawingBuilder.
PlatesToExpand
¶ Returns the plates to be expanded
-------------------------------------
Getter Method
Signature
PlatesToExpand()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX10.0.0.
License requirements: None.
Tolerance¶
-
ExpansionDrawingBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
UpperPlane¶
-
ExpansionDrawingBuilder.
UpperPlane
¶ Returns or sets the upper plane
-------------------------------------
Getter Method
Signature
UpperPlane()
Returns: Return type: NXOpen.Plane
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperPlane(upperPlane)
Parameters: upperPlane ( NXOpen.Plane
) –New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
Method Detail¶
Validate¶
-
ExpansionDrawingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.