Plane Class¶
-
class
NXOpen.
Plane
¶ Bases:
NXOpen.SmartObject
,NXOpen.IPlane
,NXOpen.ISurface
,NXOpen.IOrientation
Represents an
Plane
class.No Creator because of a problem with arrays in APIWRAP
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
Expression | Returns the plane expression. |
Flip | Returns the flip direction of the plane |
FrenetSubtype | Returns the subtype of on curve type of plane fron NX6 onwards. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Matrix | Returns or sets the matrix of the plane |
Method | Returns a plane type |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
Normal | Returns or sets the normal of the plane |
OffsetExpression | Returns or sets the plane offset expression. |
OffsetFlip | Returns the flip state of the offset direction of the plane |
Origin | Returns or sets the origin of the plane |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Percent | Returns the arclenth or the percent value |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Update | Returns the update option. |
Visibility | Returns the visibility. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
ConvertToSmartPlane | Set PLANE_parms to plane to make it smart plane |
CopySoPlane | Creates an Plane using a datum plane feature. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
DestroyPlane | Destroy the plane object |
Evaluate | Evaluates the plane |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAlternate | Returns the alternate type @return |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetGeometry | Returns the geometry @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNumberOfAlternate | Returns the number of alternate solutions @return |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetReverseSection | Returns the reverse section @return |
GetReverseSide | Returns the reverse side @return |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveOffsetData | Remove all offset data from the plane |
RemoveParameters | Removes the smart object parameters. |
RemoveViewDependency | Remove dependency on all views from an object. |
ReplaceExpression | Replace the expression in on curve plane plane |
ReplaceParameters | Edit a smart object by replacing its parameters using parameters of other smart object of the same class. |
ResetExpressionValue | Reset the expression value in on curve plane plane |
SetAlternate | Sets the alternate type |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetExpression | Sets the plane expression. |
SetFlip | Flip the direction of the plane |
SetFrenetSubtype | Sets subtype for a specific plane type where the alternate solution cannot handle. |
SetGeometry | Sets the geometry |
SetMethod | Sets a plane type |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetOffsetExpression | Sets the plane offset expression value. |
SetOffsetFlip | Sets the flip state of the offset direction of the plane |
SetPercent | Sets the arclenth or the percent value |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetReverseSection | Sets the reverse_section |
SetReverseSide | Sets the reverse side |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUpdateOption | Set to plane update |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetVisibility | Sets the visibility. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Property Detail¶
Expression¶
-
Plane.
Expression
¶ Returns the plane expression.
-------------------------------------
Getter Method
Signature
Expression()
Returns: offset value Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
Flip¶
-
Plane.
Flip
¶ Returns the flip direction of the plane
-------------------------------------
Getter Method
Signature
Flip()
Returns: flip direction Return type: bool New in version NX4.0.0.
License requirements: None.
FrenetSubtype¶
-
Plane.
FrenetSubtype
¶ Returns the subtype of on curve type of plane fron NX6 onwards.
It is a valid function for and only for on-curve type plane of NX6 onwards.
-------------------------------------
Getter Method
Signature
FrenetSubtype()
Returns: Return type: NXOpen.PlaneTypesFrenetSubtype
New in version NX6.0.0.
License requirements: None.
IsOccurrence¶
-
Plane.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Plane.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Matrix¶
-
Plane.
Matrix
¶ Returns or sets the matrix of the plane
-------------------------------------
Getter Method
Signature
Matrix()
Returns: Return type: NXOpen.Matrix3x3
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Matrix(matrix)
Parameters: matrix ( NXOpen.Matrix3x3
) –New in version NX7.5.0.
License requirements: None.
Method¶
-
Plane.
Method
¶ Returns a plane type
-------------------------------------
Getter Method
Signature
Method()
Returns: Return type: NXOpen.PlaneTypesMethodType
New in version NX4.0.0.
License requirements: None.
Name¶
-
Plane.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Normal¶
-
Plane.
Normal
¶ Returns or sets the normal of the plane
-------------------------------------
Getter Method
Signature
Normal()
Returns: Return type: NXOpen.Vector3d
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Normal(normal)
Parameters: normal ( NXOpen.Vector3d
) –New in version NX4.0.0.
License requirements: None.
OffsetExpression¶
-
Plane.
OffsetExpression
¶ Returns or sets the plane offset expression.
-------------------------------------
Getter Method
Signature
OffsetExpression()
Returns: offset value Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetExpression(valueExpression)
Parameters: valueExpression ( NXOpen.Expression
) – offset valueNew in version NX8.5.0.
License requirements: None.
OffsetFlip¶
-
Plane.
OffsetFlip
¶ Returns the flip state of the offset direction of the plane
-------------------------------------
Getter Method
Signature
OffsetFlip()
Returns: offset flip direction Return type: bool New in version NX7.5.0.
License requirements: None.
Origin¶
-
Plane.
Origin
¶ Returns or sets the origin of the plane
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Origin(origin)
Parameters: origin ( NXOpen.Point3d
) –New in version NX4.0.0.
License requirements: None.
OwningComponent¶
-
Plane.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Plane.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Percent¶
-
Plane.
Percent
¶ Returns the arclenth or the percent value
-------------------------------------
Getter Method
Signature
Percent()
Returns: arclength or percent value Return type: bool New in version NX4.0.0.
License requirements: None.
Prototype¶
-
Plane.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
ConvertToSmartPlane¶
-
Plane.
ConvertToSmartPlane
¶ Set PLANE_parms to plane to make it smart plane
Signature
ConvertToSmartPlane()
New in version NX7.0.0.
License requirements: None.
CopySoPlane¶
-
Plane.
CopySoPlane
¶ Creates an
Plane
using a datum plane feature.Signature
CopySoPlane()
Returns: Return type: NXOpen.Plane
New in version NX4.0.0.
License requirements: None.
DestroyPlane¶
-
Plane.
DestroyPlane
¶ Destroy the plane object
Signature
DestroyPlane()
New in version NX6.0.3.
License requirements: None.
Evaluate¶
-
Plane.
Evaluate
¶ Evaluates the plane
Signature
Evaluate()
New in version NX4.0.0.
License requirements: None.
FindObject¶
-
Plane.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAlternate¶
-
Plane.
GetAlternate
¶ Returns the alternate type
Signature
GetAlternate()
Returns: Return type: NXOpen.PlaneTypesAlternateType
New in version NX4.0.0.
License requirements: None.
GetGeometry¶
-
Plane.
GetGeometry
¶ Returns the geometry
Signature
GetGeometry()
Returns: Return type: list of NXOpen.NXObject
New in version NX4.0.0.
License requirements: None.
GetNumberOfAlternate¶
-
Plane.
GetNumberOfAlternate
¶ Returns the number of alternate solutions
Signature
GetNumberOfAlternate()
Returns: Return type: int New in version NX4.0.0.
License requirements: None.
GetReverseSection¶
-
Plane.
GetReverseSection
¶ Returns the reverse section
Signature
GetReverseSection()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
GetReverseSide¶
-
Plane.
GetReverseSide
¶ Returns the reverse side
Signature
GetReverseSide()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
Print¶
-
Plane.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveOffsetData¶
-
Plane.
RemoveOffsetData
¶ Remove all offset data from the plane
Signature
RemoveOffsetData()
New in version NX7.5.0.
License requirements: None.
ReplaceExpression¶
-
Plane.
ReplaceExpression
¶ Replace the expression in on curve plane plane
Signature
ReplaceExpression(expTag)
Parameters: expTag ( NXOpen.Expression
) –New in version NX7.5.0.
License requirements: None.
ResetExpressionValue¶
-
Plane.
ResetExpressionValue
¶ Reset the expression value in on curve plane plane
Signature
ResetExpressionValue()
New in version NX7.5.0.
License requirements: None.
SetAlternate¶
-
Plane.
SetAlternate
¶ Sets the alternate type
Signature
SetAlternate(type)
Parameters: type ( NXOpen.PlaneTypesAlternateType
) –New in version NX4.0.0.
License requirements: None.
SetExpression¶
-
Plane.
SetExpression
¶ Sets the plane expression.
Only valid for the following types:
PlaneTypesMethodType.Frenet
orPlaneTypesMethodType.Distance
.Signature
SetExpression(valueExpression)
Parameters: valueExpression (str) – offset value NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: None.
SetFlip¶
-
Plane.
SetFlip
¶ Flip the direction of the plane
Signature
SetFlip(flip)
Parameters: flip (bool) – flip direction New in version NX4.0.0.
License requirements: None.
SetFrenetSubtype¶
-
Plane.
SetFrenetSubtype
¶ Sets subtype for a specific plane type where the alternate solution cannot handle.
Indeed, this is for frenet type only so far, after the Nissan enhancement in NX6.
Signature
SetFrenetSubtype(subtype)
Parameters: subtype ( NXOpen.PlaneTypesFrenetSubtype
) –New in version NX6.0.0.
License requirements: None.
SetGeometry¶
-
Plane.
SetGeometry
¶ Sets the geometry
Signature
SetGeometry(geom)
Parameters: geom (list of NXOpen.NXObject
) –New in version NX4.0.0.
License requirements: None.
SetMethod¶
-
Plane.
SetMethod
¶ Sets a plane type
Signature
SetMethod(type)
Parameters: type ( NXOpen.PlaneTypesMethodType
) –New in version NX4.0.0.
License requirements: None.
SetName¶
-
Plane.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetOffsetExpression¶
-
Plane.
SetOffsetExpression
¶ Overloaded method SetOffsetExpression
SetOffsetExpression(valueExpression)
OffsetExpression(valueExpression)
-------------------------------------
Sets the plane offset expression value.
Signature
SetOffsetExpression(valueExpression)
Parameters: valueExpression (str) – offset value NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.0.
License requirements: None.
-------------------------------------
Returns or sets the plane offset expression.
-------------------------------------
Getter Method
Signature
OffsetExpression(valueExpression)
Parameters: valueExpression ( NXOpen.Expression
) – offset valueNew in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetExpression(valueExpression)
Parameters: valueExpression ( NXOpen.Expression
) – offset valueNew in version NX8.5.0.
License requirements: None.
-------------------------------------
SetOffsetFlip¶
-
Plane.
SetOffsetFlip
¶ Sets the flip state of the offset direction of the plane
Signature
SetOffsetFlip(flip)
Parameters: flip (bool) – offset flip direction New in version NX7.5.0.
License requirements: None.
SetPercent¶
-
Plane.
SetPercent
¶ Sets the arclenth or the percent value
Signature
SetPercent(percent)
Parameters: percent (bool) – arclength or percent value New in version NX4.0.0.
License requirements: None.
SetReverseSection¶
-
Plane.
SetReverseSection
¶ Sets the reverse_section
Signature
SetReverseSection(reverseSection)
Parameters: reverseSection (bool) – New in version NX4.0.0.
License requirements: None.
SetReverseSide¶
-
Plane.
SetReverseSide
¶ Sets the reverse side
Signature
SetReverseSide(reverseSide)
Parameters: reverseSide (bool) – New in version NX4.0.0.
License requirements: None.
SetUpdateOption¶
-
Plane.
SetUpdateOption
¶ Set to plane update
Signature
SetUpdateOption(update)
Parameters: update ( NXOpen.SmartObjectUpdateOption
) –New in version NX5.0.0.
License requirements: None.