ManufacturingPreparationBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ManufacturingPreparationBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
This builder is used to adds attributes to the part and body identifying manufacturing related data.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateManufacturingPreparationBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
FeatureName | Returns or sets the feature name |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SaProject | Returns or sets the project number assigned to the ship. |
SectionNumber | Returns or sets the ship section number. |
SteelComponents | Returns the design elements to prepare for manufacturing. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDesignElementAttributeValue | Get the attribute value of the given design element. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
InitializeDesignElementAttributes | Read the design attributes and use them to initialize the builder values. |
SetDesignElementAttributeValue | Set the attribute value of the given design element. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ManufacturingPreparationBuilderAttributeType Enumeration | Represents manufacturing attribute type. |
Property Detail¶
FeatureName¶
-
ManufacturingPreparationBuilder.
FeatureName
¶ Returns or sets the feature name
-------------------------------------
Getter Method
Signature
FeatureName()
Returns: Return type: str New in version NX8.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureName(featureName)
Parameters: featureName (str) – New in version NX8.0.3.
License requirements: nx_ship_concept (“Ship Concept”)
SaProject¶
-
ManufacturingPreparationBuilder.
SaProject
¶ Returns or sets the project number assigned to the ship.
-------------------------------------
Getter Method
Signature
SaProject()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaProject(saProject)
Parameters: saProject (str) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
SectionNumber¶
-
ManufacturingPreparationBuilder.
SectionNumber
¶ Returns or sets the ship section number.
-------------------------------------
Getter Method
Signature
SectionNumber()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionNumber(sectionNumber)
Parameters: sectionNumber (str) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
SteelComponents¶
-
ManufacturingPreparationBuilder.
SteelComponents
¶ Returns the design elements to prepare for manufacturing.
-------------------------------------
Getter Method
Signature
SteelComponents()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: None.
Method Detail¶
GetDesignElementAttributeValue¶
-
ManufacturingPreparationBuilder.
GetDesignElementAttributeValue
¶ Get the attribute value of the given design element.
Signature
GetDesignElementAttributeValue(designElement, attrType)
Parameters: - designElement (
NXOpen.DisplayableObject
) – the design element for manufacturing preparation. - attrType (
NXOpen.Features.ShipDesign.ManufacturingPreparationBuilderAttributeType
) – the attriubte type.
Returns: the attribute value.
Return type: str
New in version NX8.0.0.
License requirements: None.
- designElement (
InitializeDesignElementAttributes¶
-
ManufacturingPreparationBuilder.
InitializeDesignElementAttributes
¶ Read the design attributes and use them to initialize the builder values.
Signature
InitializeDesignElementAttributes(designElement)
Parameters: designElement ( NXOpen.DisplayableObject
) – the design element for manufacturing preparation.New in version NX8.0.0.
License requirements: None.
SetDesignElementAttributeValue¶
-
ManufacturingPreparationBuilder.
SetDesignElementAttributeValue
¶ Set the attribute value of the given design element.
Signature
SetDesignElementAttributeValue(designElement, attrType, attrValue)
Parameters: - designElement (
NXOpen.DisplayableObject
) – the design element for manufacturing preparation. - attrType (
NXOpen.Features.ShipDesign.ManufacturingPreparationBuilderAttributeType
) – the attriubte type. - attrValue (str) – the attribute value.
New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
- designElement (
Validate¶
-
ManufacturingPreparationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.