ShipSectionBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ShipSectionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.ShipSection
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateShipSectionBuilder
Default values.
Property Value ReadDataSet.CreateDataSetToggle 0 ReadDataSet.NativeToggle 0 XDatumFilter All XMaxOffset.Value 0 (millimeters part), 0 (inches part) XMinOffset.Value 0 (millimeters part), 0 (inches part) YMaxOffset.Value 0 (millimeters part), 0 (inches part) YMinOffset.Value 0 (millimeters part), 0 (inches part) ZDatumFilter All ZMaxOffset.Value 0 (millimeters part), 0 (inches part) ZMinOffset.Value 0 (millimeters part), 0 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AssemblyPart | Returns or sets the assembly part |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReadDataSet | Returns the Data Set Builder for reading data sets from Team Center |
ReferenceGeometry | Returns the reference geometry |
SectionName | Returns or sets the section name |
SectionPart | Returns or sets the section part |
SectionType | Returns or sets the creation method |
SectionXMax | Returns or sets the section xmax |
SectionXMin | Returns or sets the section xmin |
SectionYMax | Returns or sets the section ymax |
SectionYMin | Returns or sets the section ymin |
SectionZMax | Returns or sets the section zmax |
SectionZMin | Returns or sets the section zmin |
ShipBody | Returns the ship body |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
XDatumFilter | Returns or sets the x datum filter |
XMaxDatumFilter | Returns or sets the x max datum filter |
XMaxOffset | Returns the x max offset |
XMinDatumFilter | Returns or sets the x min datum filter |
XMinOffset | Returns the x min offset |
YDatumFilter | Returns or sets the y datum filter |
YMaxDatumFilter | Returns or sets the y max datum filter |
YMaxOffset | Returns the y max offset |
YMinDatumFilter | Returns or sets the y min datum filter |
YMinOffset | Returns the y min offset |
ZDatumFilter | Returns or sets the z datum filter |
ZMaxDatumFilter | Returns or sets the z max datum filter |
ZMaxOffset | Returns the z max offset |
ZMinDatumFilter | Returns or sets the z min datum filter |
ZMinOffset | Returns the z min offset |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShipSectionBuilderType Enumeration | Define the creation type |
ShipSectionBuilderXFilter Enumeration | Define the output option for each of the frame type |
ShipSectionBuilderZFilter Enumeration | Define the output option for each of the frame type |
Property Detail¶
AssemblyPart¶
-
ShipSectionBuilder.
AssemblyPart
¶ Returns or sets the assembly part
-------------------------------------
Getter Method
Signature
AssemblyPart()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssemblyPart(filename)
Parameters: filename (str) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ReadDataSet¶
-
ShipSectionBuilder.
ReadDataSet
¶ Returns the Data Set Builder for reading data sets from Team Center
-------------------------------------
Getter Method
Signature
ReadDataSet()
Returns: Return type: NXOpen.Features.ShipDesign.ReadDataSetBuilder
New in version NX8.5.0.
License requirements: None.
ReferenceGeometry¶
-
ShipSectionBuilder.
ReferenceGeometry
¶ Returns the reference geometry
-------------------------------------
Getter Method
Signature
ReferenceGeometry()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
SectionName¶
-
ShipSectionBuilder.
SectionName
¶ Returns or sets the section name
-------------------------------------
Getter Method
Signature
SectionName()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionName(sectionName)
Parameters: sectionName (str) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionPart¶
-
ShipSectionBuilder.
SectionPart
¶ Returns or sets the section part
-------------------------------------
Getter Method
Signature
SectionPart()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionPart(filename)
Parameters: filename (str) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionType¶
-
ShipSectionBuilder.
SectionType
¶ Returns or sets the creation method
-------------------------------------
Getter Method
Signature
SectionType()
Returns: Return type: NXOpen.Features.ShipDesign.ShipSectionBuilderType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionType(type)
Parameters: type ( NXOpen.Features.ShipDesign.ShipSectionBuilderType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionXMax¶
-
ShipSectionBuilder.
SectionXMax
¶ Returns or sets the section xmax
-------------------------------------
Getter Method
Signature
SectionXMax()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionXMax(sectionXMax)
Parameters: sectionXMax (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionXMin¶
-
ShipSectionBuilder.
SectionXMin
¶ Returns or sets the section xmin
-------------------------------------
Getter Method
Signature
SectionXMin()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionXMin(sectionXMin)
Parameters: sectionXMin (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionYMax¶
-
ShipSectionBuilder.
SectionYMax
¶ Returns or sets the section ymax
-------------------------------------
Getter Method
Signature
SectionYMax()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionYMax(sectionYMax)
Parameters: sectionYMax (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionYMin¶
-
ShipSectionBuilder.
SectionYMin
¶ Returns or sets the section ymin
-------------------------------------
Getter Method
Signature
SectionYMin()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionYMin(sectionYMin)
Parameters: sectionYMin (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionZMax¶
-
ShipSectionBuilder.
SectionZMax
¶ Returns or sets the section zmax
-------------------------------------
Getter Method
Signature
SectionZMax()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionZMax(sectionZMax)
Parameters: sectionZMax (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionZMin¶
-
ShipSectionBuilder.
SectionZMin
¶ Returns or sets the section zmin
-------------------------------------
Getter Method
Signature
SectionZMin()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionZMin(sectionZMin)
Parameters: sectionZMin (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ShipBody¶
-
ShipSectionBuilder.
ShipBody
¶ Returns the ship body
-------------------------------------
Getter Method
Signature
ShipBody()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
XDatumFilter¶
-
ShipSectionBuilder.
XDatumFilter
¶ Returns or sets the x datum filter
-------------------------------------
Getter Method
Signature
XDatumFilter()
Returns: Return type: NXOpen.Features.ShipDesign.ShipSectionBuilderXFilter
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XDatumFilter(xDatumFilter)
Parameters: xDatumFilter ( NXOpen.Features.ShipDesign.ShipSectionBuilderXFilter
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
XMaxDatumFilter¶
-
ShipSectionBuilder.
XMaxDatumFilter
¶ Returns or sets the x max datum filter
-------------------------------------
Getter Method
Signature
XMaxDatumFilter()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XMaxDatumFilter(xMaxDatumFilter)
Parameters: xMaxDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
XMaxOffset¶
-
ShipSectionBuilder.
XMaxOffset
¶ Returns the x max offset
-------------------------------------
Getter Method
Signature
XMaxOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
XMinDatumFilter¶
-
ShipSectionBuilder.
XMinDatumFilter
¶ Returns or sets the x min datum filter
-------------------------------------
Getter Method
Signature
XMinDatumFilter()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XMinDatumFilter(xMinDatumFilter)
Parameters: xMinDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
XMinOffset¶
-
ShipSectionBuilder.
XMinOffset
¶ Returns the x min offset
-------------------------------------
Getter Method
Signature
XMinOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
YDatumFilter¶
-
ShipSectionBuilder.
YDatumFilter
¶ Returns or sets the y datum filter
-------------------------------------
Getter Method
Signature
YDatumFilter()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YDatumFilter(yDatumFilter)
Parameters: yDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
YMaxDatumFilter¶
-
ShipSectionBuilder.
YMaxDatumFilter
¶ Returns or sets the y max datum filter
-------------------------------------
Getter Method
Signature
YMaxDatumFilter()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YMaxDatumFilter(yMaxDatumFilter)
Parameters: yMaxDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
YMaxOffset¶
-
ShipSectionBuilder.
YMaxOffset
¶ Returns the y max offset
-------------------------------------
Getter Method
Signature
YMaxOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
YMinDatumFilter¶
-
ShipSectionBuilder.
YMinDatumFilter
¶ Returns or sets the y min datum filter
-------------------------------------
Getter Method
Signature
YMinDatumFilter()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YMinDatumFilter(yMinDatumFilter)
Parameters: yMinDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
YMinOffset¶
-
ShipSectionBuilder.
YMinOffset
¶ Returns the y min offset
-------------------------------------
Getter Method
Signature
YMinOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ZDatumFilter¶
-
ShipSectionBuilder.
ZDatumFilter
¶ Returns or sets the z datum filter
-------------------------------------
Getter Method
Signature
ZDatumFilter()
Returns: Return type: NXOpen.Features.ShipDesign.ShipSectionBuilderZFilter
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZDatumFilter(zDatumFilter)
Parameters: zDatumFilter ( NXOpen.Features.ShipDesign.ShipSectionBuilderZFilter
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ZMaxDatumFilter¶
-
ShipSectionBuilder.
ZMaxDatumFilter
¶ Returns or sets the z max datum filter
-------------------------------------
Getter Method
Signature
ZMaxDatumFilter()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZMaxDatumFilter(zMaxDatumFilter)
Parameters: zMaxDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ZMaxOffset¶
-
ShipSectionBuilder.
ZMaxOffset
¶ Returns the z max offset
-------------------------------------
Getter Method
Signature
ZMaxOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ZMinDatumFilter¶
-
ShipSectionBuilder.
ZMinDatumFilter
¶ Returns or sets the z min datum filter
-------------------------------------
Getter Method
Signature
ZMinDatumFilter()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZMinDatumFilter(zMinDatumFilter)
Parameters: zMinDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ZMinOffset¶
-
ShipSectionBuilder.
ZMinOffset
¶ Returns the z min offset
-------------------------------------
Getter Method
Signature
ZMinOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
ShipSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.