StiffenerBuilderKnuckleOptions Enumeration¶
NXOpen.Features.ShipDesign.StiffenerBuilder.KnuckleOptions is an alias for NXOpen.Features.ShipDesign.StiffenerBuilderKnuckleOptions
-
class
NXOpen.Features.ShipDesign.
StiffenerBuilderKnuckleOptions
¶ Bases:
object
the knuckle option
Enum Members
Enum Member Enum Member Description None No special handling for knucklesSplit Split the stiffener at knuckle pointsBend Bend at the knuckle points-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-