MarkingLineDesignBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
MarkingLineDesignBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a new MarkingLine Feature builder.
This class is used in the process of creating or editing a marking line feature.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateMarkingLineDesignBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance for marking lines. |
DistanceTolerance | Returns or sets the distance tolerance for marking lines. |
GridPlanes | Returns the collection of planes defining all the intersections on the profiles and plates. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UseExistingCuttingSideFace | Returns or sets the option to decide if the current cutting side faces are used(true) or if the cutting side faces should be recalculated(false). |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetMarkingLineInformation | Get the information from the marking line feature to create a fillet type welding joint. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
IsMarkingLineFeature | Is the feature a marking line feature @return (O) - is a marking line feature |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
MarkingLineDesignBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance for marking lines.
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
DistanceTolerance¶
-
MarkingLineDesignBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance for marking lines.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
GridPlanes¶
-
MarkingLineDesignBuilder.
GridPlanes
¶ Returns the collection of planes defining all the intersections on the profiles and plates.
-------------------------------------
Getter Method
Signature
GridPlanes()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX8.0.0.
License requirements: None.
UseExistingCuttingSideFace¶
-
MarkingLineDesignBuilder.
UseExistingCuttingSideFace
¶ Returns or sets the option to decide if the current cutting side faces are used(true) or if the cutting side faces should be recalculated(false).
-------------------------------------
Getter Method
Signature
UseExistingCuttingSideFace()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseExistingCuttingSideFace(useExistingCuttingSideFace)
Parameters: useExistingCuttingSideFace (bool) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Method Detail¶
GetMarkingLineInformation¶
-
MarkingLineDesignBuilder.
GetMarkingLineInformation
¶ Get the information from the marking line feature to create a fillet type welding joint.
Specifically the target and placement faces
Signature
GetMarkingLineInformation(curve)
Parameters: curve ( NXOpen.ICurve
) –- Marking line curve.
Returns: a tuple Return type: A tuple consisting of (placementFaces, targetFaces). placementFaces is a list of NXOpen.Face
. (OF) - a set of cutting side faces that place marking line targetFaces is a list ofNXOpen.Face
. (OF) - a set of molding faces that generated the marking lineNew in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
IsMarkingLineFeature¶
-
MarkingLineDesignBuilder.
IsMarkingLineFeature
¶ Is the feature a marking line feature
Signature
IsMarkingLineFeature(frecTag)
Parameters: frecTag ( NXOpen.Features.Feature
) –- feature to check
Returns: - is a marking line feature
Return type: bool New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Validate¶
-
MarkingLineDesignBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.