PlatePreparationBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
PlatePreparationBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Used to create or edit a
NXOpen.Features.ShipDesign.PlatePreparation
feature.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreatePlatePreparationBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CalculationMethod | Returns or sets the calculation method defining methods to calculate shrinkage factors. |
CoordinateSystem | Returns or sets the coordinate system defining the origin as well as the X and Y axis for shrinkage. |
Length | Returns the expression containing the scale factor for the length direction (X). |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Width | Returns the expression containing the scale factor for the width direction (Y). |
XCount | Returns the expression containing the attached part count in x direction. |
XDirectionType | Returns or sets the option that determines how the X direction is created. |
XWidth | Returns the expression containing the width in x direction. |
YCount | Returns the expression containing the attached part count in y direction. |
YWidth | Returns the expression containing the width in y direction. |
Methods¶
Method | Description |
---|---|
AddPart | Add the part to the collection of parts to be unformed and scaled. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemovePart | Remove the part from the collection of parts to be unformed and scaled. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CalculationMethod¶
-
PlatePreparationBuilder.
CalculationMethod
¶ Returns or sets the calculation method defining methods to calculate shrinkage factors.
-------------------------------------
Getter Method
Signature
CalculationMethod()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CalculationMethod(calculationMethod)
Parameters: calculationMethod (int) – New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
CoordinateSystem¶
-
PlatePreparationBuilder.
CoordinateSystem
¶ Returns or sets the coordinate system defining the origin as well as the X and Y axis for shrinkage.
-------------------------------------
Getter Method
Signature
CoordinateSystem()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateSystem(coordinateSystem)
Parameters: coordinateSystem ( NXOpen.CoordinateSystem
) –New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Length¶
-
PlatePreparationBuilder.
Length
¶ Returns the expression containing the scale factor for the length direction (X).
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Width¶
-
PlatePreparationBuilder.
Width
¶ Returns the expression containing the scale factor for the width direction (Y).
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
XCount¶
-
PlatePreparationBuilder.
XCount
¶ Returns the expression containing the attached part count in x direction.
-------------------------------------
Getter Method
Signature
XCount()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
XDirectionType¶
-
PlatePreparationBuilder.
XDirectionType
¶ Returns or sets the option that determines how the X direction is created.
-------------------------------------
Getter Method
Signature
XDirectionType()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XDirectionType(xDirType)
Parameters: xDirType (int) – New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
XWidth¶
-
PlatePreparationBuilder.
XWidth
¶ Returns the expression containing the width in x direction.
-------------------------------------
Getter Method
Signature
XWidth()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
YCount¶
-
PlatePreparationBuilder.
YCount
¶ Returns the expression containing the attached part count in y direction.
-------------------------------------
Getter Method
Signature
YCount()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
YWidth¶
-
PlatePreparationBuilder.
YWidth
¶ Returns the expression containing the width in y direction.
-------------------------------------
Getter Method
Signature
YWidth()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Method Detail¶
AddPart¶
-
PlatePreparationBuilder.
AddPart
¶ Add the part to the collection of parts to be unformed and scaled.
Signature
AddPart(partName)
Parameters: partName (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
RemovePart¶
-
PlatePreparationBuilder.
RemovePart
¶ Remove the part from the collection of parts to be unformed and scaled.
Signature
RemovePart(partName)
Parameters: partName (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Validate¶
-
PlatePreparationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.