ShellTemplateBuilderMarkingTypes Enumeration¶
NXOpen.Features.ShipDesign.ShellTemplateBuilder.MarkingTypes is an alias for NXOpen.Features.ShipDesign.ShellTemplateBuilderMarkingTypes
-
class
NXOpen.Features.ShipDesign.
ShellTemplateBuilderMarkingTypes
¶ Bases:
object
The option for controlling which marking lines are drawn on the plate
Enum Members
Enum Member Enum Member Description None Do not draw template marking lines on plate.XDirectionOnly Draw X direction template marking lines on plate.YDirectionOnly Draw Y direction template marking lines on plate.XandYDirections Draw X and Y direction template marking lines on plate.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-