PlateBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
PlateBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.Plate
builder.This builder is used to create and edit ship plate feature. The plate feature can be created from construction curves, boundary faces or planes. And also a solid body cab be adopted as a plate.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreatePlateBuilder
Default values.
Property Value DistanceTolerance 0.0254 (millimeters part), 0.001 (inches part) MoldFaceOffset.Value 0 (millimeters part), 0 (inches part) PlateStock.KnuckleRatio 3.0 PlateStock.KnuckleSmoothAngle 3.0 PlateStock.MaterialOption 0 PlateStock.OppositeThickness.Value 0 (millimeters part), 0 (inches part) PlateStock.RestrictThicknessToMaterial true PlateStock.ThickenOption SingleSided PlateStock.Thickness.Value 10 (millimeters part), 0.5 (inches part) PlateStock.ThicknessSourceOption List RegionOption OutsideBody Tightness NonTight New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AdoptionBodies | Returns the adoption bodies, which are used to create multiple plates. |
AdoptionBodiesMoldFace | Returns the mold face of adoption bodies. |
BodyBoundary | Returns the body boundary, which can be mixed with curve, face and plane to define the plate boundary. |
CurveBoundary | Returns the curve boundary, which can be a single region or multiple regions. |
DistanceTolerance | Returns or sets the distance tolerance. |
FacePlaneBoundary | Returns the face, plane boundary, which defines a list of trimming objects with offset values. |
FlipDirection | Returns or sets the flip direction, which can change the plate thickness direction. |
MoldFace | Returns the mold face, which is used to create the plate body and define the plate placement. |
MoldFaceOffset | Returns the mold face offset, which defines an offset distance to the mold face. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlateStock | Returns the plate stock builder, which defines the plate material, grade, thickness, mass density, thicken option and opposite thickness. |
ProjectDirection | Returns the project direction, which is used to project the boundary curves to the plate mold face. |
RegionOption | Returns or sets the region option, which defines the plate areas in case of body faces as plate boundary. |
RegionPoint | Returns or sets the region point, which is used to identify the plate region. |
Regions | Returns the regions to create plates |
SplitKnuckleEdges | Returns the split knuckle edges, which are used to split a plate into separate knuckle parts. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tightness | Returns or sets the tightness, which defines the plate is tight (air tight, oil tight, water tight) or non tight. |
Type | Returns or sets the plate type, which is creation or adoption. |
Methods¶
Method | Description |
---|---|
AddRegionPoint | Adds a region point. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateRegions | Creates regions to output the selected plates. |
DeleteRegions | Deletes regions |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetMultipleRegionPoints | Gets multiple region points. |
GetObject | Returns the object currently being edited by this builder. |
GetShowMigratedBody | Gets the show migrated body flag. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
MapRegionToRegionPoint | Maps the user selected plate region to a region point. |
RemoveAllRegionPoints | Removes all region points. |
RemoveRegionPoint | Removes a region point. |
SetKnuckleEdges | Sets the knuckle edges, which include edges for both bend and split types. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetShowMigratedBody | Sets the show migrated body flag. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PlateBuilderBodyTypes Enumeration | Settings to indicate the plate output body type. |
PlateBuilderRegionOptions Enumeration | Settings to indicate what areas to create the plate when using body faces as boundaries. |
PlateBuilderTightnessOptions Enumeration | Settings to indicate what tightness to create the plate. |
PlateBuilderTypes Enumeration | Settings to indicate how the plate is generated. |
Property Detail¶
AdoptionBodies¶
-
PlateBuilder.
AdoptionBodies
¶ Returns the adoption bodies, which are used to create multiple plates.
Each plate has a single body.
-------------------------------------
Getter Method
Signature
AdoptionBodies()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.0.0.
License requirements: None.
AdoptionBodiesMoldFace¶
-
PlateBuilder.
AdoptionBodiesMoldFace
¶ Returns the mold face of adoption bodies.
-------------------------------------
Getter Method
Signature
AdoptionBodiesMoldFace()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
BodyBoundary¶
-
PlateBuilder.
BodyBoundary
¶ Returns the body boundary, which can be mixed with curve, face and plane to define the plate boundary.
-------------------------------------
Getter Method
Signature
BodyBoundary()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.0.0.
License requirements: None.
CurveBoundary¶
-
PlateBuilder.
CurveBoundary
¶ Returns the curve boundary, which can be a single region or multiple regions.
In case of multiple regions, it creates multiple plates.
-------------------------------------
Getter Method
Signature
CurveBoundary()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
DistanceTolerance¶
-
PlateBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
FacePlaneBoundary¶
-
PlateBuilder.
FacePlaneBoundary
¶ Returns the face, plane boundary, which defines a list of trimming objects with offset values.
-------------------------------------
Getter Method
Signature
FacePlaneBoundary()
Returns: Return type: NXOpen.ExpressionCollectorSetList
New in version NX8.0.0.
License requirements: None.
FlipDirection¶
-
PlateBuilder.
FlipDirection
¶ Returns or sets the flip direction, which can change the plate thickness direction.
-------------------------------------
Getter Method
Signature
FlipDirection()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipDirection(flipDirection)
Parameters: flipDirection (bool) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
MoldFace¶
-
PlateBuilder.
MoldFace
¶ Returns the mold face, which is used to create the plate body and define the plate placement.
-------------------------------------
Getter Method
Signature
MoldFace()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
MoldFaceOffset¶
-
PlateBuilder.
MoldFaceOffset
¶ Returns the mold face offset, which defines an offset distance to the mold face.
-------------------------------------
Getter Method
Signature
MoldFaceOffset()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
PlateStock¶
-
PlateBuilder.
PlateStock
¶ Returns the plate stock builder, which defines the plate material, grade, thickness, mass density, thicken option and opposite thickness.
-------------------------------------
Getter Method
Signature
PlateStock()
Returns: Plate Stock Builder Return type: NXOpen.Features.ShipDesign.PlateStockBuilder
New in version NX8.0.0.
License requirements: None.
ProjectDirection¶
-
PlateBuilder.
ProjectDirection
¶ Returns the project direction, which is used to project the boundary curves to the plate mold face.
-------------------------------------
Getter Method
Signature
ProjectDirection()
Returns: Projection Options data Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX8.0.0.
License requirements: None.
RegionOption¶
-
PlateBuilder.
RegionOption
¶ Returns or sets the region option, which defines the plate areas in case of body faces as plate boundary.
-------------------------------------
Getter Method
Signature
RegionOption()
Returns: Return type: NXOpen.Features.ShipDesign.PlateBuilderRegionOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RegionOption(regionOption)
Parameters: regionOption ( NXOpen.Features.ShipDesign.PlateBuilderRegionOptions
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
RegionPoint¶
-
PlateBuilder.
RegionPoint
¶ Returns or sets the region point, which is used to identify the plate region.
-------------------------------------
Getter Method
Signature
RegionPoint()
Returns: Return type: NXOpen.Point3d
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
RegionPoint(regionPoint)
Parameters: regionPoint ( NXOpen.Point3d
) –New in version NX9.0.3.
License requirements: nx_ship_detail (“Ship Detail Design”)
Regions¶
-
PlateBuilder.
Regions
¶ Returns the regions to create plates
-------------------------------------
Getter Method
Signature
Regions()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
SplitKnuckleEdges¶
-
PlateBuilder.
SplitKnuckleEdges
¶ Returns the split knuckle edges, which are used to split a plate into separate knuckle parts.
-------------------------------------
Getter Method
Signature
SplitKnuckleEdges()
Returns: Return type: NXOpen.SelectEdgeList
New in version NX9.0.0.
License requirements: None.
Tightness¶
-
PlateBuilder.
Tightness
¶ Returns or sets the tightness, which defines the plate is tight (air tight, oil tight, water tight) or non tight.
-------------------------------------
Getter Method
Signature
Tightness()
Returns: Return type: NXOpen.Features.ShipDesign.PlateBuilderTightnessOptions
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tightness(tightness)
Parameters: tightness ( NXOpen.Features.ShipDesign.PlateBuilderTightnessOptions
) –New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Type¶
-
PlateBuilder.
Type
¶ Returns or sets the plate type, which is creation or adoption.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.ShipDesign.PlateBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.ShipDesign.PlateBuilderTypes
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Method Detail¶
AddRegionPoint¶
-
PlateBuilder.
AddRegionPoint
¶ Adds a region point.
If there are multiple region points, do a loop to add one by one.
Signature
AddRegionPoint(regionPoint)
Parameters: regionPoint ( NXOpen.Point3d
) –New in version NX10.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
CreateRegions¶
-
PlateBuilder.
CreateRegions
¶ Creates regions to output the selected plates.
Signature
CreateRegions()
Returns: Region Bodies Return type: list of NXOpen.Body
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
DeleteRegions¶
-
PlateBuilder.
DeleteRegions
¶ Deletes regions
Signature
DeleteRegions()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
GetMultipleRegionPoints¶
-
PlateBuilder.
GetMultipleRegionPoints
¶ Gets multiple region points.
Signature
GetMultipleRegionPoints()
Returns: Return type: list of NXOpen.Point3d
New in version NX10.0.0.
License requirements: None.
GetShowMigratedBody¶
-
PlateBuilder.
GetShowMigratedBody
¶ Gets the show migrated body flag.
Reserved for administrator use only.
Signature
GetShowMigratedBody()
Returns: Return type: bool New in version NX8.5.3.
License requirements: None.
MapRegionToRegionPoint¶
-
PlateBuilder.
MapRegionToRegionPoint
¶ Maps the user selected plate region to a region point.
Signature
MapRegionToRegionPoint(plateRegionString, regionPoint)
Parameters: - plateRegionString (str) –
- regionPoint (
NXOpen.Point3d
) –
New in version NX10.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
RemoveAllRegionPoints¶
-
PlateBuilder.
RemoveAllRegionPoints
¶ Removes all region points.
Signature
RemoveAllRegionPoints()
New in version NX10.0.0.
License requirements: None.
RemoveRegionPoint¶
-
PlateBuilder.
RemoveRegionPoint
¶ Removes a region point.
Plate will find the region body by the input region point and remove the cached region point.
Signature
RemoveRegionPoint(regionPoint)
Parameters: regionPoint ( NXOpen.Point3d
) –New in version NX10.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
SetKnuckleEdges¶
-
PlateBuilder.
SetKnuckleEdges
¶ Sets the knuckle edges, which include edges for both bend and split types.
Signature
SetKnuckleEdges(knuckleEdges)
Parameters: knuckleEdges (list of NXOpen.Edge
) – G0 edgesNew in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
SetShowMigratedBody¶
-
PlateBuilder.
SetShowMigratedBody
¶ Sets the show migrated body flag.
Reserved for administrator use only.
Signature
SetShowMigratedBody(showMigratedBody)
Parameters: showMigratedBody (bool) – New in version NX8.5.3.
License requirements: nx_ship_detail (“Ship Detail Design”)
Validate¶
-
PlateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.