ProjectionOptions Class¶
-
class
NXOpen.GeometricUtilities.
ProjectionOptions
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a ProjectionOptions
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ProjectDirectionMethod | Returns or sets the Projection direction method |
ProjectVector | Returns or sets the Projection vector |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ProjectionOptionsDirectionType Enumeration | This enum represents the projection direction types |
Property Detail¶
ProjectDirectionMethod¶
-
ProjectionOptions.
ProjectDirectionMethod
¶ Returns or sets the Projection direction method
-------------------------------------
Getter Method
Signature
ProjectDirectionMethod()
Returns: 0: Face normal; 1: Vector constructor Return type: NXOpen.GeometricUtilities.ProjectionOptionsDirectionType
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectDirectionMethod(projectDirectionMethod)
Parameters: projectDirectionMethod ( NXOpen.GeometricUtilities.ProjectionOptionsDirectionType
) – 0: Face normal; 1: Vector constructorNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
ProjectVector¶
-
ProjectionOptions.
ProjectVector
¶ Returns or sets the Projection vector
-------------------------------------
Getter Method
Signature
ProjectVector()
Returns: Direction Return type: NXOpen.Direction
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectVector(projectDirection)
Parameters: projectDirection ( NXOpen.Direction
) – DirectionNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
ProjectionOptions.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.