SplitStandardPartBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
SplitStandardPartBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ShipDesign.SplitStandardPartBuilder
.This class is for splitting ship standard part
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateSplitStandardPartBuilder
Default values.
Property Value AngularTolerance 0.5 BaseCornerCut.DistanceTolerance 0.0254 (millimeters part), 0.001 (inches part) DistanceTolerance 0.0254 LocationOffset.Value 0 (millimeters part), 0 (inches part) OrientationAngle.Value 0 ReinforceOffset.Value 0 (millimeters part), 0 (inches part) SplitReinforcement 1 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AngularTolerance | Returns or sets the tolerance, in degrees, used to determine when angles are zero. |
BaseCornerCut | Returns the corner cut at the base point on the standard part. |
DistanceTolerance | Returns or sets the tolerance used to determine when distances are considered zero. |
LocationOffset | Returns the offset value to the split location on the standard part base. |
OrientationAngle | Returns the orientation angle relative to the split curve or plane to split the standard part. |
ReinforceOffset | Returns the offset value to the split location on the standard part reinforcement. |
ReinforcementCornerCut | Returns the corner cut at the reinforcement point. |
ReverseSplitDirection | Returns or sets the flag to indicate whether to reverse the split direction or not. |
SplitReinforcement | Returns or sets the flag to indicate whether to split the reinforcement part on the standard part. |
Tag | Returns the Tag for this object. |
ToolCurve | Returns the tool curve which used to split the standard part. |
ToolFacePlane | Returns the tool face or plane used to split the standard part. |
ToolType | Returns or sets the split tool type to split the standard part. |
WeldCharacteristics | Returns the weld characteristics assigned to the split edges. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
ConvertObjectsToAdd | Converts the selected objects to acceptable one and add to the selection list. |
ConvertObjectsToRemove | Converts the selected objects to acceptable one and remove it from the selection list. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Reset | Resets the calculation results of standard part split when tool object changes. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SplitStandardPartBuilderToolTypes Enumeration | Represents the split tool types. |
Property Detail¶
AngularTolerance¶
-
SplitStandardPartBuilder.
AngularTolerance
¶ Returns or sets the tolerance, in degrees, used to determine when angles are zero.
-------------------------------------
Getter Method
Signature
AngularTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularTolerance(angularTolerance)
Parameters: angularTolerance (float) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
BaseCornerCut¶
-
SplitStandardPartBuilder.
BaseCornerCut
¶ Returns the corner cut at the base point on the standard part.
-------------------------------------
Getter Method
Signature
BaseCornerCut()
Returns: Return type: NXOpen.Features.ShipDesign.CornerCutBuilder
New in version NX9.0.0.
License requirements: None.
DistanceTolerance¶
-
SplitStandardPartBuilder.
DistanceTolerance
¶ Returns or sets the tolerance used to determine when distances are considered zero.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
LocationOffset¶
-
SplitStandardPartBuilder.
LocationOffset
¶ Returns the offset value to the split location on the standard part base.
-------------------------------------
Getter Method
Signature
LocationOffset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
OrientationAngle¶
-
SplitStandardPartBuilder.
OrientationAngle
¶ Returns the orientation angle relative to the split curve or plane to split the standard part.
-------------------------------------
Getter Method
Signature
OrientationAngle()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReinforceOffset¶
-
SplitStandardPartBuilder.
ReinforceOffset
¶ Returns the offset value to the split location on the standard part reinforcement.
-------------------------------------
Getter Method
Signature
ReinforceOffset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReinforcementCornerCut¶
-
SplitStandardPartBuilder.
ReinforcementCornerCut
¶ Returns the corner cut at the reinforcement point.
-------------------------------------
Getter Method
Signature
ReinforcementCornerCut()
Returns: Return type: NXOpen.Features.ShipDesign.CornerCutBuilder
New in version NX9.0.0.
License requirements: None.
ReverseSplitDirection¶
-
SplitStandardPartBuilder.
ReverseSplitDirection
¶ Returns or sets the flag to indicate whether to reverse the split direction or not.
-------------------------------------
Getter Method
Signature
ReverseSplitDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseSplitDirection(reverseSplitDirection)
Parameters: reverseSplitDirection (bool) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SplitReinforcement¶
-
SplitStandardPartBuilder.
SplitReinforcement
¶ Returns or sets the flag to indicate whether to split the reinforcement part on the standard part.
-------------------------------------
Getter Method
Signature
SplitReinforcement()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SplitReinforcement(splitReinforcement)
Parameters: splitReinforcement (bool) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ToolCurve¶
-
SplitStandardPartBuilder.
ToolCurve
¶ Returns the tool curve which used to split the standard part.
-------------------------------------
Getter Method
Signature
ToolCurve()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
ToolFacePlane¶
-
SplitStandardPartBuilder.
ToolFacePlane
¶ Returns the tool face or plane used to split the standard part.
-------------------------------------
Getter Method
Signature
ToolFacePlane()
Returns: Return type: NXOpen.SelectNXObject
New in version NX9.0.0.
License requirements: None.
ToolType¶
-
SplitStandardPartBuilder.
ToolType
¶ Returns or sets the split tool type to split the standard part.
-------------------------------------
Getter Method
Signature
ToolType()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolType(toolType)
Parameters: toolType (int) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
WeldCharacteristics¶
-
SplitStandardPartBuilder.
WeldCharacteristics
¶ Returns the weld characteristics assigned to the split edges.
-------------------------------------
Getter Method
Signature
WeldCharacteristics()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
ConvertObjectsToAdd¶
-
SplitStandardPartBuilder.
ConvertObjectsToAdd
¶ Converts the selected objects to acceptable one and add to the selection list.
Signature
ConvertObjectsToAdd(selectedObjectTags)
Parameters: selectedObjectTags (list of NXOpen.DisplayableObject
) –New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ConvertObjectsToRemove¶
-
SplitStandardPartBuilder.
ConvertObjectsToRemove
¶ Converts the selected objects to acceptable one and remove it from the selection list.
Signature
ConvertObjectsToRemove(selectedObjectTags)
Parameters: selectedObjectTags (list of NXOpen.DisplayableObject
) –New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
Reset¶
-
SplitStandardPartBuilder.
Reset
¶ Resets the calculation results of standard part split when tool object changes.
Signature
Reset()
New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
Validate¶
-
SplitStandardPartBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.