AnchorPointList Class¶
-
class
NXOpen.Features.ShipDesign.
AnchorPointList
¶ Bases:
NXOpen.TaggedObject
Represents a list of objects.
To create a new instance of this class, use
NXOpen.Part.CreateObjectList
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Length | Returns the length of the list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Append | Appends a set of objects to the list |
Clear | Clears the entire list |
ClearIndex | Deletes the item at the index specified. |
Erase | Erases the object from the list, but does not delete the object. |
FindIndex | Finds the index where the input object appears. |
FindItem | Returns the object at the input index. |
GetContents | Gets the contents of the entire list @return The list contents |
Insert | Inserts an object at the specified location |
MoveToBottom | Move object at the specified location to the bottom of the list. |
MoveToTop | Move object at the specified location to the top of the list. |
SetContents | Sets the contents of the entire list. |
Swap | Exchanges the position of two objects inside the list. |
Property Detail¶
Method Detail¶
Append¶
-
AnchorPointList.
Append
¶ Overloaded method Append
Append(objects)
Append(object)
-------------------------------------
Appends a set of objects to the list
Signature
Append(objects)
Parameters: objects (list of NXOpen.Features.ShipDesign.AnchorPoint
) – items to appendNew in version NX4.0.0.
License requirements: None.
-------------------------------------
Appends an object to the list
Signature
Append(object)
Parameters: object ( NXOpen.Features.ShipDesign.AnchorPoint
) – item to appendNew in version NX5.0.0.
License requirements: None.
-------------------------------------
Clear¶
-
AnchorPointList.
Clear
¶ Overloaded method Clear
Clear()
Clear(deleteOption)
-------------------------------------
Clears the entire list
Signature
Clear()
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Clears the entire list
Signature
Clear(deleteOption)
Parameters: deleteOption ( NXOpen.ObjectListDeleteOption
) – whether to delete the objects when removing themNew in version NX5.0.0.
License requirements: None.
-------------------------------------
ClearIndex¶
-
AnchorPointList.
ClearIndex
¶ Deletes the item at the index specified.
The size of the list does * not change, but the item at this index is set to NULL.
Signature
ClearIndex(deleteIdx)
Parameters: deleteIdx (int) – index of item to be deleted New in version NX4.0.0.
License requirements: None.
Erase¶
-
AnchorPointList.
Erase
¶ Overloaded method Erase
Erase(index)
Erase(index, deleteOption)
Erase(obj)
Erase(obj, deleteOption)
-------------------------------------
Erases the object from the list, but does not delete the object. The list is shifted so that there isn’t a null where the object used to be.
Signature
Erase(index)
Parameters: index (int) – index of item to be removed from the list New in version NX5.0.0.
License requirements: None.
-------------------------------------
Erases the object at the given position from the list. The list is shifted so that there isn’t a null where the object used to be.
Signature
Erase(index, deleteOption)
Parameters: - index (int) – index of item to be removed from the list
- deleteOption (
NXOpen.ObjectListDeleteOption
) – whether to delete the object
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Erases the object from the list, but does not delete the object. The list is shifted so that there isn’t a null where the object used to exist.
Signature
Erase(obj)
Parameters: obj ( NXOpen.Features.ShipDesign.AnchorPoint
) – object to be removed from the listNew in version NX5.0.0.
License requirements: None.
-------------------------------------
Erases the object from the list. The list is shifted so that there isn’t a null where the object used to exist.
Signature
Erase(obj, deleteOption)
Parameters: - obj (
NXOpen.Features.ShipDesign.AnchorPoint
) – object to be removed from the list - deleteOption (
NXOpen.ObjectListDeleteOption
) – whether to delete the object
New in version NX5.0.0.
License requirements: None.
-------------------------------------
FindIndex¶
-
AnchorPointList.
FindIndex
¶ Finds the index where the input object appears.
If it does not appear, * -1 is returned.
Signature
FindIndex(obj)
Parameters: obj ( NXOpen.Features.ShipDesign.AnchorPoint
) – Object to find index forReturns: index of input object, -1 if not on list Return type: int New in version NX4.0.0.
License requirements: None.
FindItem¶
-
AnchorPointList.
FindItem
¶ Returns the object at the input index.
May be NULL.
Signature
FindItem(index)
Parameters: index (int) – index of object to return Returns: object found at input index Return type: NXOpen.Features.ShipDesign.AnchorPoint
New in version NX4.0.0.
License requirements: None.
GetContents¶
-
AnchorPointList.
GetContents
¶ Gets the contents of the entire list
Signature
GetContents()
Returns: The list contents Return type: list of NXOpen.Features.ShipDesign.AnchorPoint
New in version NX5.0.0.
License requirements: None.
Insert¶
-
AnchorPointList.
Insert
¶ Inserts an object at the specified location
Signature
Insert(location, object)
Parameters: - location (int) – location at which to insert the object
- object (
NXOpen.Features.ShipDesign.AnchorPoint
) – object to be inserted
New in version NX5.0.0.
License requirements: None.
MoveToBottom¶
-
AnchorPointList.
MoveToBottom
¶ Move object at the specified location to the bottom of the list.
Signature
MoveToBottom(index)
Parameters: index (int) – location of the item New in version NX10.0.0.
License requirements: None.
MoveToTop¶
-
AnchorPointList.
MoveToTop
¶ Move object at the specified location to the top of the list.
Signature
MoveToTop(index)
Parameters: index (int) – location of the item New in version NX10.0.0.
License requirements: None.
SetContents¶
-
AnchorPointList.
SetContents
¶ Sets the contents of the entire list.
This overwrites the previous contents of this list, but does not delete any objects that were originally on the list.
Signature
SetContents(objects)
Parameters: objects (list of NXOpen.Features.ShipDesign.AnchorPoint
) – The list contentsNew in version NX5.0.0.
License requirements: None.
Swap¶
-
AnchorPointList.
Swap
¶ Overloaded method Swap
Swap(index1, index2)
Swap(object1, object2)
-------------------------------------
Exchanges the position of two objects inside the list. The first object is placed where the second used to be, and second object where the first used to be.
Signature
Swap(index1, index2)
Parameters: - index1 (int) – location of the first item
- index2 (int) – location of the second item
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Exchanges the position of two objects inside the list. The first object is placed where the second used to be, and second object where the first used to be.
Signature
Swap(object1, object2)
Parameters: - object1 (
NXOpen.Features.ShipDesign.AnchorPoint
) – first item - object2 (
NXOpen.Features.ShipDesign.AnchorPoint
) – second item
New in version NX5.0.0.
License requirements: None.
-------------------------------------