SetModeBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
SetModeBuilder
¶ Bases:
NXOpen.Builder
This class is used to set the mode to design or manufacturing.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateSetModeBuilder
Default values.
Property Value ManufacturingDesignMode DesignMode New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DesignElementToSetMode | Returns the design element selection object to be processed in the change of mode processing. |
ManufacturingDesignMode | Returns or sets the manufacturing and design mode. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetMode | Loops through all the parts and sets mode to design or manufacturing @return |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SetModeBuilderDesMfgMode Enumeration | Manufacturing Mode type. |
Property Detail¶
DesignElementToSetMode¶
-
SetModeBuilder.
DesignElementToSetMode
¶ Returns the design element selection object to be processed in the change of mode processing.
-------------------------------------
Getter Method
Signature
DesignElementToSetMode()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
ManufacturingDesignMode¶
-
SetModeBuilder.
ManufacturingDesignMode
¶ Returns or sets the manufacturing and design mode.
-------------------------------------
Getter Method
Signature
ManufacturingDesignMode()
Returns: Return type: NXOpen.Features.ShipDesign.SetModeBuilderDesMfgMode
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ManufacturingDesignMode(manufacturingDesignMode)
Parameters: manufacturingDesignMode ( NXOpen.Features.ShipDesign.SetModeBuilderDesMfgMode
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Method Detail¶
SetMode¶
-
SetModeBuilder.
SetMode
¶ Loops through all the parts and sets mode to design or manufacturing
Signature
SetMode()
Returns: Return type: int New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Validate¶
-
SetModeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.