BulkHeadsBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
BulkHeadsBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.BulkHeads
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateBulkHeadsBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AutoBulkHeadName | Returns or sets the bulkHead name. |
AutoNameToggle | Returns or sets the auto name toggle. |
BulkHeadList | Returns the bulkHead list. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the bulkhead type. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateBulkheadListItem | Create a list to generate a single bulkHead. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BulkHeadsBuilderBulkheadType Enumeration | Represents the bulkhead type. |
Property Detail¶
AutoBulkHeadName¶
-
BulkHeadsBuilder.
AutoBulkHeadName
¶ Returns or sets the bulkHead name.
-------------------------------------
Getter Method
Signature
AutoBulkHeadName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoBulkHeadName(bulkHeadName)
Parameters: bulkHeadName (str) – New in version NX5.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
AutoNameToggle¶
-
BulkHeadsBuilder.
AutoNameToggle
¶ Returns or sets the auto name toggle.
-------------------------------------
Getter Method
Signature
AutoNameToggle()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoNameToggle(autoNameToggle)
Parameters: autoNameToggle (bool) – New in version NX5.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
BulkHeadList¶
-
BulkHeadsBuilder.
BulkHeadList
¶ Returns the bulkHead list.
-------------------------------------
Getter Method
Signature
BulkHeadList()
Returns: Return type: NXOpen.Features.ShipDesign.BulkHeadListItemBuilderList
New in version NX5.0.0.
License requirements: None.
Type¶
-
BulkHeadsBuilder.
Type
¶ Returns or sets the bulkhead type.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.ShipDesign.BulkHeadsBuilderBulkheadType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.ShipDesign.BulkHeadsBuilderBulkheadType
) –New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
CreateBulkheadListItem¶
-
BulkHeadsBuilder.
CreateBulkheadListItem
¶ Create a list to generate a single bulkHead.
Signature
CreateBulkheadListItem(bulkheadsType)
Parameters: bulkheadsType ( NXOpen.Features.ShipDesign.BulkHeadsBuilderBulkheadType
) –Returns: Return type: NXOpen.Features.ShipDesign.BulkHeadListItemBuilder
New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Validate¶
-
BulkHeadsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.