ShipnameFieldBuilderType Enumeration¶
-
class
NXOpen.Features.ShipDesign.
ShipnameFieldBuilderType
¶ Bases:
object
Field Type Enum Members
Enum Member Enum Member Description Fixed Field with an unchanging stringOption Field whose value can be one of several stringsIndex Field which will have a number generatedAny Field whose value will be a user enterred stringNone Unknown Field Type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-