StiffenerSystemBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
StiffenerSystemBuilder
¶ Bases:
NXOpen.Features.ShipDesign.ProfileSystemBuilder
This class is used to create or edit a
NXOpen.Features.ShipDesign.StiffenerSystem
feature.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateStiffenerSystemBuilder
Default values.
Property Value EndCutEnd Connected EndCutStart Connected MeasureAlongMode AlongSurfaceLength MountingMethod NoOffset OffsetDistance.Value 0 (millimeters part), 0 (inches part) OffsetDistanceEnd.Value 0 (millimeters part), 0 (inches part) OffsetDistanceStart.Value 0 (millimeters part), 0 (inches part) OffsetNumber 0 OffsetSpacing.Value 0 (millimeters part), 0 (inches part) OffsetSpacingEnd.Value 0 (millimeters part), 0 (inches part) OffsetSpacingMode Single OffsetSpacingStart.Value 0 (millimeters part), 0 (inches part) OrientationAngle.Value 0 (millimeters part), 0 (inches part) OrientationDefinitionBuilder.MeasureAngles NormaltoCurve OrientationDefinitionBuilder.ShowSurfaceAngles 0 OrientationDefinitionBuilder.ShowTwistRate 0 OrientationDefinitionBuilder.ShowWebAngles 0 OrientationMethod FaceNormal StiffenerBySupportPathData.LengthParams.Value 300 (millimeters part), 100 (inches part) StiffenerBySupportPathData.OrientationBySupport 0 StockData.AnchorPoint 0 StockData.PlateHeight.Value 50 (millimeters part), 2 (inches part) StockData.PlateStockData.KnuckleRatio 3.0 StockData.PlateStockData.KnuckleSmoothAngle 3.0 StockData.PlateStockData.MaterialOption 0 StockData.PlateStockData.OppositeThickness.Value 0 (millimeters part), 0 (inches part) StockData.PlateStockData.RestrictThicknessToMaterial true StockData.PlateStockData.ThickenOption SingleSided StockData.PlateStockData.Thickness.Value 10 (millimeters part), 0.5 (inches part) StockData.PlateStockData.ThicknessSourceOption List StockData.SectionType Profile Type Curves New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the tolerance, in degrees, used to determine when angles are zero. |
ApplyFlangeSetback | Returns or sets the flange set back option for stiffener by support, which indicates if the flange set back should be applied or not |
ApplyWebSetback | Returns or sets the web set back option for stiffener by support, which indicates if the web set back should be applied or not |
Boundary1 | Returns the collector containing the plate system, profile system, or datum plane that will be used to trim the first end of the generated profile system. |
Boundary1Plane | Returns or sets the defined plane that will be used to trim the first end of the generated profile system. |
Boundary2 | Returns the collector containing the plate system, profile system, or datum plane that will be used to trim the second end of the generated profile system. |
Boundary2Plane | Returns or sets the defined plane that will be used to trim the second end of the generated profile system. |
BoundaryReverse | Returns or sets the indication if the side of a single boundary should be changed to the other side or not. |
ConnectAngle | Returns or sets the connect angle of stiffener by support in degrees, negative value is not allowed |
Curves | Returns the curves selected that define the path of the stiffener system. |
DistanceTolerance | Returns or sets the tolerance used to determine when distances are considered zero. |
EndCutEnd | Returns or sets the end cut to use at the end of the complete stiffener system. |
EndCutStart | Returns or sets the end cut to use at the start of the complete stiffener system. |
FirstIntersectionPoints | Returns the selected intersection points between the curves and the first boundary. |
MeasureAlongMode | Returns or sets the method used to measure distances between planes. |
MountingMethod | Returns or sets the mounting method |
OffsetDistance | Returns the distance from the OffsetPlane to generate the first plane. |
OffsetDistanceEnd | Returns the distance from the OffsetPlane to generate the location at the end of the stiffener system. |
OffsetDistanceStart | Returns the distance from the OffsetPlane to generate the location at the start of the stiffener system. |
OffsetNumber | Returns or sets the number of offset planes to generate that define the path of the stiffener system. |
OffsetPlane | Returns or sets the first plane of the set of offset planes that define the path of the stiffener system. |
OffsetSpacing | Returns the distance between generated planes. |
OffsetSpacingEnd | Returns the distance between generated locations at the end of the stiffener system. |
OffsetSpacingMode | Returns or sets the indication whether spacing of the offset planes is defined at each end of the stiffener system, or if a constant spacing is desired. |
OffsetSpacingStart | Returns the distance between generated locations at the start of the stiffener system. |
OrientationAngle | Returns the angle at which the stiffener system is placed relative to the reference. |
OrientationAngleRule | Returns or sets the angle rule to use when measuring angles. |
OrientationDefinitionBuilder | Returns the builder used to define the orientation for the stiffener system. |
OrientationMethod | Returns or sets the method used to define the reference for the orientation angle of stiffener system. |
OrientationVector | Returns or sets the vector specified for the orientation angle reference. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlaneList | Returns the list of defined planes that define the path of the stiffener system. |
PlanePairList | Returns the list of pairs of planes that generate points on the ship structure to define the path of the stiffener system. |
Planes | Returns the planes selected that define the path of the stiffener system. |
PointList | Returns the list of selected or defined points that define the path of the stiffener system. |
PointMethod | Returns or sets the method used to define the generated points on the ship structure to define the path of the stiffener system. |
ProjectionDirection | Returns the direction used to project the stiffener path object |
Reverse | Returns or sets the indication whether the direction of the stiffener flange should be reversed. |
SecondIntersectionPoints | Returns the selected intersection points between the curves and the second boundary. |
ShipNames | Returns the Ship Names builder, used to assign names to the Stiffener Systems created. |
ShipStructure | Returns the ship structure upon which to create the stiffener system. |
StiffenerBySupportPathData | Returns the path data used to define the support information of the stiffener. |
StockData | Returns the stock data used to define the stock information of the stiffener. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
SwitchSide | Returns or sets the indication whether the side of the ship structure should be switched. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the method used to define the path of the stiffener system. |
Weld | Returns the builder used to specify the welding characteristics for the stiffener system. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreatePathCurves | Creates path curves for all the paths of the profile system. |
CreatePlaneForList | Create a NXOpen.Features.ShipDesign.PlaneListBuilder to add a defined plane to a list. |
CreatePlanePairBuilder | Creates a NXOpen.Features.ShipDesign.PlanePairBuilder to add another pair of planes to the list. |
DeleteLastPathCurves | Deletes the path curves returned from a call to GetLastPathCurves . |
DeletePathCurves | Deletes the path curves created from a call to CreatePathCurves . |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetLastPathCurves | Gets the path curves used by NXOpen.Features.ShipDesign.OrientationDefinitionBuilder . |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetBoundaryOnePoints | Sets the selected intersection points for the first boundary. |
SetBoundaryTwoPoints | Set the selected intersection points for the second boundary. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StiffenerSystemBuilderEndCutTypes Enumeration | Used to specify the type of end cut to be used at the extreme ends of the stiffener system. |
StiffenerSystemBuilderMeasureAlongModes Enumeration | Used to specify how the spacing and offset is to be measured. |
StiffenerSystemBuilderMountingMethods Enumeration | the mounting method offset type |
StiffenerSystemBuilderOffsetSpacingModes Enumeration | Used to specify if a single or double offset and spacing definition is to be used. |
StiffenerSystemBuilderOrientationMethods Enumeration | Used to specify the type of reference to use for specifying the orientation of the stiffener system. |
StiffenerSystemBuilderPointMethods Enumeration | Used to specify whether points or planes are being used for the points definition. |
StiffenerSystemBuilderTypes Enumeration | Used to specify how the path of the stiffener system is defined. |
Property Detail¶
ApplyFlangeSetback¶
-
StiffenerSystemBuilder.
ApplyFlangeSetback
¶ Returns or sets the flange set back option for stiffener by support, which indicates if the flange set back should be applied or not
-------------------------------------
Getter Method
Signature
ApplyFlangeSetback()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyFlangeSetback(applyFlangeSetback)
Parameters: applyFlangeSetback (bool) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ApplyWebSetback¶
-
StiffenerSystemBuilder.
ApplyWebSetback
¶ Returns or sets the web set back option for stiffener by support, which indicates if the web set back should be applied or not
-------------------------------------
Getter Method
Signature
ApplyWebSetback()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyWebSetback(applyWebSetback)
Parameters: applyWebSetback (bool) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ConnectAngle¶
-
StiffenerSystemBuilder.
ConnectAngle
¶ Returns or sets the connect angle of stiffener by support in degrees, negative value is not allowed
-------------------------------------
Getter Method
Signature
ConnectAngle()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConnectAngle(connectAngle)
Parameters: connectAngle (float) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Curves¶
-
StiffenerSystemBuilder.
Curves
¶ Returns the curves selected that define the path of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.Curves
.-------------------------------------
Getter Method
Signature
Curves()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
EndCutEnd¶
-
StiffenerSystemBuilder.
EndCutEnd
¶ Returns or sets the end cut to use at the end of the complete stiffener system.
-------------------------------------
Getter Method
Signature
EndCutEnd()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutEnd(endCutEnd)
Parameters: endCutEnd ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
EndCutStart¶
-
StiffenerSystemBuilder.
EndCutStart
¶ Returns or sets the end cut to use at the start of the complete stiffener system.
-------------------------------------
Getter Method
Signature
EndCutStart()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutStart(endCutStart)
Parameters: endCutStart ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
MeasureAlongMode¶
-
StiffenerSystemBuilder.
MeasureAlongMode
¶ Returns or sets the method used to measure distances between planes.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
.-------------------------------------
Getter Method
Signature
MeasureAlongMode()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderMeasureAlongModes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeasureAlongMode(measureAlongMode)
Parameters: measureAlongMode ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderMeasureAlongModes
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
MountingMethod¶
-
StiffenerSystemBuilder.
MountingMethod
¶ Returns or sets the mounting method
-------------------------------------
Getter Method
Signature
MountingMethod()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderMountingMethods
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MountingMethod(mountingMethod)
Parameters: mountingMethod ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderMountingMethods
) –New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
OffsetDistance¶
-
StiffenerSystemBuilder.
OffsetDistance
¶ Returns the distance from the OffsetPlane to generate the first plane.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
and OffsetSpacing isNXOpen.Features.ShipDesign.StiffenerSystemBuilderOffsetSpacingModes.Single
.-------------------------------------
Getter Method
Signature
OffsetDistance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OffsetDistanceEnd¶
-
StiffenerSystemBuilder.
OffsetDistanceEnd
¶ Returns the distance from the OffsetPlane to generate the location at the end of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
and OffsetSpacing isNXOpen.Features.ShipDesign.StiffenerSystemBuilderOffsetSpacingModes.Double
.-------------------------------------
Getter Method
Signature
OffsetDistanceEnd()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OffsetDistanceStart¶
-
StiffenerSystemBuilder.
OffsetDistanceStart
¶ Returns the distance from the OffsetPlane to generate the location at the start of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
and OffsetSpacing isNXOpen.Features.ShipDesign.StiffenerSystemBuilderOffsetSpacingModes.Double
.-------------------------------------
Getter Method
Signature
OffsetDistanceStart()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OffsetNumber¶
-
StiffenerSystemBuilder.
OffsetNumber
¶ Returns or sets the number of offset planes to generate that define the path of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
.-------------------------------------
Getter Method
Signature
OffsetNumber()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetNumber(number)
Parameters: number (int) – New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
OffsetPlane¶
-
StiffenerSystemBuilder.
OffsetPlane
¶ Returns or sets the first plane of the set of offset planes that define the path of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
.-------------------------------------
Getter Method
Signature
OffsetPlane()
Returns: Return type: NXOpen.Plane
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetPlane(offsetPlane)
Parameters: offsetPlane ( NXOpen.Plane
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
OffsetSpacing¶
-
StiffenerSystemBuilder.
OffsetSpacing
¶ Returns the distance between generated planes.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
and OffsetSpacing isNXOpen.Features.ShipDesign.StiffenerSystemBuilderOffsetSpacingModes.Single
.-------------------------------------
Getter Method
Signature
OffsetSpacing()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OffsetSpacingEnd¶
-
StiffenerSystemBuilder.
OffsetSpacingEnd
¶ Returns the distance between generated locations at the end of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
and OffsetSpacing isNXOpen.Features.ShipDesign.StiffenerSystemBuilderOffsetSpacingModes.Double
.-------------------------------------
Getter Method
Signature
OffsetSpacingEnd()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OffsetSpacingMode¶
-
StiffenerSystemBuilder.
OffsetSpacingMode
¶ Returns or sets the indication whether spacing of the offset planes is defined at each end of the stiffener system, or if a constant spacing is desired.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
.-------------------------------------
Getter Method
Signature
OffsetSpacingMode()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderOffsetSpacingModes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetSpacingMode(offsetSpacingMode)
Parameters: offsetSpacingMode ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderOffsetSpacingModes
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
OffsetSpacingStart¶
-
StiffenerSystemBuilder.
OffsetSpacingStart
¶ Returns the distance between generated locations at the start of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.OffsetPlanes
and OffsetSpacing isNXOpen.Features.ShipDesign.StiffenerSystemBuilderOffsetSpacingModes.Double
.-------------------------------------
Getter Method
Signature
OffsetSpacingStart()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OrientationAngle¶
-
StiffenerSystemBuilder.
OrientationAngle
¶ Returns the angle at which the stiffener system is placed relative to the reference.
-------------------------------------
Getter Method
Signature
OrientationAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OrientationDefinitionBuilder¶
-
StiffenerSystemBuilder.
OrientationDefinitionBuilder
¶ Returns the builder used to define the orientation for the stiffener system.
-------------------------------------
Getter Method
Signature
OrientationDefinitionBuilder()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationDefinitionBuilder
New in version NX9.0.0.
License requirements: None.
OrientationMethod¶
-
StiffenerSystemBuilder.
OrientationMethod
¶ Returns or sets the method used to define the reference for the orientation angle of stiffener system.
-------------------------------------
Getter Method
Signature
OrientationMethod()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationMethod(orientationMethod)
Parameters: orientationMethod ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
OrientationVector¶
-
StiffenerSystemBuilder.
OrientationVector
¶ Returns or sets the vector specified for the orientation angle reference.
Only used when when Method is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods.Vector
..-------------------------------------
Getter Method
Signature
OrientationVector()
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationVector(orientationVector)
Parameters: orientationVector ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
PlaneList¶
-
StiffenerSystemBuilder.
PlaneList
¶ Returns the list of defined planes that define the path of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.Planes
.-------------------------------------
Getter Method
Signature
PlaneList()
Returns: Return type: NXOpen.Features.ShipDesign.PlaneListBuilderList
New in version NX8.0.0.
License requirements: None.
PlanePairList¶
-
StiffenerSystemBuilder.
PlanePairList
¶ Returns the list of pairs of planes that generate points on the ship structure to define the path of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.Points
and PointMethod isNXOpen.Features.ShipDesign.StiffenerSystemBuilderPointMethods.Planes
.-------------------------------------
Getter Method
Signature
PlanePairList()
Returns: Return type: NXOpen.NXObjectList
New in version NX8.0.0.
License requirements: None.
Planes¶
-
StiffenerSystemBuilder.
Planes
¶ Returns the planes selected that define the path of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.Planes
.-------------------------------------
Getter Method
Signature
Planes()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
PointList¶
-
StiffenerSystemBuilder.
PointList
¶ Returns the list of selected or defined points that define the path of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.Points
and PointMethod isNXOpen.Features.ShipDesign.StiffenerSystemBuilderPointMethods.Points
.-------------------------------------
Getter Method
Signature
PointList()
Returns: Return type: NXOpen.NXObjectList
New in version NX8.0.0.
License requirements: None.
PointMethod¶
-
StiffenerSystemBuilder.
PointMethod
¶ Returns or sets the method used to define the generated points on the ship structure to define the path of the stiffener system.
Only used when Type is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes.Points
.-------------------------------------
Getter Method
Signature
PointMethod()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderPointMethods
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointMethod(method)
Parameters: method ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderPointMethods
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
ProjectionDirection¶
-
StiffenerSystemBuilder.
ProjectionDirection
¶ Returns the direction used to project the stiffener path object
-------------------------------------
Getter Method
Signature
ProjectionDirection()
Returns: Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX9.0.0.
License requirements: None.
Reverse¶
-
StiffenerSystemBuilder.
Reverse
¶ Returns or sets the indication whether the direction of the stiffener flange should be reversed.
The default direction is based on the ship structure that the stiffener is being built upon.
-------------------------------------
Getter Method
Signature
Reverse()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Reverse(reverse)
Parameters: reverse (bool) – New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
ShipNames¶
-
StiffenerSystemBuilder.
ShipNames
¶ Returns the Ship Names builder, used to assign names to the Stiffener Systems created.
-------------------------------------
Getter Method
Signature
ShipNames()
Returns: Ship Names Builder Return type: NXOpen.Features.ShipDesign.ShipNamesBuilder
New in version NX9.0.2.
License requirements: None.
ShipStructure¶
-
StiffenerSystemBuilder.
ShipStructure
¶ Returns the ship structure upon which to create the stiffener system.
-------------------------------------
Getter Method
Signature
ShipStructure()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
StiffenerBySupportPathData¶
-
StiffenerSystemBuilder.
StiffenerBySupportPathData
¶ Returns the path data used to define the support information of the stiffener.
-------------------------------------
Getter Method
Signature
StiffenerBySupportPathData()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBySupportPathBuilder
New in version NX9.0.0.
License requirements: None.
StockData¶
-
StiffenerSystemBuilder.
StockData
¶ Returns the stock data used to define the stock information of the stiffener.
-------------------------------------
Getter Method
Signature
StockData()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerStockBuilder
New in version NX8.0.0.
License requirements: None.
SwitchSide¶
-
StiffenerSystemBuilder.
SwitchSide
¶ Returns or sets the indication whether the side of the ship structure should be switched.
The default direction is based on the ship structure that the stiffener is being built upon.
-------------------------------------
Getter Method
Signature
SwitchSide()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SwitchSide(switchSide)
Parameters: switchSide (bool) – New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Type¶
-
StiffenerSystemBuilder.
Type
¶ Returns or sets the method used to define the path of the stiffener system.
Four types are supported: curves, planes, offset planes, and points.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderTypes
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Weld¶
-
StiffenerSystemBuilder.
Weld
¶ Returns the builder used to specify the welding characteristics for the stiffener system.
-------------------------------------
Getter Method
Signature
Weld()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
CreatePlanePairBuilder¶
-
StiffenerSystemBuilder.
CreatePlanePairBuilder
¶ Creates a
NXOpen.Features.ShipDesign.PlanePairBuilder
to add another pair of planes to the list.Signature
CreatePlanePairBuilder()
Returns: Return type: NXOpen.Features.ShipDesign.PlanePairBuilder
New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Validate¶
-
StiffenerSystemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.