EditStockBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
EditStockBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Used to create a
NXOpen.Features.ShipDesign.EditStockBuilder
which is used to change the stock information on the basic design features.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateEditStockBuilder
Default values.
Property Value Offset.Value 0 (millimeters part), 0 (inches part) PlateStock.KnuckleRatio 3.0 PlateStock.KnuckleSmoothAngle 3.0 PlateStock.MaterialOption 0 PlateStock.OppositeThickness.Value 0 (millimeters part), 0 (inches part) PlateStock.RestrictThicknessToMaterial true PlateStock.ThickenOption SingleSided PlateStock.Thickness.Value 10 (millimeters part), 0.5 (inches part) PlateStock.ThicknessSourceOption List SectionType Profile StiffenerStock.AnchorPoint 0 StiffenerStock.PlateHeight.Value 50 (millimeters part), 2 (inches part) StiffenerStock.SectionType Profile New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BuiltUpPillarStock | Returns the stock data used to define the built up stock information of the pillar. |
EndCutEnd | Returns or sets the end cut to use at the end of the stiffener sub system. |
EndCutStart | Returns or sets the end cut to use at the start of the stiffener sub system. |
MountingMethod | Returns or sets the mounting method |
Offset | Returns the offset to apply to the current plate system mold face to produce the desired mold face. |
OrientationAngle | Returns the angle at which the stiffener system is placed relative to the reference. |
OrientationAnglePillar | Returns the angle at which the pillar system is placed relative to the reference. |
OrientationLinePillar | Returns the line specified for the pillar system angle reference. |
OrientationMethod | Returns or sets the method used to define the reference for the orientation angle of stiffener system. |
OrientationVector | Returns or sets the vector specified for the orientation angle reference. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PillarStock | Returns the stock data used to define the stock information of the pillar. |
PlateStock | Returns the plate stock builder, used to define the plate material, grade, thickness, mass density, thicken option and opposite thickness. |
Reverse | Returns or sets the indication whether the direction of the flange should be reversed on this stiffener system. |
SectionType | Returns or sets the section type (profile or built up) for pillar system. |
ShipStructure | Returns the ship structures to change the stock information |
StiffenerStock | Returns the stock data used to define the stock information of the stiffener. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tightness | Returns or sets the tightness to apply to plate and subplate systems. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetPillarDirection | Sets the pillar direction. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateStockInformation | Update stock information |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BuiltUpPillarStock¶
-
EditStockBuilder.
BuiltUpPillarStock
¶ Returns the stock data used to define the built up stock information of the pillar.
-------------------------------------
Getter Method
Signature
BuiltUpPillarStock()
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX9.0.0.
License requirements: None.
EndCutEnd¶
-
EditStockBuilder.
EndCutEnd
¶ Returns or sets the end cut to use at the end of the stiffener sub system.
-------------------------------------
Getter Method
Signature
EndCutEnd()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutEnd(endCutEnd)
Parameters: endCutEnd ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
EndCutStart¶
-
EditStockBuilder.
EndCutStart
¶ Returns or sets the end cut to use at the start of the stiffener sub system.
-------------------------------------
Getter Method
Signature
EndCutStart()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutStart(endCutStart)
Parameters: endCutStart ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
MountingMethod¶
-
EditStockBuilder.
MountingMethod
¶ Returns or sets the mounting method
-------------------------------------
Getter Method
Signature
MountingMethod()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderMountingMethods
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MountingMethod(mountingMethod)
Parameters: mountingMethod ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderMountingMethods
) –New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Offset¶
-
EditStockBuilder.
Offset
¶ Returns the offset to apply to the current plate system mold face to produce the desired mold face.
The offset is applied in the thickness direction defined in the plate system feature
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OrientationAngle¶
-
EditStockBuilder.
OrientationAngle
¶ Returns the angle at which the stiffener system is placed relative to the reference.
-------------------------------------
Getter Method
Signature
OrientationAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
Deprecated since version NX10.0.0: Orientation angle can only be modified on the full profile system itself.
License requirements: None.
OrientationAnglePillar¶
-
EditStockBuilder.
OrientationAnglePillar
¶ Returns the angle at which the pillar system is placed relative to the reference.
-------------------------------------
Getter Method
Signature
OrientationAnglePillar()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
OrientationLinePillar¶
-
EditStockBuilder.
OrientationLinePillar
¶ Returns the line specified for the pillar system angle reference.
-------------------------------------
Getter Method
Signature
OrientationLinePillar()
Returns: Return type: NXOpen.SelectCurve
New in version NX8.5.0.
License requirements: None.
OrientationMethod¶
-
EditStockBuilder.
OrientationMethod
¶ Returns or sets the method used to define the reference for the orientation angle of stiffener system.
-------------------------------------
Getter Method
Signature
OrientationMethod()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods
New in version NX8.5.0.
Deprecated since version NX10.0.0: Orientation method can only be modified on the full profile system itself.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationMethod(orientationMethod)
Parameters: orientationMethod ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods
) –New in version NX8.5.0.
Deprecated since version NX10.0.0: Orientation method can only be modified on the full profile system itself.
License requirements: nx_ship_basic (“Ship Basic Design”)
OrientationVector¶
-
EditStockBuilder.
OrientationVector
¶ Returns or sets the vector specified for the orientation angle reference.
Only used when when Method is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods.Vector
..-------------------------------------
Getter Method
Signature
OrientationVector()
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
Deprecated since version NX10.0.0: Orientation vector can only be modified on the full profile system itself.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationVector(orientationVector)
Parameters: orientationVector ( NXOpen.Direction
) –New in version NX8.5.0.
Deprecated since version NX10.0.0: Orientation vector can only be modified on the full profile system itself.
License requirements: nx_ship_basic (“Ship Basic Design”)
PillarStock¶
-
EditStockBuilder.
PillarStock
¶ Returns the stock data used to define the stock information of the pillar.
-------------------------------------
Getter Method
Signature
PillarStock()
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX8.0.0.
License requirements: None.
PlateStock¶
-
EditStockBuilder.
PlateStock
¶ Returns the plate stock builder, used to define the plate material, grade, thickness, mass density, thicken option and opposite thickness.
-------------------------------------
Getter Method
Signature
PlateStock()
Returns: Plate Stock Builder Return type: NXOpen.Features.ShipDesign.PlateStockBuilder
New in version NX8.0.0.
License requirements: None.
Reverse¶
-
EditStockBuilder.
Reverse
¶ Returns or sets the indication whether the direction of the flange should be reversed on this stiffener system.
The default direction is based on the ship structure that the stiffener is being built upon.
-------------------------------------
Getter Method
Signature
Reverse()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Reverse(reverse)
Parameters: reverse (bool) – New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
SectionType¶
-
EditStockBuilder.
SectionType
¶ Returns or sets the section type (profile or built up) for pillar system.
-------------------------------------
Getter Method
Signature
SectionType()
Returns: Return type: NXOpen.Features.ShipDesign.PillarSystemBuilderStockSectionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionType(sectionType)
Parameters: sectionType ( NXOpen.Features.ShipDesign.PillarSystemBuilderStockSectionType
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
ShipStructure¶
-
EditStockBuilder.
ShipStructure
¶ Returns the ship structures to change the stock information
-------------------------------------
Getter Method
Signature
ShipStructure()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.0.0.
License requirements: None.
StiffenerStock¶
-
EditStockBuilder.
StiffenerStock
¶ Returns the stock data used to define the stock information of the stiffener.
-------------------------------------
Getter Method
Signature
StiffenerStock()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerStockBuilder
New in version NX8.0.0.
License requirements: None.
Tightness¶
-
EditStockBuilder.
Tightness
¶ Returns or sets the tightness to apply to plate and subplate systems.
-------------------------------------
Getter Method
Signature
Tightness()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tightness(tightness)
Parameters: tightness (int) – New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Method Detail¶
SetPillarDirection¶
-
EditStockBuilder.
SetPillarDirection
¶ Sets the pillar direction.
Signature
SetPillarDirection(direction)
Parameters: direction ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
UpdateStockInformation¶
-
EditStockBuilder.
UpdateStockInformation
¶ Update stock information
Signature
UpdateStockInformation(shipStructure)
Parameters: shipStructure ( NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Validate¶
-
EditStockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.