SynchronizeDesignViewBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
SynchronizeDesignViewBuilder
¶ Bases:
NXOpen.Builder
This class is used to synchronize body features from design view to manufacturing view.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateSynchronizeDesignViewBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DesignElementToSynchronizeDesignView | Returns the design element selection object to be processed in the change of mode processing. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SynchronizeDesignView | Loops through all selected parts and synchronizes body features from design view to manufacturing view. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DesignElementToSynchronizeDesignView¶
-
SynchronizeDesignViewBuilder.
DesignElementToSynchronizeDesignView
¶ Returns the design element selection object to be processed in the change of mode processing.
-------------------------------------
Getter Method
Signature
DesignElementToSynchronizeDesignView()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Method Detail¶
SynchronizeDesignView¶
-
SynchronizeDesignViewBuilder.
SynchronizeDesignView
¶ Loops through all selected parts and synchronizes body features from design view to manufacturing view.
Signature
SynchronizeDesignView()
Returns: Return type: int New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Validate¶
-
SynchronizeDesignViewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.