BuiltUpManModeBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
BuiltUpManModeBuilder
¶ Bases:
NXOpen.Builder
This class allows you to set the NX Ship BuiltUp Profile Manufacturing Mode for one or more components.
This mode may be either “Bend After Join” or “Cut To Shape”.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateBuiltUpManModeBuilder
Default values.
Property Value BuiltupManMode CutToShape New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BuiltupComps | Returns the components for which the Manufacturing Mode will be set |
BuiltupManMode | Returns or sets the builtup Manufactirng Mode |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BuiltUpManModeBuilderBuiltUpManModeType Enumeration | This enum defines the allowable values for the BuiltUp Profile Manufacturing Mode which may be either Cut To Shape or Bend After Join. |
Property Detail¶
BuiltupComps¶
-
BuiltUpManModeBuilder.
BuiltupComps
¶ Returns the components for which the Manufacturing Mode will be set
-------------------------------------
Getter Method
Signature
BuiltupComps()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX9.0.0.
License requirements: None.
BuiltupManMode¶
-
BuiltUpManModeBuilder.
BuiltupManMode
¶ Returns or sets the builtup Manufactirng Mode
-------------------------------------
Getter Method
Signature
BuiltupManMode()
Returns: Return type: NXOpen.Features.ShipDesign.BuiltUpManModeBuilderBuiltUpManModeType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BuiltupManMode(builtupManMode)
Parameters: builtupManMode ( NXOpen.Features.ShipDesign.BuiltUpManModeBuilderBuiltUpManModeType
) –New in version NX9.0.0.
License requirements: nx_ship_mfg_prep (“Ship Manufacturing”)
Method Detail¶
Validate¶
-
BuiltUpManModeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.