QualifySketchBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
QualifySketchBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ShipDesign.QualifySketchBuilder
builder.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateQualifySketchBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ActiveRowIndex | Returns or sets the active row index. |
BaseLine | Returns the selected base line. |
ContextAttribute | Returns or sets the context attribute. |
Feature | Returns or sets the steel feture type. |
ModelFile | Returns or sets the model file name. |
ModelList | Returns the model list. |
ModelPath | Returns or sets the model file path. |
MoldLine | Returns the selected mold line. |
OpposingMoldLine | Returns the selected opposing mold line. |
SectionType | Returns or sets the section type. |
ShearLine | Returns the selected shear line. |
ShipNo | Returns or sets the ship no. |
SpreadSheetFile | Returns or sets the parameter spreadsheet file. |
SpreadSheetPath | Returns or sets the parameter spreadsheet path. |
Tag | Returns the Tag for this object. |
TaperLine | Returns the selected taper line. |
TopLine | Returns the selected top line. |
Methods¶
Method | Description |
---|---|
AssignAttribute | Assigns attributes to the anchor point. |
Commit | Commits any edits that have been applied to the builder. |
CreateNewAnchorPoint | Creates the anchor point. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
OpenParameterSpreadSheetToEdit | Opens parameter spreadsheet to edit. |
OpenPartFile | Opens the template part file. |
OpenRegistrationSpreadSheetToEdit | Opens registration spreadsheet to edit. |
PreviewLeftImage | Previews left image. |
PreviewRightImage | Previews right image. |
ReloadParameterSpreadSheet | Reloads parameter spreadsheet. |
ReloadRegisterSpreadSheet | Reloads registration spreadsheet. |
ReloadTable | Reloads expression table. |
RemoveAttribute | Removes attributes from the entity. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateSketch | Updates sketch. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateCurves | Validates Curves. |
ValidateParameterSpreadSheet | Validates parameter spreadsheet. |
ValidatePartAttributes | Validates the part attributes. |
ValidateSketchCurves | Validates the sketch curves. |
Property Detail¶
ActiveRowIndex¶
-
QualifySketchBuilder.
ActiveRowIndex
¶ Returns or sets the active row index.
-------------------------------------
Getter Method
Signature
ActiveRowIndex()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveRowIndex(activeRowIndex)
Parameters: activeRowIndex (int) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
BaseLine¶
-
QualifySketchBuilder.
BaseLine
¶ Returns the selected base line.
-------------------------------------
Getter Method
Signature
BaseLine()
Returns: Return type: NXOpen.SelectCurve
New in version NX8.0.0.
License requirements: None.
ContextAttribute¶
-
QualifySketchBuilder.
ContextAttribute
¶ Returns or sets the context attribute.
-------------------------------------
Getter Method
Signature
ContextAttribute()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContextAttribute(contextAttribute)
Parameters: contextAttribute (int) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
Feature¶
-
QualifySketchBuilder.
Feature
¶ Returns or sets the steel feture type.
-------------------------------------
Getter Method
Signature
Feature()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Feature(feature)
Parameters: feature (int) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ModelFile¶
-
QualifySketchBuilder.
ModelFile
¶ Returns or sets the model file name.
-------------------------------------
Getter Method
Signature
ModelFile()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModelFile(modelFile)
Parameters: modelFile (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ModelList¶
-
QualifySketchBuilder.
ModelList
¶ Returns the model list.
-------------------------------------
Getter Method
Signature
ModelList()
Returns: Return type: NXOpen.Features.ShipDesign.AnchorPointList
New in version NX8.0.0.
License requirements: None.
ModelPath¶
-
QualifySketchBuilder.
ModelPath
¶ Returns or sets the model file path.
-------------------------------------
Getter Method
Signature
ModelPath()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModelPath(modelPath)
Parameters: modelPath (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
MoldLine¶
-
QualifySketchBuilder.
MoldLine
¶ Returns the selected mold line.
-------------------------------------
Getter Method
Signature
MoldLine()
Returns: Return type: NXOpen.SelectCurve
New in version NX8.0.0.
License requirements: None.
OpposingMoldLine¶
-
QualifySketchBuilder.
OpposingMoldLine
¶ Returns the selected opposing mold line.
-------------------------------------
Getter Method
Signature
OpposingMoldLine()
Returns: Return type: NXOpen.SelectCurve
New in version NX8.0.0.
License requirements: None.
SectionType¶
-
QualifySketchBuilder.
SectionType
¶ Returns or sets the section type.
-------------------------------------
Getter Method
Signature
SectionType()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionType(sectionType)
Parameters: sectionType (int) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ShearLine¶
-
QualifySketchBuilder.
ShearLine
¶ Returns the selected shear line.
-------------------------------------
Getter Method
Signature
ShearLine()
Returns: Return type: NXOpen.SelectCurve
New in version NX8.0.0.
License requirements: None.
ShipNo¶
-
QualifySketchBuilder.
ShipNo
¶ Returns or sets the ship no.
-------------------------------------
Getter Method
Signature
ShipNo()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShipNo(shipNo)
Parameters: shipNo (int) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SpreadSheetFile¶
-
QualifySketchBuilder.
SpreadSheetFile
¶ Returns or sets the parameter spreadsheet file.
-------------------------------------
Getter Method
Signature
SpreadSheetFile()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpreadSheetFile(spreadSheetFile)
Parameters: spreadSheetFile (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SpreadSheetPath¶
-
QualifySketchBuilder.
SpreadSheetPath
¶ Returns or sets the parameter spreadsheet path.
-------------------------------------
Getter Method
Signature
SpreadSheetPath()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpreadSheetPath(spreadSheetPath)
Parameters: spreadSheetPath (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
TaperLine¶
-
QualifySketchBuilder.
TaperLine
¶ Returns the selected taper line.
-------------------------------------
Getter Method
Signature
TaperLine()
Returns: Return type: NXOpen.SelectCurve
New in version NX8.0.0.
License requirements: None.
TopLine¶
-
QualifySketchBuilder.
TopLine
¶ Returns the selected top line.
-------------------------------------
Getter Method
Signature
TopLine()
Returns: Return type: NXOpen.SelectCurve
New in version NX8.0.0.
License requirements: None.
Method Detail¶
AssignAttribute¶
-
QualifySketchBuilder.
AssignAttribute
¶ Assigns attributes to the anchor point.
Signature
AssignAttribute(entity, category, title, value, attrType, objName)
Parameters: - entity (
NXOpen.TaggedObject
) – - category (str) –
- title (str) –
- value (str) –
- attrType (int) –
- objName (str) –
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
- entity (
CreateNewAnchorPoint¶
-
QualifySketchBuilder.
CreateNewAnchorPoint
¶ Creates the anchor point.
Signature
CreateNewAnchorPoint()
Returns: Return type: NXOpen.Features.ShipDesign.AnchorPoint
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
OpenParameterSpreadSheetToEdit¶
-
QualifySketchBuilder.
OpenParameterSpreadSheetToEdit
¶ Opens parameter spreadsheet to edit.
Signature
OpenParameterSpreadSheetToEdit()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
OpenPartFile¶
-
QualifySketchBuilder.
OpenPartFile
¶ Opens the template part file.
Signature
OpenPartFile()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
OpenRegistrationSpreadSheetToEdit¶
-
QualifySketchBuilder.
OpenRegistrationSpreadSheetToEdit
¶ Opens registration spreadsheet to edit.
Signature
OpenRegistrationSpreadSheetToEdit()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
PreviewLeftImage¶
-
QualifySketchBuilder.
PreviewLeftImage
¶ Previews left image.
Signature
PreviewLeftImage()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
PreviewRightImage¶
-
QualifySketchBuilder.
PreviewRightImage
¶ Previews right image.
Signature
PreviewRightImage()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ReloadParameterSpreadSheet¶
-
QualifySketchBuilder.
ReloadParameterSpreadSheet
¶ Reloads parameter spreadsheet.
Signature
ReloadParameterSpreadSheet()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ReloadRegisterSpreadSheet¶
-
QualifySketchBuilder.
ReloadRegisterSpreadSheet
¶ Reloads registration spreadsheet.
Signature
ReloadRegisterSpreadSheet()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ReloadTable¶
-
QualifySketchBuilder.
ReloadTable
¶ Reloads expression table.
Signature
ReloadTable()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
RemoveAttribute¶
-
QualifySketchBuilder.
RemoveAttribute
¶ Removes attributes from the entity.
Signature
RemoveAttribute(entity, category, title, attrType)
Parameters: - entity (
NXOpen.TaggedObject
) – - category (str) –
- title (str) –
- attrType (int) –
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
- entity (
UpdateSketch¶
-
QualifySketchBuilder.
UpdateSketch
¶ Updates sketch.
Signature
UpdateSketch()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
Validate¶
-
QualifySketchBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateCurves¶
-
QualifySketchBuilder.
ValidateCurves
¶ Validates Curves.
Signature
ValidateCurves()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ValidateParameterSpreadSheet¶
-
QualifySketchBuilder.
ValidateParameterSpreadSheet
¶ Validates parameter spreadsheet.
Signature
ValidateParameterSpreadSheet()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)