ShipCoordinatesBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ShipCoordinatesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ShipDesign.ShipCoordinates
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateShipCoordinatesBuilder
Default values.
Property Value AbsXValue 0 AbsYValue 0 AbsZValue 0 DeltaX 0 DeltaY 0 DeltaZ 0 XDirection Forward XDistance 0 YDirection Port YDistance 0 ZDirection Above ZDistance 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AbsXValue | Returns or sets the X value in absolute coordinate system. |
AbsYValue | Returns or sets the Y value in absolute coordinate system. |
AbsZValue | Returns or sets the Z value in absolute coordinate system. |
DeltaX | Returns or sets the delta value whic is distance between current point and previous point along X-direction. |
DeltaY | Returns or sets the delta value whic is distance between current point and previous point along Y-direction. |
DeltaZ | Returns or sets the delta value which is distance between current point and previous point long Z-direction. |
Point | Returns or sets the point to define ship coordinates. |
RoutingComponent | Returns the routing component. |
SelectionType | Returns or sets the selection type. |
Tag | Returns the Tag for this object. |
XDirection | Returns or sets the X-frame direction. |
XDistance | Returns or sets the distance along X-direction. |
XFrameOption | Returns or sets the X-frame option. |
YDirection | Returns or sets the Y-frame direction. |
YDistance | Returns or sets the distance along Y-direction. |
YFrameOption | Returns or sets the Y-frame option. |
ZDirection | Returns or sets the Z-frame direction. |
ZDistance | Returns or sets the distance along Z-direction. |
ZFrameOption | Returns or sets the Z-frame option. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreatePointByCoordinates | Creates a standard point. |
CycleRoutingPorts | Cycles through the ports on the selected routing component. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EvaluatePointInformation | Evaluates the point per position and and sets them into ShipCoordinatesBuilder builder. |
EvaluateSinglePortInformation | Evaluates the Nth ports information and sets them into ShipCoordinatesBuilder builder, the index starts from 1 and should be equal or less than number of ports. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetPorts | Gets ports in component. |
SetPosition | Sets the point information into the ShipCoordinate builder and a standard point will be created according to the position. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShipCoordinatesBuilderSelection Enumeration | Represents the options to select point or component. |
ShipCoordinatesBuilderXDirectionType Enumeration | Represents X-frame direction. |
ShipCoordinatesBuilderYDirectionType Enumeration | Represents Y-frame direction. |
ShipCoordinatesBuilderZDirectionType Enumeration | Represents Z-frame direction. |
Property Detail¶
AbsXValue¶
-
ShipCoordinatesBuilder.
AbsXValue
¶ Returns or sets the X value in absolute coordinate system.
-------------------------------------
Getter Method
Signature
AbsXValue()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AbsXValue(doubleABSX)
Parameters: doubleABSX (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
AbsYValue¶
-
ShipCoordinatesBuilder.
AbsYValue
¶ Returns or sets the Y value in absolute coordinate system.
-------------------------------------
Getter Method
Signature
AbsYValue()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AbsYValue(doubleABSY)
Parameters: doubleABSY (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
AbsZValue¶
-
ShipCoordinatesBuilder.
AbsZValue
¶ Returns or sets the Z value in absolute coordinate system.
-------------------------------------
Getter Method
Signature
AbsZValue()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AbsZValue(doubleABSZ)
Parameters: doubleABSZ (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
DeltaX¶
-
ShipCoordinatesBuilder.
DeltaX
¶ Returns or sets the delta value whic is distance between current point and previous point along X-direction.
-------------------------------------
Getter Method
Signature
DeltaX()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
DeltaX(deltaX)
Parameters: deltaX (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
DeltaY¶
-
ShipCoordinatesBuilder.
DeltaY
¶ Returns or sets the delta value whic is distance between current point and previous point along Y-direction.
-------------------------------------
Getter Method
Signature
DeltaY()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
DeltaY(deltaY)
Parameters: deltaY (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
DeltaZ¶
-
ShipCoordinatesBuilder.
DeltaZ
¶ Returns or sets the delta value which is distance between current point and previous point long Z-direction.
-------------------------------------
Getter Method
Signature
DeltaZ()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
DeltaZ(deltaZ)
Parameters: deltaZ (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
Point¶
-
ShipCoordinatesBuilder.
Point
¶ Returns or sets the point to define ship coordinates.
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Point(selectPoint)
Parameters: selectPoint ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
RoutingComponent¶
-
ShipCoordinatesBuilder.
RoutingComponent
¶ Returns the routing component.
-------------------------------------
Getter Method
Signature
RoutingComponent()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
SelectionType¶
-
ShipCoordinatesBuilder.
SelectionType
¶ Returns or sets the selection type.
-------------------------------------
Getter Method
Signature
SelectionType()
Returns: Return type: NXOpen.Features.ShipDesign.ShipCoordinatesBuilderSelection
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
SelectionType(type)
Parameters: type ( NXOpen.Features.ShipDesign.ShipCoordinatesBuilderSelection
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
XDirection¶
-
ShipCoordinatesBuilder.
XDirection
¶ Returns or sets the X-frame direction.
-------------------------------------
Getter Method
Signature
XDirection()
Returns: Return type: NXOpen.Features.ShipDesign.ShipCoordinatesBuilderXDirectionType
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
XDirection(xDirection)
Parameters: xDirection ( NXOpen.Features.ShipDesign.ShipCoordinatesBuilderXDirectionType
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
XDistance¶
-
ShipCoordinatesBuilder.
XDistance
¶ Returns or sets the distance along X-direction.
-------------------------------------
Getter Method
Signature
XDistance()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
XDistance(doubleXDistance)
Parameters: doubleXDistance (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
XFrameOption¶
-
ShipCoordinatesBuilder.
XFrameOption
¶ Returns or sets the X-frame option.
-------------------------------------
Getter Method
Signature
XFrameOption()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
XFrameOption(xFrame)
Parameters: xFrame (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
YDirection¶
-
ShipCoordinatesBuilder.
YDirection
¶ Returns or sets the Y-frame direction.
-------------------------------------
Getter Method
Signature
YDirection()
Returns: Return type: NXOpen.Features.ShipDesign.ShipCoordinatesBuilderYDirectionType
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
YDirection(yDirection)
Parameters: yDirection ( NXOpen.Features.ShipDesign.ShipCoordinatesBuilderYDirectionType
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
YDistance¶
-
ShipCoordinatesBuilder.
YDistance
¶ Returns or sets the distance along Y-direction.
-------------------------------------
Getter Method
Signature
YDistance()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
YDistance(doubleYDistance)
Parameters: doubleYDistance (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
YFrameOption¶
-
ShipCoordinatesBuilder.
YFrameOption
¶ Returns or sets the Y-frame option.
-------------------------------------
Getter Method
Signature
YFrameOption()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
YFrameOption(yFrame)
Parameters: yFrame (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
ZDirection¶
-
ShipCoordinatesBuilder.
ZDirection
¶ Returns or sets the Z-frame direction.
-------------------------------------
Getter Method
Signature
ZDirection()
Returns: Return type: NXOpen.Features.ShipDesign.ShipCoordinatesBuilderZDirectionType
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ZDirection(zDirection)
Parameters: zDirection ( NXOpen.Features.ShipDesign.ShipCoordinatesBuilderZDirectionType
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
ZDistance¶
-
ShipCoordinatesBuilder.
ZDistance
¶ Returns or sets the distance along Z-direction.
-------------------------------------
Getter Method
Signature
ZDistance()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ZDistance(doubleZDistance)
Parameters: doubleZDistance (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
ZFrameOption¶
-
ShipCoordinatesBuilder.
ZFrameOption
¶ Returns or sets the Z-frame option.
-------------------------------------
Getter Method
Signature
ZFrameOption()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ZFrameOption(zFrame)
Parameters: zFrame (str) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
Method Detail¶
CreatePointByCoordinates¶
-
ShipCoordinatesBuilder.
CreatePointByCoordinates
¶ Creates a standard point.
Signature
CreatePointByCoordinates()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
CycleRoutingPorts¶
-
ShipCoordinatesBuilder.
CycleRoutingPorts
¶ Cycles through the ports on the selected routing component.
Signature
CycleRoutingPorts()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
EvaluatePointInformation¶
-
ShipCoordinatesBuilder.
EvaluatePointInformation
¶ Evaluates the point per position and and sets them into ShipCoordinatesBuilder builder.
Signature
EvaluatePointInformation(position)
Parameters: position ( NXOpen.Point3d
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
EvaluateSinglePortInformation¶
-
ShipCoordinatesBuilder.
EvaluateSinglePortInformation
¶ Evaluates the Nth ports information and sets them into ShipCoordinatesBuilder builder, the index starts from 1 and should be equal or less than number of ports.
Signature
EvaluateSinglePortInformation(portIndex)
Parameters: portIndex (int) – New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
GetPorts¶
-
ShipCoordinatesBuilder.
GetPorts
¶ Gets ports in component.
Signature
GetPorts()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
SetPosition¶
-
ShipCoordinatesBuilder.
SetPosition
¶ Sets the point information into the ShipCoordinate builder and a standard point will be created according to the position.
Signature
SetPosition(position)
Parameters: position ( NXOpen.Point3d
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”) OR routing_base (“Routing Basic”)
Validate¶
-
ShipCoordinatesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.