EdgeCutBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
EdgeCutBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.EdgeCut
builder.The Edge Cut creates a series of cuts with an offset from an edge or curve.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateEdgeCutBuilder
Default values.
Property Value CutCount 0 CutOrientationAngle.Value 0 GuideOffset.Value 50 (millimeters part), 2 (inches part) SpaceBetweenCuts.Value 50 (millimeters part), 2 (inches part) Spacing EvenDistribution SymmetricOffsets 0 New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CutCount | Returns or sets the number of cuts |
CutOrientationAngle | Returns the cut orientation angle. |
EndPositionOnGuide | Returns the offset from the end of the guide curve (or end trim object) where cut placement will end. |
GuideCurve | Returns the guide curve used to place the cuts (may be made up of edges or curves). |
GuideOffset | Returns the guide offset (how far away to place the cuts from the guide curve) |
ManufacturingInformation | Returns the manufacturing stock builder that holds the manufacturing data. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PathGeometry | Returns the path geometry. |
PathReverseDirection | Returns or sets the path reverse direction flag. |
PlacementGeometry | Returns the placement geometry. |
ReferenceDirection | Returns or sets the reference direction |
ReferencePoint | Returns or sets the reference point (part units) |
SelectEndLimit | Returns the select end limit. |
SelectStartLimit | Returns the select start limit. |
SelectTargetFace | Returns the select target face. |
SketchBlock | Returns the sketch block. |
SpaceBetweenCuts | Returns the distance between each cut. |
Spacing | Returns or sets the spacing (even distribution or custom defined) |
StartPositionOnGuide | Returns the offset from the start of the guide curve (or start trim object) where cut placement will begin |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
SymmetricOffsets | Returns or sets the symmetric offsets toggle. |
Tag | Returns the Tag for this object. |
Version | Returns the version of the feature (used to determine which properties and methods are applicable) during edit. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EdgeCutBuilderArraySpacing Enumeration | available methods used to define the spacing between the cuts |
EdgeCutBuilderVersionID Enumeration | version identifiers for the different revisions of the edge cut feature. |
Property Detail¶
CutCount¶
-
EdgeCutBuilder.
CutCount
¶ Returns or sets the number of cuts
-------------------------------------
Getter Method
Signature
CutCount()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutCount(cutCount)
Parameters: cutCount (int) – New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
CutOrientationAngle¶
-
EdgeCutBuilder.
CutOrientationAngle
¶ Returns the cut orientation angle.
Typically the x axis of the cut’s cross section sketch is parallel to the guide curve, the orientation angle rotates the sketch away from the guide curve
-------------------------------------
Getter Method
Signature
CutOrientationAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
EndPositionOnGuide¶
-
EdgeCutBuilder.
EndPositionOnGuide
¶ Returns the offset from the end of the guide curve (or end trim object) where cut placement will end.
Note if the spacing is set to CustomDefined, you won’t notice the end trim getting used, unless you try to place too many cuts between along the guide (including any trim objects and offsets added by the Start and End positions on the guide).
-------------------------------------
Getter Method
Signature
EndPositionOnGuide()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.5.0.
License requirements: None.
GuideCurve¶
-
EdgeCutBuilder.
GuideCurve
¶ Returns the guide curve used to place the cuts (may be made up of edges or curves).
NOTE this is only used on features that were created prior to NX901. If editing a feature created in NX9.0.1 or beyond, use the path geometry property instead.
-------------------------------------
Getter Method
Signature
GuideCurve()
Returns: Return type: NXOpen.Section
New in version NX8.5.0.
License requirements: None.
GuideOffset¶
-
EdgeCutBuilder.
GuideOffset
¶ Returns the guide offset (how far away to place the cuts from the guide curve)
-------------------------------------
Getter Method
Signature
GuideOffset()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ManufacturingInformation¶
-
EdgeCutBuilder.
ManufacturingInformation
¶ Returns the manufacturing stock builder that holds the manufacturing data.
-------------------------------------
Getter Method
Signature
ManufacturingInformation()
Returns: Return type: NXOpen.Features.ShipDesign.ManufacturingStockBuilder
New in version NX8.5.1.
License requirements: None.
PathGeometry¶
-
EdgeCutBuilder.
PathGeometry
¶ Returns the path geometry.
NOTE this is only used on features that were created in NX901 or later. If editing a feature created before NX9.0.1, use the guide curve property instead.
-------------------------------------
Getter Method
Signature
PathGeometry()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX9.0.1.
License requirements: None.
PathReverseDirection¶
-
EdgeCutBuilder.
PathReverseDirection
¶ Returns or sets the path reverse direction flag.
NOTE this is only used on features that were created in NX901 or later.
-------------------------------------
Getter Method
Signature
PathReverseDirection()
Returns: Return type: bool New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
PathReverseDirection(pathReverseDirection)
Parameters: pathReverseDirection (bool) – New in version NX9.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”)
PlacementGeometry¶
-
EdgeCutBuilder.
PlacementGeometry
¶ Returns the placement geometry.
NOTE this is only used on features that were created in NX901 or later. If editing a feature created before NX9.0.1, use the select target face property instead.
-------------------------------------
Getter Method
Signature
PlacementGeometry()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX9.0.1.
License requirements: None.
ReferenceDirection¶
-
EdgeCutBuilder.
ReferenceDirection
¶ Returns or sets the reference direction
-------------------------------------
Getter Method
Signature
ReferenceDirection()
Returns: Return type: NXOpen.Vector3d
New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceDirection(referenceDirection)
Parameters: referenceDirection ( NXOpen.Vector3d
) –New in version NX9.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”)
ReferencePoint¶
-
EdgeCutBuilder.
ReferencePoint
¶ Returns or sets the reference point (part units)
-------------------------------------
Getter Method
Signature
ReferencePoint()
Returns: Return type: NXOpen.Point3d
New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePoint(referencePoint)
Parameters: referencePoint ( NXOpen.Point3d
) –New in version NX9.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”)
SelectEndLimit¶
-
EdgeCutBuilder.
SelectEndLimit
¶ Returns the select end limit.
The end limit is used to trim the end of the guide curve. Note if the spacing is set to CustomDefined, you won’t notice the end trim getting used, unless you try to place too many cuts between the start and end trim (including any offsets added by the Start and End positions on the guide). NOTE features created before NX9.0.1 could use solid edges, lines, circles, splines, spcurves, datum planes, and planar faces as a limit object. Any feature created in NX9.0.1 or beyond can use any of those limit objects as well as non-planar faces.
-------------------------------------
Getter Method
Signature
SelectEndLimit()
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.5.0.
License requirements: None.
SelectStartLimit¶
-
EdgeCutBuilder.
SelectStartLimit
¶ Returns the select start limit.
The start limit is used to trim the start of the guide curve. NOTE features created before NX9.0.1 could use solid edges, lines, circles, splines, spcurves, datum planes, and planar faces as a limit object. Any feature created in NX9.0.1 or beyond can use any of those limit objects as well as non-planar faces.
-------------------------------------
Getter Method
Signature
SelectStartLimit()
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.5.0.
License requirements: None.
SelectTargetFace¶
-
EdgeCutBuilder.
SelectTargetFace
¶ Returns the select target face.
NOTE this is only used on features that were created prior to NX901. If editing a feature created in NX9.0.1 or beyond, use the placement geometry property instead.
-------------------------------------
Getter Method
Signature
SelectTargetFace()
Returns: Return type: NXOpen.SelectFaceList
New in version NX8.5.0.
License requirements: None.
SketchBlock¶
-
EdgeCutBuilder.
SketchBlock
¶ Returns the sketch block.
Users can specify the hole shape using a single sketch. The sketch type and its parameters are controlled by the
NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
.-------------------------------------
Getter Method
Signature
SketchBlock()
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX8.5.0.
License requirements: None.
SpaceBetweenCuts¶
-
EdgeCutBuilder.
SpaceBetweenCuts
¶ Returns the distance between each cut.
Note this is ignored if spacing is set to equal spacing.
-------------------------------------
Getter Method
Signature
SpaceBetweenCuts()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Spacing¶
-
EdgeCutBuilder.
Spacing
¶ Returns or sets the spacing (even distribution or custom defined)
-------------------------------------
Getter Method
Signature
Spacing()
Returns: Return type: NXOpen.Features.ShipDesign.EdgeCutBuilderArraySpacing
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Spacing(spacing)
Parameters: spacing ( NXOpen.Features.ShipDesign.EdgeCutBuilderArraySpacing
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
StartPositionOnGuide¶
-
EdgeCutBuilder.
StartPositionOnGuide
¶ Returns the offset from the start of the guide curve (or start trim object) where cut placement will begin
-------------------------------------
Getter Method
Signature
StartPositionOnGuide()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.5.0.
License requirements: None.
SymmetricOffsets¶
-
EdgeCutBuilder.
SymmetricOffsets
¶ Returns or sets the symmetric offsets toggle.
Note this is ignored if spacing is set to custom defined. When symmetric offsets are used, the length of the guide is divided by the number of cuts to define the space between cuts, and half of the distance between each cut is applied as a start and end offset along the guide.
-------------------------------------
Getter Method
Signature
SymmetricOffsets()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymmetricOffsets(symmetricOffsets)
Parameters: symmetricOffsets (bool) – New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Version¶
-
EdgeCutBuilder.
Version
¶ Returns the version of the feature (used to determine which properties and methods are applicable) during edit.
The version of new features during create will be NX901
-------------------------------------
Getter Method
Signature
Version()
Returns: Return type: NXOpen.Features.ShipDesign.EdgeCutBuilderVersionID
New in version NX9.0.1.
License requirements: None.
Method Detail¶
Validate¶
-
EdgeCutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.