See: Description
Interface | Description |
---|---|
AlongGuideCut |
Represents a corner cut feature
To create or edit an instance of this class, use AlongGuideCutBuilder Created in NX8.5.0 |
AlongGuideCutBuilder |
Represents a
AlongGuideCut builder
To create a new instance of this class, use ShipCollection.createAlongGuideCutBuilder(nxopen.features.shipdesign.AlongGuideCut) Default values. |
AnchorPoint |
Represents a
AnchorPoint builder. |
AnchorPointList |
Represents a list of objects.
|
BuiltUpBlockBuilder | |
BuiltUpManModeBuilder |
This class allows you to set the NX Ship BuiltUp Profile Manufacturing Mode for
one or more components.
|
BuiltUpOffsetBuilder |
Represents a
BuiltUpOffsetBuilder .This class is for splitting ship built-up solidbodies
Created in NX9.0.0 |
BulkHeadListItemBuilder | |
BulkHeadListItemBuilderList |
Represents a list of objects.
|
BulkHeads |
Represents a bulk head feature
To create or edit an instance of this class, use BulkHeadsBuilder Created in NX5.0.0 |
BulkHeadsBuilder |
Represents a
BulkHeads builder
To create a new instance of this class, use ShipCollection.createBulkHeadsBuilder(Feature) Created in NX5.0.0 |
CompareModeBuilder |
This class is used to compare between the two Shipbuilding modes of Design and Manufacturing.
|
CopyObjectsBuilder |
Represents a
CopyObjectsBuilder
It is used in Ship Building Application. |
CopyPasteNewBuilder |
Represents a
CopyPasteNewBuilder
It is used in Ship Building Application. |
CornerCut |
Represents a corner cut feature
To create or edit an instance of this class, use CornerCutBuilder Created in NX8.5.0 |
CornerCutBuilder |
Builder used to create or edit a
CornerCut feature. |
CornerCutListItemBuilder |
Used to supply the list of corner cut locations and seam curves to the
CornerCutBuilder
To create a new instance of this class, use ShipCollection.createCornerCutListitemBuilder() Created in NX8.5.0 |
CornerCutListItemBuilderList |
Represents a list of objects.
|
CustomBracket |
Represents a custom bracket feature
To create or edit an instance of this class, use CustomBracketBuilder Created in NX7.5.0 |
CustomBracketBuilder |
Represents a
CustomBracket builder
To create a new instance of this class, use ShipCollection.createCustomBracketBuilder(Feature) Default values. |
Cutout2 |
Represents a cutout2 feature
To create or edit an instance of this class, use Cutout2Builder Created in NX8.0.0 |
Cutout2Builder |
Represents a
Cutout2 builder
To create a new instance of this class, use ShipCollection.createCutout2Builder(nxopen.features.shipdesign.Cutout2) Default values. |
CuttingSideFacesBuilder |
Used to create a
CuttingSideFacesBuilder which
is used to attribute the cutting side, and opposing cutting side, faces on the plate bodies. |
Deck |
Represents a Deck feature in Basic Design.
|
DeckBuilder |
This class is used to create or edit a
Deck feature. |
DeckListItemBuilder |
Represents a DeckListItemBuilder.
|
DeckListItemBuilderList |
Represents a list of objects.
|
Decks |
Represents a decks feature
To create or edit an instance of this class, use DecksBuilder Created in NX5.0.0 |
DecksBuilder |
Represents a
Decks builder. |
DeleteSeamBuilder |
Used to create a
DeleteSeamBuilder which
is used to delete the seams from the ship structural components. |
DisplaySolidBuilder |
This class is used to identify ship structure that is to have a temporary
solid display built for it.
|
DrawingTemplateBuilder |
Represents a drawing template selection block .
|
DvToMvMapping |
Represents a plate feature
To create or edit an instance of this class, use DvToMvMappingBuilder Created in NX8.5.0 |
DvToMvMappingBuilder |
Represents a
DvToMvMapping builder. |
EdgeCut |
Represents a edge cut feature
To create or edit an instance of this class, use EdgeCutBuilder Created in NX8.5.0 |
EdgeCutBuilder |
Represents a
EdgeCut builder. |
EdgeReinforcement |
Represents a edge reinforcement feature.
|
EdgeReinforcementBuilder |
Represents a
EdgeReinforcement builder which is used to create or edit a edge reinforcement system feature. |
EditContextAttributesBuilder |
Represents the class Features.ShipDesign.EditContextAttributesBuilder which is used to
edit the context attributes on the basic design features.
|
EditStockBuilder |
Used to create a
EditStockBuilder which
is used to change the stock information on the basic design features. |
EditWeldingBuilder |
Used to create a
EditWeldingBuilder which
is used to change the welding characteristics on the seams in the plate systems. |
EndCut |
Represents an end cut feature
To create or edit an instance of this class, use EndCutBuilder Created in NX8.0.0 |
EndCutBuilder |
Represents a
EndCut builder. |
ExcessMaterial |
Represents a excess material feature
To create or edit an instance of this class, use ExcessMaterialBuilder Created in NX7.5.0 |
ExcessMaterialBuilder |
Represents a
ExcessMaterial builder. |
ExpansionDrawing |
Represents a expansion drawing feature.
|
ExpansionDrawingBuilder |
Represents a
ExpansionDrawingBuilder . |
FeatureParmsBuilder |
This class is used to create or edit the information shared among all Ship Design features.
|
FeaturesBatchOperationBuilder |
Use this to cycle through the assembly components and perform the operation globally on the specified feature type.
|
FeaturesToTagBuilder |
This class is used to add an attribute to profile features that have been modified by
the user to display a 'Metal to Metal' design 'feature'.
|
FilterBuilder |
A builder that allows the user to define common properties of ship objects and then
add objects of similar properties to the select object list.
|
FrameBarOut |
Represents a FrameBarOut
To create or edit an instance of this class, use FrameBarOutBuilder Created in NX5.0.0 |
FrameBarOutBuilder |
Represents a
FrameBarOut builder. |
GenericPlateSystem |
Represents a Generic Plate System feature.
|
GenericPlateSystemBuilder |
This class is used to create or edit a
GenericPlateSystem feature. |
Hull |
Represents a Hull feature.
|
HullBuilder |
This class is used to create or edit a
Hull feature. |
InsertFramesBuilder |
Represents a
InsertFramesBuilder builder
To create a new instance of this class, use ShipCollection.createInsertFramesBuilder(Feature) Created in NX5.0.0 |
InsertSheetBody |
Represents a insert sheet body feature
To create or edit an instance of this class, use InsertSheetBodyBuilder Created in NX5.0.0 |
InsertSheetBodyBuilder |
Represents a
InsertSheetBody builder
To create a new instance of this class, use ShipCollection.createInsertSheetBodyBuilder(nxopen.features.shipdesign.InsertSheetBody) Created in NX5.0.0 |
InverseBendingLines |
Represents a inverse bending lines feature
To create or edit an instance of this class, use InverseBendingLinesBuilder Created in NX8.0.0 |
InverseBendingLinesBuilder |
Used to create or edit a
InverseBendingLines feature. |
ItFrameListItemBuilder | |
ItFrameListItemBuilderList |
Represents a list of objects.
|
ItFrames |
Represents a Inter Transverse Frame feature
To create or edit an instance of this class, use ItFramesBuilder Created in NX5.0.0 |
ItFramesBuilder |
Represents a
ItFrames builder
To create a new instance of this class, use ShipCollection.createItFramesBuilder(Feature) Created in NX5.0.0 |
KnuckledProfiles |
Represents a knuckled profiles manufacturing preparation feature
To create or edit an instance of this class, use KnuckledProfilesBuilder Created in NX5.0.3 |
KnuckledProfilesBuilder |
Represents a
KnuckledProfiles builder
To create a new instance of this class, use ShipCollection.createKnuckledProfilesBuilder(nxopen.features.shipdesign.KnuckledProfiles) Created in NX5.0.3 |
LongitudinalBulkhead |
Represents a Longitudinal Bulkhead feature.
|
LongitudinalBulkheadBuilder |
This class is used to create or edit a
LongitudinalBulkhead feature. |
MainDimensions |
Represents a main dimensions feature
To create or edit an instance of this class, use MainDimensionsBuilder Created in NX5.0.0 |
MainDimensionsBuilder |
Represents a
MainDimensions builder. |
ManufacturingDataBuilder |
This class is used to generate Manufacturing data.
|
ManufacturingOut |
Represents a ManufacturingOut
To create or edit an instance of this class, use ManufacturingOutBuilder Created in NX5.0.0 |
ManufacturingOutBuilder |
Represents a
ManufacturingOut builder
To create a new instance of this class, use ShipCollection.createManufacturingOutBuilder(Feature) Created in NX5.0.0 |
ManufacturingPreparation |
Represents a manufacturing preparation feature
To create or edit an instance of this class, use ManufacturingPreparationBuilder Created in NX8.0.2 |
ManufacturingPreparationBuilder |
This builder is used to adds attributes to the part and body identifying manufacturing related data.
|
ManufacturingStockBuilder |
Represents a
ManufacturingStockBuilder builder. |
MarkingLine |
Represents a marking line feature.
|
MarkingLineBuilder |
Represents a MarkingLine Feature builder
To create a new instance of this class, use ShipCollection.createMarkingLineBuilder(Feature) Created in NX5.0.0 |
MarkingLineDesign |
Represents a marking line feature.
|
MarkingLineDesignBuilder |
Represents a new MarkingLine Feature builder.
|
MaterialAllowanceBuilder |
Represents the material allowance feature builder to examine steel feature.
|
MaterialEstimationBuilder |
Represents the class Features.ShipDesign.MaterialEstimationBuilder which is used to
calculate the material estimation information.
|
MirrorShipStructureBuilder |
Copy the selected parts (components) about the Mirror Plane with full model history and feature data.
|
OrientationAngleMethodsBuilder |
This class defines the method of angle definition used in the definition of the region's orientation.
|
OrientationDefinition |
Represents a Orientation SubObject.
|
OrientationDefinitionBuilder |
This class defines the top level object for use in definining the orientation
of stiffeners and edge reinforcements.
|
OrientationPointMethodsBuilder |
This class is used to define the boundary of the regions when definining the orientation of a profile.
|
OrientationRegionItemBuilder |
This class defines each region of the orientation.
|
OrientationRegionItemBuilderList |
Represents a list of objects.
|
PenetrationAssociationBuilder |
Represents a
PenetrationAssociationBuilder builder To create a new instance of this class, use PenetrationRequestCollection.createPenetrationAssociationBuilder(boolean, nxopen.features.shipdesign.PenetrationRequest) Created in NX8.0.0 |
PenetrationAttachment |
Represents the Penetration Attachment object.
|
PenetrationCutoutBuilder |
Represents a
PenetrationRequest builder To create a new instance of this class, use PenetrationRequestCollection.createPenetrationCutoutBuilder(nxopen.features.shipdesign.PenetrationRequest) Default values. |
PenetrationFolder |
Represents the Penetration Folder object.
|
PenetrationList |
Represents the Penetration List object.
|
PenetrationManager |
Contains the collection objects for creating and iterating over Penetration Request Properties objects.
|
PenetrationRequest |
Represents the Penetration Request object.
|
PenetrationRequestBuilder |
Represents a
PenetrationRequest builder To create a new instance of this class, use PenetrationRequestCollection.createPenetrationRequestBuilder(nxopen.features.shipdesign.PenetrationRequest) Default values. |
PenetrationRequestCollection |
Represents a
FunctionObjectCollection To obtain an instance of this class, refer to PenetrationManager Created in NX8.0.0 |
PenetrationRequestForCutoutBuilder |
Represents a
Features.ShipDesign.PenetrationRequest builder To create a new instance of this class, use PenetrationRequestCollection.createPenetrationRequestForCutoutBuilder() Created in NX8.5.0 |
PenetrationReviewRequestBuilder |
Represents a
Features.ShipDesign.PenetrationRequest builder To create a new instance of this class, use PenetrationRequestCollection.createPenetrationReviewRequestBuilder(nxopen.features.shipdesign.PenetrationRequest[]) Created in NX8.0.0 |
PenetrationSite |
Represents the Penetration Site object.
|
PenetrationUtils |
Contains various penetration utility methods
To obtain an instance of this class, refer to PenetrationManager Created in NX8.0.0 |
Pillar |
Represents a Pillar feature
To create or edit an instance of this class, use PillarBuilder Created in NX8.0.0 |
PillarBuilder |
Represents a
Pillar builder
To create a new instance of this class, use ShipCollection.createPillarBuilder(nxopen.features.shipdesign.Pillar) Default values. |
PillarSystem |
Represents a pillar system feature.
|
PillarSystemBuilder |
Represents a
PillarSystem builder which is used to create or edit a pillar system feature. |
PinJig |
Represents a Pinjig feature
To create or edit an instance of this class, use PinJigBuilder Created in NX10.0.0 |
PinJigBuilder |
Represents a
PinJig builder
To create a new instance of this class, use ShipCollection.createPinJigBuilder(nxopen.features.shipdesign.PinJig) Created in NX10.0.0 |
PlaneListBuilder |
This class is used to place a plane into a list.
|
PlaneListBuilderList |
Represents a list of objects.
|
PlanePairBuilder |
This class is used to define a pair of planes in a list.
|
Plate |
Represents a plate feature
To create or edit an instance of this class, use PlateBuilder Created in NX8.0.0 |
PlateBuilder |
Represents a
Plate builder. |
PlateChamfer |
Represents a plate chamfer feature
To create or edit an instance of this class, use PlateChamferBuilder Created in NX8.0.0 |
PlateChamferBuilder |
Represents a
PlateChamfer builder. |
PlatePreparation |
Represents a ship plate preparation feature
To create or edit an instance of this class, use PlatePreparationBuilder Created in NX8.0.0 |
PlatePreparationBuilder |
Used to create or edit a
PlatePreparation feature. |
PlateStockBuilder |
This builder allows you to define the stock information for plate system features in ship design.
|
PlateSystem |
Represents a Plate System feature.
|
PlateSystemBuilder |
This class is used to create or edit the information shared between all the Basic Design plate system
features in the Ship Design application.
|
PointPairBuilder |
This class is used to define a pair of points in a list.
|
Profile |
Represents a profile feature
To create or edit an instance of this class, use ProfileBuilder Created in NX7.5.0 |
ProfileBuilder |
Represents a
Profile builder
To create a new instance of this class, use ShipCollection.createProfileBuilder(Feature) Default values. |
ProfileCutout |
Represents a profile cutout feature for NX8.
|
ProfileCutoutBuilder |
Represents a
ProfileCutout builder
To create a new instance of this class, use ShipCollection.createProfileCutoutBuilder(Feature) Default values. |
ProfileList |
Represents a profile list feature
To create or edit an instance of this class, use ProfileListBuilder Created in NX5.0.0 |
ProfileListBuilder |
Represents a
ProfileList builder
To create a new instance of this class, use ShipCollection.createProfileListBuilder(Feature) Created in NX5.0.0 |
ProfileSystem |
Represents a profile system feature.
|
ProfileSystemBuilder |
This class is used to create or edit the information shared between all the Basic Design profile system
features in the Ship Design application.
|
ProfileTransition |
Represents a profile transition feature
To create or edit an instance of this class, use ProfileTransitionBuilder Created in NX9.0.0 |
ProfileTransitionBuilder |
Builder used to create or edit a
ProfileTransition feature. |
QualifySketchBuilder |
Represents a
QualifySketchBuilder builder. |
ReadDataSetBuilder |
This class will read a data set file from Team Center .
|
RebaseBuilder |
This class is used to synchronize the end cuts from the ones in mfg group to design group.
|
ReferenceLine |
Represents a reference line feature.
|
ReferenceLineBuilder |
Represents a
ReferenceLine builder. |
RemoveSplitBuilder |
Represents a
RemoveSplitBuilder .This class is for removing split features. |
ReverseSplitBuilder |
This class is used to provide the capability to reverse the split interaction between
ship structures.
|
RollingLine |
Represents a rolling line feature.
|
RollingLineBuilder |
Represents a
RollingLine builder. |
Seam |
Represents a ship design seam feature.
|
SeamBlockBuilder |
Represents a
SeamBlockBuilder
To create a new instance of this class, use BuiltUpBlockBuilder.createSeamBlockBuilder() Created in NX9.0.0 |
SeamBlockBuilderList |
Represents a list of objects.
|
SeamBuilder |
A
SeamBuilder used to create or edit a
ship design Seam feature. |
SectionDrawingBuilder |
This builder allows you to define the section drawing information.
|
SectionViewBuilder |
This builder allows you to define the section view information for ship drawing.
|
SectionViewBuilderList |
Represents a list of objects.
|
SetModeBuilder |
This class is used to set the mode to design or manufacturing.
|
ShellExpansion |
Represents a shell expansion feature
To create or edit an instance of this class, use ShellExpansionBuilder Created in NX7.5.0 |
ShellExpansionBuilder |
Represents a
ShellExpansion builder
To create a new instance of this class, use ShipCollection.createShellExpansionBuilder(nxopen.features.shipdesign.ShellExpansion) Default values. |
ShellTemplate |
Represents a shell template feature.
|
ShellTemplateBuilder |
Used to edit or create a
ShellTemplate feature. |
ShipAttributeHolder |
Represents a
ShipAttributeHolder builder
This is an abstract class. |
ShipContainerBuilder |
This class is used to specify the "container" part for the Ship Structures application, i.e., that
part that should have newly created Ship Stiffeners, Plates, Standard Parts added to it as assembly
components.
|
ShipCoordinates |
Represents a ship coordinates feature
Ship Coordinates is not supported in KF. |
ShipCoordinatesBuilder |
Represents a
ShipCoordinates builder
To create a new instance of this class, use ShipCollection.createShipCoordinatesBuilder() Default values. |
ShipCutout |
Represents a ship cutout feature
To create or edit an instance of this class, use ShipCutoutBuilder Created in NX7.5.0 |
ShipCutoutBuilder |
Represents a
ShipCutout builder
To create a new instance of this class, use ShipCollection.createShipCutoutBuilder(nxopen.features.shipdesign.ShipCutout) Default values. |
ShipDesignPreferencesBuilder |
Represents a
ShipDesignPreferencesBuilder which
is used to change default object display settings for ship structures. |
ShipDesignVersionUpBuilder |
Represents a
ShipDesignVersionUpBuilder builder. |
ShipEndCut |
Represents a ship end cut feature
To create or edit an instance of this class, use ShipEndCutBuilder Created in NX7.5.0 |
ShipEndCutBuilder |
Represents a
ShipEndCut builder
To create a new instance of this class, use ShipCollection.createShipEndCutBuilder(nxopen.features.shipdesign.ShipEndCut) Default values. |
ShipFeatureConverter |
This class is used to convert/upgrade legacy Ship Design features.
|
ShipFlatPattern | Deprecated
Deprecated in NX8.0.0.
|
ShipFlatPatternBuilder | Deprecated
Deprecated in NX8.0.0.
|
ShipIntersections |
Represents a ship intersection feature
To create or edit an instance of this class, use ShipIntersectionsBuilder Created in NX7.5.0 |
ShipIntersectionsBuilder |
Represents a
ShipIntersections builder
To create a new instance of this class, use ShipCollection.createShipIntersectionsBuilder(nxopen.features.shipdesign.ShipIntersections) Default values. |
ShipNameFieldBuilder |
A field, combined with other fields, to generate a name for a Ship Basic Design Object such as a Deck.
|
ShipNamesBuilder |
This class provides the mechanism for defining the names of Basic Design objects
such as Decks, Bulkheads, Stiffener Systems, etc.
|
ShipNamesBuilderList |
Represents a list of objects.
|
ShipNamesListBuilder |
This class provides a list of
ShipNamesBuilder objects. |
ShipPreparationBuilder |
Creates a builder used to prepare basic design data for meshing.
|
ShipProfileCutout |
Represents a profile cutout feature for NX75 using sketch expression modifier block.
|
ShipProfileCutoutBuilder |
Represents a
ProfileCutout builder for editing legacy(NX75) profile cutout feature. |
ShipSection |
Represents a ship section feature
To create or edit an instance of this class, use ShipSectionBuilder Created in NX7.5.0 |
ShipSectionBuilder |
Represents a
ShipSection builder
To create a new instance of this class, use ShipCollection.createShipSectionBuilder(nxopen.features.shipdesign.ShipSection) Default values. |
ShipTrimBody |
Represents a ship trim body feature
To create or edit an instance of this class, use ShipTrimBodyBuilder Created in NX9.0.1 |
ShipTrimBodyBuilder |
Represents a
ShipTrimBodyBuilder . |
SmartRule |
Represents a smart rule feature.
|
SmartRuleBuilder |
Represents a
SmartRule builder
To create a new instance of this class, use ShipCollection.createSmartRuleBuilder(nxopen.features.shipdesign.SmartRule) Created in NX8.0.0 |
SplitProfilePlateBuilder |
Represents a
SplitProfilePlateBuilder .This class is for splitting ship profile/plate solidbodies
To create a new instance of this class, use ShipCollection.createSplitProfilePlateBuilder() Default values. |
SplitStandardPart |
Represents a split standard part feature.
|
SplitStandardPartBuilder |
Represents a
SplitStandardPartBuilder .This class is for splitting ship standard part
To create a new instance of this class, use ShipCollection.createSplitStandardPartBuilder(nxopen.features.shipdesign.SplitStandardPart) Default values. |
StandardPart |
Represents a standard part feature.
|
StandardPartFrameworkBuilder |
Represents the standard part framework builder to add or edit ship standard part.
|
StandardPartItemBuilder |
Represents the ship standard part item builder.
|
StandardPartItemBuilderList |
Represents a list of objects.
|
StandardPartSCAssist |
Represents
To create or edit an instance of this class, use StandardPartFrameworkBuilder Created in NX9.0.0 |
SteelCollarPlate |
Represents a collar plate steel feature
To create or edit an instance of this class, use SteelCollarPlateBuilder Created in NX7.5.0 |
SteelCollarPlateBuilder |
Represents a
SteelCollarPlate builder
To create a new instance of this class, use ShipCollection.createSteelCollarPlateBuilder(nxopen.features.shipdesign.SteelCollarPlate) Default values. |
SteelDistribution |
Represents a steel distribution feature
To create or edit an instance of this class, use SteelDistributionBuilder Created in NX5.0.0 |
SteelDistributionBuilder |
Represents a
SteelDistribution builder
To create a new instance of this class, use ShipCollection.createSteelDistributionBuilder(Feature) Created in NX5.0.0 |
SteelInsulation |
Represents a steel insulation feature.
|
SteelInsulationBoundaryBuilder |
Represents a Steel Insulation Boundary builder.
|
SteelInsulationBoundaryBuilderList |
Represents a list of objects.
|
SteelInsulationBuilder |
Represents a builder that is used to create or edit a
SteelInsulation feature. |
SteelVentHoles |
Represents a ship vent holes feature
To create or edit an instance of this class, use SteelVentHolesBuilder Created in NX7.5.0 |
SteelVentHolesBuilder |
Represents a
SteelVentHoles builder
To create a new instance of this class, use ShipCollection.createSteelVentHolesBuilder(nxopen.features.shipdesign.SteelVentHoles) Default values. |
Stiffener |
Represents a stiffener feature
To create or edit an instance of this class, use StiffenerBuilder Created in NX8.0.0 |
StiffenerBuilder |
Represents a
Stiffener builder
To create a new instance of this class, use ShipCollection.createStiffenerBuilder(nxopen.features.shipdesign.Stiffener) Default values. |
StiffenerBySupportPathBuilder |
This class defines the builder to collect stiffener by support path data for Stiffener feature.
|
StiffenerLimitBuilder |
This class defines the path limit method used by a Stiffener or Edge Reinforcement feature.
|
StiffenerStockBuilder |
This class defines the Profile or Plate stock for a Stiffener or Edge Reinforcement feature.
|
StiffenerSystem |
Represents a stiffener system feature.
|
StiffenerSystemBuilder |
This class is used to create or edit a
StiffenerSystem feature. |
SubSystemBuilder |
This class is used to
edit the Sub System Definition of a
SubSystems feature. |
SubSystemBuilderList |
Represents a list of objects.
|
SubSystems |
Represents a sub systems feature.
|
SubSystemsBuilder |
This class is used to
edit a
SubSystems feature. |
SynchronizeDesignViewBuilder |
This class is used to synchronize body features from design view to manufacturing view.
|
ThicknessDirectionBuilder |
This class allows you to define the thickness direction for plate system features in Ship Basic Design and
and for grid planes in Ship Concept Design.
|
TraceLines |
Represents a trace lines feature
To create or edit an instance of this class, use TraceLinesBuilder Created in NX7.5.0 |
TraceLinesBuilder |
Represents a
TraceLines builder
To create a new instance of this class, use ShipCollection.createTraceLinesBuilder(nxopen.features.shipdesign.TraceLines) Default values. |
TransFrame |
Represents a TransVerse Frame feature
To create or edit an instance of this class, use TransFrameBuilder Created in NX5.0.0 |
TransFrameBuilder |
Represents a
TransFrame builder
To create a new instance of this class, use ShipCollection.createTransFrameBuilder(Feature) Created in NX5.0.0 |
TransFrameListItemBuilder | |
TransFrameListItemBuilderList |
Represents a list of objects.
|
TransitionBuilder |
This is to create a
TransitionBuilder which is used to create Detail Design elements from Basic Design elements. |
TransverseBulkhead |
Represents a Transverse Bulkhead feature.
|
TransverseBulkheadBuilder |
This class is used to create or edit a
TransverseBulkhead feature. |
UnfoldedMinRecBuilder |
Represents the class Features.ShipDesign.UnfoldedMinRecBuilder which is used to
calculate the unfolded minimum rectangle of ship basic design plates or standard parts.
|
UpdateShipLibrary |
Represents a update ship library feature
To create or edit an instance of this class, use UpdateShipLibraryBuilder Created in NX5.3.0 |
UpdateShipLibraryBuilder |
Represents a
UpdateShipLibrary builder
To create a new instance of this class, use ShipCollection.createUpdateShipLibraryBuilder(Feature) Default values. |
VentHolesMarking |
Represents a vent holes marking feature
To create or edit an instance of this class, use VentHolesMarkingBuilder Created in NX5.0.3 |
VentHolesMarkingBuilder |
Represents a
VentHolesMarking builder
To create a new instance of this class, use ShipCollection.createVentHolesMarkingBuilder(nxopen.features.shipdesign.VentHolesMarking) Created in NX5.0.3 |
VentilationHoles2 |
Represents a ventilation holes2 feature
To create or edit an instance of this class, use VentilationHoles2Builder Created in NX8.0.0 |
VentilationHoles2Builder |
Represents a
VentilationHoles2 builder
To create a new instance of this class, use ShipCollection.createVentilationHoles2Builder(nxopen.features.shipdesign.VentilationHoles2) Default values. |
VerifyPenetrationBuilder |
Represents a
VerifyPenetrationBuilder builder To create a new instance of this class, use PenetrationRequestCollection.createVerifyPenetrationBuilder() Created in NX8.5.0 |
WeightAndCGBuilder |
Represents the class Features.ShipDesign.WeightAndCGBuilder which is used to
calculate the weight and cg information.
|
WeldCut |
Represents a weld cut feature
To create or edit an instance of this class, use WeldCutBuilder Created in NX7.5.0 |
WeldCut2 |
Represents a weld cut2 feature
To create or edit an instance of this class, use WeldCut2Builder Created in NX8.0.1 |
WeldCut2Builder |
Represents a
WeldCut2 builder
To create a new instance of this class, use ShipCollection.createWeldCut2Builder(nxopen.features.shipdesign.WeldCut2) Default values. |
WeldCutBuilder |
Represents a
WeldCut builder
To create a new instance of this class, use ShipCollection.createWeldCutBuilder(Feature) Default values. |
YFrameBuilder |
Represents a
YFrameBuilder
To create a new instance of this class, use ShipCollection.createYFrameBuilder(Feature) Created in NX5.0.0 |
ZFrameBuilder |
Represents a
ZFrameBuilder
To create a new instance of this class, use ShipCollection.createZFrameBuilder(Feature) Created in NX5.0.0 |
Class | Description |
---|---|
AlongGuideCutBuilder.CreationMethod |
Creation method used to define the placement of the along guide cut
|
AlongGuideCutBuilder.WaterStopOffsetMethod |
Offset option used to define the placement of the water stop guide cut
|
BuiltUpManModeBuilder.BuiltUpManModeType |
This enum defines the allowable values for the BuiltUp Profile Manufacturing Mode which
may be either "Cut To Shape" or "Bend After Join".
|
BulkHeadsBuilder.BulkheadType |
Represents the bulkhead type.
|
CompareModeBuilder.CompareMode |
Compare Mode type
|
CopyObjectsBuilder.Type |
Type of Source Objects.
|
CornerCutBuilder.CutOption |
Represents the corner cut option.
|
CustomBracketBuilder.CreationMethod |
Creation method used to define the placement of the bracket
|
Cutout2Builder.CreationMethod |
available methods used to place a cutout object
|
CuttingSideFacesBuilder.Types |
Type of operation to perform on the plate.
|
DeckBuilder.Types |
Indicates the method that is being used to define the mold face of the deck.
|
DeckListItemBuilder.DatumDir |
Represents the thickening direction.
|
DisplaySolidBuilder.DisplayOptionTypes |
Used to specify how the basic design profile system objects are displayed.
|
EdgeCutBuilder.ArraySpacing |
available methods used to define the spacing between the cuts
|
EdgeCutBuilder.VersionID |
version identifiers for the different revisions of the edge cut feature.
|
EdgeReinforcementBuilder.EndCutTypes |
Used to specify the type of end cut to be used at the extreme ends of the edge reinforcement system.
|
EdgeReinforcementBuilder.OrientationMethods |
Used to specify the type of reference to use for specifying the orientation of the edge reinforcement system.
|
EdgeReinforcementBuilder.Types |
Used to specify how the edge reinforcement system is defined.
|
EndCutBuilder.ConnectionTypes |
This enum defines the different ways a limiting geometry can connect to the endcut face. |
EndCutBuilder.DraftTypes |
This enum defines the types of draft to be applied.
|
EndCutBuilder.LimitTypes |
This enum defines the different ways users can trim the ends of a profile or a plate.
|
EndCutBuilder.SelectionTypes |
This enum defines the Placement Face and Placement Edge Selection Type.
|
ExamineSteelFeatureBuilderCheck |
Represents the object types to examine.
|
ExamineSteelFeatureBuilderResult |
Represents the status of examining result.
|
ExcessMaterialBuilder.Offset |
The offset type (only applicable for excess material, fitup will ignore the offset type)
|
ExcessMaterialBuilder.Types |
The feature type
|
ExcessMaterialBuilder.VersionID |
version identifiers for the different revisions of the excess material feature.
|
FeatureParmsBuilder.OrientationAngleRuleTypes |
Settings to indicate how angles are to be measured.
|
FeaturesBatchOperationBuilder.Types |
The option for which kind of operation will be performed.
|
GenericPlateSystemBuilder.Types |
Indicates the method that is being used to define the mold face of the generic plate system.
|
HullBuilder.Types |
Indicates the method that is being used to define the mold face of the hull.
|
InsertFramesBuilder.Types |
Represents the Insert Frame Builder type.
|
InverseBendingLinesBuilder.FailedProfilesData |
This class holds the data returned from
InverseBendingLinesBuilder.getFailedProfiles() |
InverseBendingLinesBuilder.MeasureType |
The direction to measure from.
|
InverseBendingLinesBuilder.MethodType |
The method used to generate the bending curves.
|
InverseBendingLinesBuilder.NeutralMethodType |
The method used to calculate the neutral line.
|
InverseBendingLinesBuilder.ReferencePlaneType |
The reference plane to draw the diagram on.
|
LongitudinalBulkheadBuilder.Types |
Indicates the method that is being used to define the mold face of the longitudinal bulkhead.
|
ManufacturingPreparationBuilder.AttributeType |
Represents manufacturing attribute type.
|
ManufacturingStockBuilder.CheckBoxStatus |
the check box status.
|
ManufacturingStockBuilder.LockedStatus |
the NX attribute locked status.
|
ManufacturingStockBuilder.ObjectType |
the object to which the manufacturing attributes will be written.
|
ManufacturingStockBuilder.StockDataSourceType |
the data source from which the intial manufacturing data will be read.
|
MarkingLineDesignBuilder.MarkingLineInformationData |
This class holds the data returned from
MarkingLineDesignBuilder.getMarkingLineInformation(nxopen.ICurve) |
MaterialEstimationBuilder.SelectionMethods |
Settings to indicate how the objects are selected.
|
OrientationAngleMethodsBuilder.AlignAtTypes |
Is the angle to be aligned with the region adjacent to start of this region or adjacent to the end of this region.
|
OrientationAngleMethodsBuilder.MethodTypes |
Settings used to determine how the angle is defined.
|
OrientationDefinitionBuilder.MeasureAngleTypes |
Settings to indicate how angles are measured in all orientation objects.
|
OrientationDefinitionBuilder.PlacementSideTypes |
Settings to indicate which side of the placement faces the stiffener is to be placed.
|
OrientationPointMethodsBuilder.MeasureAlongTypes |
Settings to indicate how the distance is measured.
|
OrientationPointMethodsBuilder.PointMethodTypes |
Settings to indicate how the boundary is defined.
|
OrientationRegionItemBuilder.OrientationMethodTypes |
Settings to indicate how the web orientation is defined for this region.
|
PenetrationRequest.CompensationType |
Represents the Compensation type
|
PenetrationRequest.CoutoutType |
Represents the Coutout type
|
PenetrationRequest.DirectionType |
Represents the Direction type
|
PenetrationRequest.PenetrationType |
Represents the penetration type
|
PenetrationRequest.RequestType |
Represents the request type
|
PenetrationRequestBuilder.RequestDialogType |
Represents the dialog type
|
PenetrationUtils.Referencetype |
Represents the reference type
|
PenetrationUtils.RequestState |
Representes the request state
|
PenetrationUtils.Verify_penetrationsData |
This class holds the data returned from
#verifyPenetrations |
PillarBuilder.CapOptions |
Settings to indicate how the cap is designed.
|
PillarBuilder.CreationMethod |
Method used to create the support feature.
|
PillarBuilder.EndCutTypes |
this specifies how the end cuts are applied
|
PillarBuilder.EndTreatmentTypes |
this specifies how the end is treated
|
PillarBuilder.EndTypeOptions |
this specifies end type option
|
PillarBuilder.StockSectionType |
SpreadSheet Type Profile or BuiltUp
|
PillarSystemBuilder.StockSectionType |
SpreadSheet Type Profile or BuiltUp
|
PillarSystemBuilder.Types |
Used to specify how the pillar system is defined.
|
PlateBuilder.BodyTypes |
Settings to indicate the plate output body type.
|
PlateBuilder.RegionOptions |
Settings to indicate what areas to create the plate when using body faces as boundaries.
|
PlateBuilder.TightnessOptions |
Settings to indicate what tightness to create the plate.
|
PlateBuilder.Types |
Settings to indicate how the plate is generated.
|
PlateChamferBuilder.AngleMethod |
The option to specify the method for defining angle or ratio.
|
PlateChamferBuilder.OffsetMethod |
The option to specify the method for chamfer offset method.
|
PlateChamferBuilder.Types |
The option for the type of associativity for chamfer.
|
PlateStockBuilder.ThickenOptions |
Settings to indicate how to apply the thickness to the mold face or offset mold face .
|
PlateStockBuilder.ThicknessSourceOptions |
Settings to indicate where the material thickness source resides.
|
PlateSystemBuilder.StiffenerDirectionType |
Settings used to indicate the default primary and secondary stiffener direction.
|
ProfileBuilder.Alignment |
Creation method used to define the placement of the belt this
is disabled for profiles
|
ProfileBuilder.EndCutOption |
Creation method used to define the end cut type
|
ProfileBuilder.OrientationOption |
Creation method used to define the placement of the profile this
is disabled for belt creation
|
ProfileBuilder.SectionOption |
Creation of profile from the library or a plate
|
ProfileBuilder.TypeOption |
Creation type either a belt or a profile
|
ProfileCutoutBuilder.Orientation |
Represents the profile cutout orientation values.
|
ProfileTransitionBuilder.FeatureModeType |
Represents the feature mode option.
|
ProfileTransitionBuilder.MisalignedModeType |
Represents the misaligned profile mode.
|
RollingLineBuilder.ConstructionMethodTypes |
The option to specify the method for creation of the pressure line.
|
RollingLineBuilder.StartEvaluationTypes |
The option for how the starting point for the evaluation of the sheet is to be created if
it is not given.
|
RollingLineBuilder.Types |
The option for the type of manufacturing operation to be performed on the sheet
to form it.
|
SeamBlockBuilder.SeamType |
this specifies seam type option
|
SeamBuilder.DefinitionMethods |
Used to indicate the method being used to define the seam locations.
|
SeamBuilder.StaggerShiftAlongMethods |
Used to indicate the method being used to define which direction the seam stagger will shift along.
|
SeamBuilder.Types |
Used to indicate the type of seam that is being created.
|
SectionDrawingBuilder.SectionsPerDrawingOptions |
Settings to indicate the section per drawing.
|
SectionDrawingBuilder.ViewsPerSheetOptions |
Settings to indicate the views per sheet.
|
SectionViewBuilder.DirectionOptions |
Settings to indicate the view direction
|
SectionViewBuilder.PlaneTypes |
Settings to indicate the plane type
|
SectionViewBuilder.SectionRuleOptions |
Settings to indicate the section rule
|
SetModeBuilder.DesMfgMode |
Manufacturing Mode type.
|
ShellTemplateBuilder.MarkingTypes |
The option for controlling which marking lines are drawn on the plate
|
ShellTemplateBuilder.PlaneLocationTypes |
The option for how the plane locations will be specified as input.
|
ShellTemplateBuilder.Types |
The option for controlling how the coordinate system for template creation is specified.
|
ShipCoordinatesBuilder.Selection |
Represents the options to select point or component.
|
ShipCoordinatesBuilder.XDirectionType |
Represents X-frame direction.
|
ShipCoordinatesBuilder.YDirectionType |
Represents Y-frame direction.
|
ShipCoordinatesBuilder.ZDirectionType |
Represents Z-frame direction.
|
ShipCutoutBuilder.CreationMethod |
available methods used to place a cutout object
|
ShipDesignPreferencesBuilder.AngleRuleTypes |
The methods that can be used to measure angles in ship design.
|
ShipDesignPreferencesBuilder.ColorType |
the color option type
|
ShipDesignPreferencesBuilder.Types |
This enum represents the ship structure types.
|
ShipEndCutBuilder.CreationMethod |
available methods used to place a cutout object
|
ShipFeatureConverter.PartScope |
Settings for the conversion scope
|
ShipIntersectionsBuilder.CreationType |
Define the creation type
|
ShipIntersectionsBuilder.Type |
Define the output option for each of the frame type
|
ShipnameFieldBuilderType |
Field Type
|
ShipnamesBuilderType |
The type of Ship Object for which automatically generated names will be created
|
ShipSectionBuilder.Type |
Define the creation type
|
ShipSectionBuilder.XFilter |
Define the output option for each of the frame type
|
ShipSectionBuilder.ZFilter |
Define the output option for each of the frame type
|
SplitProfilePlateBuilder.ProfileType |
Represents the target body type.
|
SplitProfilePlateBuilder.SplitDirectionOptionType |
Represents split direction to trim profile or plate solid body .
|
SplitProfilePlateBuilder.ToolOptionType |
Represents trim tool type to trim profile or plate solid body.
|
SplitStandardPartBuilder.ToolTypes |
Represents the split tool types.
|
StandardPartFrameworkBuilder.CheckSpreadsheetInputData |
This class holds the data returned from
StandardPartFrameworkBuilder.checkSpreadsheetInput(nxopen.features.shipdesign.StandardPartItemBuilder) |
StandardPartFrameworkBuilder.CreationType |
Indicates the creation type
|
StandardPartFrameworkBuilder.RunSmartRuleData | |
StandardPartFrameworkBuilder.SmartRuleStage |
Indicates the stage of the smart rule.
|
StandardPartItemBuilder.Direction |
Represents the ship standard part installation direction and thickness direction.
|
SteelDistributionBuilder.SaForm |
Sa Form
|
SteelDistributionBuilder.SaMaterial |
Sa Material
|
SteelDistributionBuilder.SaName |
Sa Name
|
SteelDistributionBuilder.SaSize |
Sa Size
|
SteelDistributionBuilder.SaType |
Sa Type
|
StiffenerBuilder.AttachmentOption |
The stiffener attachment plate option
|
StiffenerBuilder.CreatePathData |
This class holds the data returned from
StiffenerBuilder.createPath() |
StiffenerBuilder.EdgeReinforcementAlignmentMethod |
the edge reinforcement alignment method
|
StiffenerBuilder.EdgeReinforcementPlacementMethods |
The edge reinforcement placement method
|
StiffenerBuilder.EndCutTypes |
this specifies how the end cuts are applied
|
StiffenerBuilder.KnuckleOptions |
the knuckle option
|
StiffenerBuilder.MountingMethods |
the mounting method offset type
|
StiffenerBuilder.OrientationMethod |
The stiffener orientation method
|
StiffenerBuilder.Types |
the feature type: Stiffener or Edge Reinforcement
|
StiffenerBySupportPathBuilder.AlignedTo |
Which face the stiffener is aligned to
|
StiffenerBySupportPathBuilder.Method |
Type of Stiffener by Support Method
|
StiffenerBySupportPathBuilder.Scenario |
Scenarios of Stiffener by Support
|
StiffenerLimitBuilder.LimitType |
Path limiting method
|
StiffenerStockBuilder.StockSectionType |
Type of Stiffener/Edge Reinforcement stock: Profile or Plate
|
StiffenerSystemBuilder.EndCutTypes |
Used to specify the type of end cut to be used at the extreme ends of the stiffener system.
|
StiffenerSystemBuilder.MeasureAlongModes |
Used to specify how the spacing and offset is to be measured.
|
StiffenerSystemBuilder.MountingMethods |
the mounting method offset type
|
StiffenerSystemBuilder.OffsetSpacingModes |
Used to specify if a single or double offset and spacing definition is to be used.
|
StiffenerSystemBuilder.OrientationMethods |
Used to specify the type of reference to use for specifying the orientation of the stiffener system.
|
StiffenerSystemBuilder.PointMethods |
Used to specify whether points or planes are being used for the points definition.
|
StiffenerSystemBuilder.Types |
Used to specify how the path of the stiffener system is defined.
|
SubSystemsBuilder.Types |
Used to indicate the type of sub system definition that is being edited.
|
ThicknessDirectionBuilder.ThicknessDirectionType |
Settings used to indicate the direction of thickness from the mold face or grid plane.
|
TraceLinesBuilder.TraceLineType |
Define the traceline creation method
|
TransitionBuilder.TransitionMethods |
Transition Method.
|
TransitionBuilder.TransitionTypes |
Transition Type.
|
TransverseBulkheadBuilder.Types |
Indicates the method that is being used to define the mold face of the transverse bulkhead.
|
UpdateShipLibraryBuilder.ShipLibAssemblyOption |
Assembly update library options
|
UpdateShipLibraryBuilder.ShipLibOptionType |
Ship Library Types
Note the weld along edge option is no longer used in NX7.5, and will be removed in NX8.
|
VentilationHoles2Builder.ArraySpacing |
available methods used to define the spacing between the holes
|
VerifyPenetrationBuilder.SelectionDialogType |
Represents the selection dialog type
|
WeightAndCGBuilder.SelectionMethods |
Settings to indicate how the objects are selected.
|
WeldCut2Builder.CreationMethod |
Creation method used to define the placement of the weld cut
|
WeldCutBuilder.CreationMethod |
Creation method used to define the placement of the weld cut
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.