public static class OrientationDefinitionBuilder.MeasureAngleTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NORMALTO_CURVE
Angles are measured in a plane normal to the landing curve.
|
static int |
_ORTHOGONAL
Angles are measured in an orthogonal plane closest to the normal of the
landing curve.
|
static OrientationDefinitionBuilder.MeasureAngleTypes |
NORMALTO_CURVE
Angles are measured in a plane normal to the landing curve.
|
static OrientationDefinitionBuilder.MeasureAngleTypes |
ORTHOGONAL
Angles are measured in an orthogonal plane closest to the normal of the
landing curve.
|
Modifier and Type | Method and Description |
---|---|
static OrientationDefinitionBuilder.MeasureAngleTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationDefinitionBuilder.MeasureAngleTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationDefinitionBuilder.MeasureAngleTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final OrientationDefinitionBuilder.MeasureAngleTypes NORMALTO_CURVE
public static final OrientationDefinitionBuilder.MeasureAngleTypes ORTHOGONAL
public static final int _NORMALTO_CURVE
public static final int _ORTHOGONAL
public static OrientationDefinitionBuilder.MeasureAngleTypes valueOf(int value)
public static OrientationDefinitionBuilder.MeasureAngleTypes valueOf(String name)
public static OrientationDefinitionBuilder.MeasureAngleTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.