See: Description
Interface | Description |
---|---|
AeroFlangeBuilder |
Represents a Aerospace Sheet Metal Flange Builder.
|
AeroFlatPatternBuilder |
Represents a Flat Pattern feature builder.
|
AeroFlatSolidBuilder |
Represents a Flat As Solid feature builder.
|
AeroJoggleBuilder |
Represents a Aerospace Sheet Metal Joggle Builder.
|
AeroLighteningCutoutBuilder |
Represents a
AeroLighteningCutoutBuilder
To create a new instance of this class, use AeroSheetmetalManager.createAeroLighteningCutoutBuilder(nxopen.features.Feature) Default values. |
AeroReformBuilder |
Represents a Aerospace Sheet Metal REFORM Builder.
|
AeroSheetmetalManager |
Provides methods for manipulating the Knowledge Fusion rules in a part
To obtain an instance of this class, refer to FeatureCollection Created in NX4.0.0 |
AeroUnformBuilder |
Represents a Aerospace Sheet Metal UNFORM Builder.
|
BeadBuilder |
Represents a Bead feature builder.
|
BendBuilder |
Represents a Bend feature builder.
|
BendOptions |
Represents a Sheetmetal Bend Options class.
|
BendTaperBuilder |
Represents a Bend Taper feature builder
To create a new instance of this class, use SheetmetalManager.createBendTaperBuilder(nxopen.features.Feature) Default values. |
BreakCornerBuilder |
Represents a break corner feature builder.
|
BridgeTransitionBuilder |
Represents a Bridge Transition builder
To create a new instance of this class, use SheetmetalManager.createBridgeTransitionBuilder(nxopen.features.Feature) Created in NX5.0.2 |
CleanUpUtilityBuilder |
Represents a Clean-Up Utility builder builder
To create a new instance of this class, use SheetmetalManager.createCleanUpUtilityBuilder() Default values. |
ClosedCornerBuilder |
Represents a Closed corner feature builder.
|
ContourFlangeBuilder |
Represents a Contour Flange feature builder.
|
ConvertToSheetmetalBuilder |
This is the feature builder for the convert to sheetmetal feature.
|
CornerTreatmentBuilder |
The CornerTreatmentBuilder class is used to manage a builder object for
a corner treatment in the flat solid and flat pattern dialogs.
|
DimpleBuilder |
Represents a Dimple feature builder.
|
DrawnCutoutBuilder |
Represents a Drawn Cutout feature builder.
|
EdgeRipBuilder |
Represents a Edge Rip feature builder.
|
EditBendBuilder |
Represents a
EditBend builder
To create a new instance of this class, use SheetmetalManager.createEditBendBuilder(nxopen.features.Feature) Created in NX7.5.0 |
EditCornerBuilder |
Represents a
EditCornerBuilder
To create a new instance of this class, use SheetmetalManager.createEditCornerBuilder() Default values. |
ExportFlatPatternBuilder |
Represents a Export flat pattern builder.
|
FlangeBuilder |
Represents a Flange feature builder.
|
FlatPatternBuilder |
Represents a Flat Pattern feature builder.
|
FlatSolidBuilder |
Represents a Flat As Solid feature builder.
|
FlexibleCableBuilder |
Represents a Flexible Cable feature builder.
|
FlexibleCableSegment |
Represents a Flexible Cable Segment class.
|
GussetBuilder |
Represents a NX Sheet Metal
Gusset builder
To create a new instance of this class, use SheetmetalManager.createGussetBuilder(nxopen.features.Feature) Default values. |
HemFlangeBuilder |
Represents a
HemFlange builder
To create a new instance of this class, use SheetmetalManager.createHemFlangeFeatureBuilder(nxopen.features.Feature) Created in NX5.0.0 |
JogBuilder |
Represents a Jog feature builder.
|
LoftedFlangeBuilder |
Represents a Lofted Flange feature builder.
|
LouverBuilder |
Represents a louver feature builder.
|
MetaformBuilder |
Represents a
Metaform builder
To create a new instance of this class, use SheetmetalManager.createMetaformBuilder(nxopen.features.Feature) Default values. |
MigratedPanelBuilder |
Represents an I-DEAS Migrated Panel feature builder
This builder cannot be instantiated separately. |
MiterOptions |
Represents a Miter Data Options builder.
|
NormalCutoutBuilder |
Represents a NormalCutout feature builder.
|
RebendBuilder |
The Rebend feature class.
|
ResizeBendAngleBuilder |
Represents a
ResizeBendAngle builder
To create a new instance of this class, use SheetmetalManager.createResizeBendAngleBuilder(nxopen.features.Feature) Created in NX5.0.0 |
ResizeBendRadiusBuilder |
Represents a ResizeBendRadius feature builder.
|
ResizeNeutralFactorBuilder |
Represents a Resize Neutral Factor Builder
To create a new instance of this class, use SheetmetalManager.createResizeNeutralFactorBuilder(nxopen.features.Feature) Created in NX5.0.0 |
SheetmetalBaseBuilder |
Represents a Sheet Metal Feature Builder to be used in the creation and modification of features.
|
SheetMetalFromSolidBuilder |
Represents a
nxopen.features.sheetmetalFromSolid builder
(Sheet Metal from Solid). |
SheetmetalManager |
Represents an object that manages sheetmetal features
To obtain an instance of this class, refer to FeatureCollection Created in NX4.0.0 |
SMBoundaryConditionBuilder |
Represents a Boundary condition object for Metaform.
|
SMBoundaryConditionBuilderList |
Represents a list of objects.
|
SolidPunchBuilder |
Represents a
SolidPunchBuilder
To create a new instance of this class, use SheetmetalManager.createSolidPunchBuilder(nxopen.features.Feature) Created in NX5.0.0 |
TabBuilder |
Represents a Tab feature builder.
|
ThreeBendCornerBuilder |
The Three Bend Corner feature class.
|
UnbendBuilder |
The Unbend feature class.
|
Class | Description |
---|---|
AeroFlangeBuilder.CompType |
This method defines the types of Flange Compensation
|
AeroFlangeBuilder.DimType |
This enum defines the flange length dimension types
|
AeroFlangeBuilder.DirType |
This enum defines the type of direction vector
|
AeroFlangeBuilder.EndCompensationData |
This class holds the data returned from
AeroFlangeBuilder.getEndCompensation(nxopen.features.sheetmetal.AeroFlangeBuilder.EndType) |
AeroFlangeBuilder.EndType |
This enum defines the ends of a bend edge
|
AeroFlangeBuilder.LengthData |
This class holds the data returned from
AeroFlangeBuilder.getLength() |
AeroFlangeBuilder.LengthType |
This enum defines the length type options.
|
AeroFlangeBuilder.MatType |
This enum defines the material types
|
AeroJoggleBuilder.SideType |
This enum defines the side of a twin joggle
only side1 is used for a single joggle
|
AeroLighteningCutoutBuilder.Types |
Represents the cutout type.
|
ApplicationContext |
This is the enum representing application context of the feature
|
BeadBuilder.CrossSectionTypeOptions |
This enum represents the cross section type options for the Bead.
|
BeadBuilder.EndTypeOptions |
This enum represents the end type options for the Bead.
|
BeadBuilder.HeightSideOptions |
This enum represents the depth direction for the Bead.
|
BendBuilder.BendDirectionOptions |
This enum represents the Bend Direction for Bend.
|
BendBuilder.BendLocationOptions |
This enum represents the Bend Location (Material Side) for Bend.
|
BendBuilder.FixedSideOptions |
This enum represents the Fixed Side for Bend.
|
BendOptions.BendReliefTypeOptions |
This enum represents the bend relief type.
|
BendOptions.CornerReliefTypeOptions |
This enum represents the corner relief type.
|
BendTaperBuilder.BendTaperInputMethod |
This enum represents the input methods for the bend taper.
|
BendTaperBuilder.BendTaperSides |
This enum represents the taper sides options for the bend taper.
|
BendTaperBuilder.BendTaperType |
This enum represents the bend taper types for the bend taper.
|
BendTaperBuilder.ChainingType | Deprecated
Deprecated in NX8.5.0.
|
BendTaperBuilder.StartType |
This enum represents the start types for the bend taper.
|
BendTaperBuilder.WebTaperType |
This enum represents the web taper types for the bend taper.
|
BreakCornerBuilder.TypeOptions |
This enum represents the break corner type.
|
BridgeTransitionBuilder.InsetOptions |
Enum representing the side of the Bridge Transition material with respect to
the specified tangent plane.
|
BridgeTransitionBuilder.TypeOptions |
Enum representing types for Bridge Transition feature.
|
BridgeTransitionBuilder.WidthDirectionOptions |
Enum representing the width direction for the Bridge Transition.
|
BridgeTransitionBuilder.WidthOptions |
Enum representing width option types for Bridge Transition feature.
|
ClosedCornerBuilder.ClosureTypeOptions |
This enum represents Corner Closure type
|
ClosedCornerBuilder.FacePairData |
This class holds the data returned from
ClosedCornerBuilder.getFacePair(int) |
ClosedCornerBuilder.OriginTypes |
This enum represents Origin type
|
ClosedCornerBuilder.TreatmentTypeOptions |
This enum represents Corner treatment type
|
ClosedCornerBuilder.Types |
This enum represents the feature types.
|
ContourFlangeBuilder.SectionSideOptions |
This enum represents the side of the section in which material is created.
|
ContourFlangeBuilder.SweepSideOptions |
This enum represents the side in which the contour flange will be swept.
|
ContourFlangeBuilder.SweepTypeOptions |
This enum represents the sweep type of the contour flange
|
ConvertToSheetmetalBuilder.BendReliefTypeOptions |
This enum represents the bend relief type.
|
CornerTreatmentBuilder.CornerTreatmentType |
Corner Treatment Type
|
DimpleBuilder.DepthTypeOptions |
This enum represents the depth direction for the dimple.
|
DimpleBuilder.DimensionTypeOptions |
the Dimension options for dimple.
|
DimpleBuilder.SectionSideOptions |
This enum represents the side of the section that the dimple punches material.
|
DimpleBuilder.SidewallTypeOptions |
the side walls material option.
|
DrawnCutoutBuilder.DepthTypeOptions |
This enum represents the depth direction for the drawn cutout.
|
DrawnCutoutBuilder.SectionSideOptions |
This enum represents the side of the section that the drawn cutout punches material.
|
DrawnCutoutBuilder.SidewallTypeOptions |
The side walls material option.
|
EditCornerBuilder.BendClosureTypeOptions |
This enum specifies the type of bend closure required at the corner.
|
EditCornerBuilder.CornerReliefTypeOptions |
This enum specifies the type of relief required at the corner.
|
EditCornerBuilder.FacePairData |
This class holds the data returned from
EditCornerBuilder.getFacePair(int) |
EditCornerBuilder.PlateClosureTypeOptions |
This enum specifies the type of plate closure required at the corner.
|
ExportFlatPatternBuilder.DxfRevisionType |
Specifies the DXF Revisions for flat pattern export
|
ExportFlatPatternBuilder.FileType |
Specifies the flat pattern export type
|
FeatureProperty |
This is a common enum that comprises of values to be used for various features.
|
FlangeBuilder.InsetTypeOptions |
This enum represents the inset type for the material of the flange.
|
FlangeBuilder.LengthTypeOptions |
This enum indicates the two ways that the flange length can be measured.
|
FlangeBuilder.MatchFaceOptions |
This enum represents the match face option for the flange.
|
FlangeBuilder.OffsetTypeOptions |
This enum represents the offset type for the flange.
|
FlangeBuilder.WidthTypeOptions |
This enum represents the width type for the flange.
|
FlatSolidBuilder.TransformComponentsOption |
The enum defines how to represent PCB components on flat solid.
|
FlexibleCableBuilder.BendAngleDirectionOptions |
This enum represents the bend angle direction for the bend segment.
|
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions |
This enum represents the path adjustment angle direction for the bend segment.
|
FlexibleCableBuilder.SegmentTypeOptions |
Represents the Flexible Cable segment options.
|
GussetBuilder.PlacementOriginAndDirectionData |
This class holds the data returned from
GussetBuilder.getPlacementOriginAndDirection() |
GussetBuilder.PlacementTypes |
This enum represents the different options for placing an automatic profile Gusset.
|
GussetBuilder.Shapes |
This enum represents the two different shapes for Gusset.
|
GussetBuilder.Types |
This enum represents the two Gusset Feature types.
|
GussetBuilder.WidthSides |
This enum represents the different options for thickening the user defined profile Gusset.
|
HemFlangeBuilder.BendReliefOptions |
This enum represents the Bend relief type of the hem flange.
|
HemFlangeBuilder.InsetTypeOptions |
This enum represents the inset type for the material of the hem flange.
|
HemFlangeBuilder.TypeOptions |
Represents the Hem Flange type.
|
JogBuilder.BendLocationOptions |
Represents the bend location type.
|
JogBuilder.DimensionTypeOptions |
the Dimension options for jog.
|
JogBuilder.DirectionTypeOptions |
this enum represents the direction for the Jog.
|
JogBuilder.FixedSideOptions |
The "left" option represents the side to the left of a person who is walking along the section in the direction of its curves
when the section normal is pointing up.
|
LoftedFlangeBuilder.SectionSideOptions |
This enum represents the side of the section that the lofted flange creates thickness.
|
LouverBuilder.DepthSideOptions |
This enum represents the depth side for the louver.
|
LouverBuilder.EndTypeOptions |
This enum represents the end type for the louver.
|
LouverBuilder.SectionSideOptions |
This enum represents the side of the section that the louver width is measured.
|
MiterOptions.ClosedCornerTypeOptions |
the closed corner type options.
|
MiterOptions.PositionOptions |
the miter positions options.
|
MiterOptions.TypeOptions |
the miter type options.
|
NormalCutoutBuilder.CutTypeOptions |
This enum represents the cut type for the normal cutout.
|
NormalCutoutBuilder.DepthSideOptions |
This enum represents the depth direction for the normal cutout.
|
NormalCutoutBuilder.DepthTypeOptions |
This enum represents the depth type for the normal cutout.
|
NormalCutoutBuilder.SectionSideOptions |
This enum represents the side of the section that the normal cutout removes material.
|
NormalCutoutBuilder.TypeOptions |
Represents the type of the normal cutout - sketch type OR 3D-curve type
|
ResizeBendRadiusBuilder.BendReliefTypeOptions |
This enum represents the bend relief type.
|
ResizeBendRadiusBuilder.Types |
This enum represents the feature types.
|
SheetmetalBendParameters |
This structure contains the bend parameters for a Sheet Metal bend area.
|
SheetmetalBendState |
Bend State
|
SheetmetalFaceLayer |
Face Layer
|
SheetmetalFaceType |
Face Type
|
SheetmetalManager.InnerBendFacesData |
This class holds the data returned from
SheetmetalManager.getInnerBendFaces(nxopen.Body) |
SheetmetalManagerFlangeWidthOption |
Flange width option
|
SheetmetalManagerTabSweepDir |
This enum is for Tab sweep direction flag.
|
SheetmetalManagerTabType |
This is the enum for Tab type i.e. base tab and secondary tab.
|
SMBoundaryConditionBuilder.ConstraintTypes |
Types of Boundary condition constraints
|
SolidPunchBuilder.Types |
Represents the punch type
|
TabBuilder.SectionSideOptions |
This enum represents the side of the section that the dimple punches material.
|
TabBuilder.ThicknessSideOptions |
This enum represents the extent direction for the Tab.
|
ThreeBendCornerBuilder.FacePairData |
This class holds the data returned from
ThreeBendCornerBuilder.getFacePair(int) |
ThreeBendCornerBuilder.OriginTypes |
This enum represents Origin type
|
ThreeBendCornerBuilder.TreatmentTypeOptions |
This enum represents the corner treatment type.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.