public static class ShipDesignPreferencesBuilder.AngleRuleTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_RIGHT_HAND
Angle is measured using the right hand rule system.
|
static int |
_SHIP_ORIENTATION
Angle direction and reference position is determined by the location in the ship.
|
static ShipDesignPreferencesBuilder.AngleRuleTypes |
RIGHT_HAND
Angle is measured using the right hand rule system.
|
static ShipDesignPreferencesBuilder.AngleRuleTypes |
SHIP_ORIENTATION
Angle direction and reference position is determined by the location in the ship.
|
Modifier and Type | Method and Description |
---|---|
static ShipDesignPreferencesBuilder.AngleRuleTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipDesignPreferencesBuilder.AngleRuleTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipDesignPreferencesBuilder.AngleRuleTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShipDesignPreferencesBuilder.AngleRuleTypes RIGHT_HAND
public static final ShipDesignPreferencesBuilder.AngleRuleTypes SHIP_ORIENTATION
public static final int _RIGHT_HAND
public static final int _SHIP_ORIENTATION
public static ShipDesignPreferencesBuilder.AngleRuleTypes valueOf(int value)
public static ShipDesignPreferencesBuilder.AngleRuleTypes valueOf(String name)
public static ShipDesignPreferencesBuilder.AngleRuleTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.