public static class RollingLineBuilder.StartEvaluationTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NEW_POINT
Use the newly created, or specified, point as the seed point to start the evaluation.
|
static int |
_POINT_ON_FACE
Use a point on the selected face to start the evaluation.
|
static int |
_SHEET_MIDPOINT
Use the midpoint of the sheet as the seed point for evaluation.
|
static RollingLineBuilder.StartEvaluationTypes |
NEW_POINT
Use the newly created, or specified, point as the seed point to start the evaluation.
|
static RollingLineBuilder.StartEvaluationTypes |
POINT_ON_FACE
Use a point on the selected face to start the evaluation.
|
static RollingLineBuilder.StartEvaluationTypes |
SHEET_MIDPOINT
Use the midpoint of the sheet as the seed point for evaluation.
|
Modifier and Type | Method and Description |
---|---|
static RollingLineBuilder.StartEvaluationTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RollingLineBuilder.StartEvaluationTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RollingLineBuilder.StartEvaluationTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final RollingLineBuilder.StartEvaluationTypes SHEET_MIDPOINT
public static final RollingLineBuilder.StartEvaluationTypes POINT_ON_FACE
public static final RollingLineBuilder.StartEvaluationTypes NEW_POINT
public static final int _SHEET_MIDPOINT
public static final int _POINT_ON_FACE
public static final int _NEW_POINT
public static RollingLineBuilder.StartEvaluationTypes valueOf(int value)
public static RollingLineBuilder.StartEvaluationTypes valueOf(String name)
public static RollingLineBuilder.StartEvaluationTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.