public static class RollingLineBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_GEODESIC
Create a single geodesic line on the surface.
|
static int |
_MANUAL
Creates a single line on the surface where the maximum force is to be applied.
|
static int |
_PRESSURE
Create multiple lines on the surface where the tangential for each line is constant on intersecting plane sections.
|
static int |
_STEPPED_PRESSURE
Create a saw tooth set of curves on the surface where the tangential for each line is constant on intersecting plane sections.
|
static RollingLineBuilder.Types |
GEODESIC
Create a single geodesic line on the surface.
|
static RollingLineBuilder.Types |
MANUAL
Creates a single line on the surface where the maximum force is to be applied.
|
static RollingLineBuilder.Types |
PRESSURE
Create multiple lines on the surface where the tangential for each line is constant on intersecting plane sections.
|
static RollingLineBuilder.Types |
STEPPED_PRESSURE
Create a saw tooth set of curves on the surface where the tangential for each line is constant on intersecting plane sections.
|
Modifier and Type | Method and Description |
---|---|
static RollingLineBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RollingLineBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RollingLineBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final RollingLineBuilder.Types MANUAL
public static final RollingLineBuilder.Types PRESSURE
public static final RollingLineBuilder.Types GEODESIC
public static final RollingLineBuilder.Types STEPPED_PRESSURE
public static final int _MANUAL
public static final int _PRESSURE
public static final int _GEODESIC
public static final int _STEPPED_PRESSURE
public static RollingLineBuilder.Types valueOf(int value)
public static RollingLineBuilder.Types valueOf(String name)
public static RollingLineBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.