public static class AlongGuideCutBuilder.WaterStopOffsetMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ASYMMETRIC
The left offset and right offset are asymmetric
|
static int |
_SYMMETRIC
The left offset and right offset are symmetric
|
static AlongGuideCutBuilder.WaterStopOffsetMethod |
ASYMMETRIC
The left offset and right offset are asymmetric
|
static AlongGuideCutBuilder.WaterStopOffsetMethod |
SYMMETRIC
The left offset and right offset are symmetric
|
Modifier and Type | Method and Description |
---|---|
static AlongGuideCutBuilder.WaterStopOffsetMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlongGuideCutBuilder.WaterStopOffsetMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlongGuideCutBuilder.WaterStopOffsetMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final AlongGuideCutBuilder.WaterStopOffsetMethod SYMMETRIC
public static final AlongGuideCutBuilder.WaterStopOffsetMethod ASYMMETRIC
public static final int _SYMMETRIC
public static final int _ASYMMETRIC
public static AlongGuideCutBuilder.WaterStopOffsetMethod valueOf(int value)
public static AlongGuideCutBuilder.WaterStopOffsetMethod valueOf(String name)
public static AlongGuideCutBuilder.WaterStopOffsetMethod[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.