public static class SeamBuilder.DefinitionMethods extends Enum
SeamBuilder.Types.INTERSECTION
.Modifier and Type | Field and Description |
---|---|
static int |
_CURVES_PLANES_SHIP
Can use curves, planes or other ship structure to define the seam location.
|
static int |
_EQUALLY_SPACED
Create a specified number of seams equidistant between two selected curves.
|
static int |
_RECTANGULAR
Create a rectangular pattern of seams based on an origin, direction, and size of rectangles.
|
static SeamBuilder.DefinitionMethods |
CURVES_PLANES_SHIP
Can use curves, planes or other ship structure to define the seam location.
|
static SeamBuilder.DefinitionMethods |
EQUALLY_SPACED
Create a specified number of seams equidistant between two selected curves.
|
static SeamBuilder.DefinitionMethods |
RECTANGULAR
Create a rectangular pattern of seams based on an origin, direction, and size of rectangles.
|
Modifier and Type | Method and Description |
---|---|
static SeamBuilder.DefinitionMethods |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeamBuilder.DefinitionMethods |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeamBuilder.DefinitionMethods[] |
values()
Returns an array that contains the values for this enum.
|
public static final SeamBuilder.DefinitionMethods CURVES_PLANES_SHIP
public static final SeamBuilder.DefinitionMethods EQUALLY_SPACED
public static final SeamBuilder.DefinitionMethods RECTANGULAR
public static final int _CURVES_PLANES_SHIP
public static final int _EQUALLY_SPACED
public static final int _RECTANGULAR
public static SeamBuilder.DefinitionMethods valueOf(int value)
public static SeamBuilder.DefinitionMethods valueOf(String name)
public static SeamBuilder.DefinitionMethods[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.