Represents a shell template feature. The template is made up of a grid of
sheets, or thin solids, that would physically sit on the floor and the ship
shell (typically the hull) would be placed on top of the templates to measure
and verify the shape of the shell. The physical fixture eventually created in
the manufacturing environment may be framed inside (or together) with a box.
To create or edit an instance of this class, use
ShellTemplateBuilder
Created in NX8.0.0