public static class CuttingSideFacesBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
Process all the visible solids to assign the cutting side face attributes.
|
static int |
_MANUAL
Process all the selected solids to assign the cutting side attributes.
|
static int |
_REVERSE
Reverse the cutting side attributes of the selected solids.
|
static CuttingSideFacesBuilder.Types |
AUTOMATIC
Process all the visible solids to assign the cutting side face attributes.
|
static CuttingSideFacesBuilder.Types |
MANUAL
Process all the selected solids to assign the cutting side attributes.
|
static CuttingSideFacesBuilder.Types |
REVERSE
Reverse the cutting side attributes of the selected solids.
|
Modifier and Type | Method and Description |
---|---|
static CuttingSideFacesBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CuttingSideFacesBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CuttingSideFacesBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final CuttingSideFacesBuilder.Types AUTOMATIC
public static final CuttingSideFacesBuilder.Types MANUAL
public static final CuttingSideFacesBuilder.Types REVERSE
public static final int _AUTOMATIC
public static final int _MANUAL
public static final int _REVERSE
public static CuttingSideFacesBuilder.Types valueOf(int value)
public static CuttingSideFacesBuilder.Types valueOf(String name)
public static CuttingSideFacesBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.