public static class ExcessMaterialBuilder.VersionID extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NX902
This feature builder is used to create or edit an NX902 or beyond feature.
|
static int |
_ORIGINAL
This feature builder is used to edit an existing NX75 - NX901 excess material feature.
|
static ExcessMaterialBuilder.VersionID |
NX902
This feature builder is used to create or edit an NX902 or beyond feature.
|
static ExcessMaterialBuilder.VersionID |
ORIGINAL
This feature builder is used to edit an existing NX75 - NX901 excess material feature.
|
Modifier and Type | Method and Description |
---|---|
static ExcessMaterialBuilder.VersionID |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExcessMaterialBuilder.VersionID |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExcessMaterialBuilder.VersionID[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExcessMaterialBuilder.VersionID ORIGINAL
public static final ExcessMaterialBuilder.VersionID NX902
public static final int _ORIGINAL
public static final int _NX902
public static ExcessMaterialBuilder.VersionID valueOf(int value)
public static ExcessMaterialBuilder.VersionID valueOf(String name)
public static ExcessMaterialBuilder.VersionID[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.